Hi
These questions pertain to CCSv4.1.3 graphs selected by doing Tools->Graph->Single Time
1) Is there a way to make the x-axis refresh start at zero instead of continuing from zero each time the graph is refreshed? It would be really handy for viewing arrays to NOT have the x-axis roll its values and restart at zero.
2) Why does the "reset the graph" button destroy the data. You have to select "show the graph properties" and select OK to get the graph data displayed again.
3) When I select "Toggle measurement marker mode", the cute little bubbles follow my cursor as I move along the x-axis. But if I move the cursor to the point where one of the bubbles exit the left side of the graph, the bubbles are gone and can't get them back. This means you can't use the marker on the left most point. Bug perhaps?
4) Is there a way to delete say the X2 marker without having to start over again?
Cheers