This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error 0x80002240/-151 Fatal Error during: Initialization, OCS, Control



Hi,

Can somebody tell me why these errors occur and how to fix them?

Error connecting to the target: Error 0x80002240/-151 Fatal Error during: Initialization, OCS, Control, This error was generated by TI's USCIF driver.

SC_ERR_POD_OPEN <-151> This utility failed to open the adapter for a custom emulator. The adapter returned an error.

the borad had already worked and was conected to target well, I start to get this error  after physically move the board and bring it back,

I tried the solution  I saw in the suport forum of TI , witout any success

 I checked also that the HW connection (USB and power)  are ok.

Awaitng reply.

Thanks.

R.A