This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
https://www.components-mart.com/datasheets/10/BOOST-CC2564MODA.pdf
Hi.
We have studied the above link.
By using the CCS to build / flash the code onto MSP432.
It won't work.
It will only show us those logs:
OpenStack().
Stack Init Failed: -4.
Unable to open the stack.
So, may you tell us how to solve this?
Do we have re-work the jumper or anything?
What's the SW config to make it work?
BR Rio
Hi .
I also read this:
http://www.ti.com/lit/ug/swru453b/swru453b.pdf
In the section as the below:
4. Move nSHUTD to nS2 on the BOOST-CC2564MODA jumper J5.
5. Add a jumper to TX_DBG on J8.
6. Ensure that J22 and J4 are DNI.
7. Populate J1 and J2.
8. Stack the BOOST-CC2564MODA onto the CC31XXEMUBOOST.
9. Fit the CC31XXEMUBOOST onto the MSP-EXP432P401R LaunchPad development kit.
Can you tell me the
A. Step6, where is the J22 / J4?
B. What is DNI?
C. Where is J1/J2?
D. I'm using the SDK v4.2.1.1, does this SDK working as the PDF saying?
BR Rio
Rio,
If you look at figure 4 and 5, there is a pictures of the jumper placements required for the different stack ups. I would suggest following what the jumper placement here.
For the SDK, did you download the latest from here? http://www.ti.com/tool/CC256XMS432BTBLESW
Best Regards,
Vince
Rio,
Let me know if you have any other questions on this issue. If you have another issue, please create a new thread.
Best Regards,
Vince