I want to replace the current light engine with a 780 nm laser. How reflective are the mirrors at this wavelength?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eldon,
Welcome to TI DLP E2E Forum.
The mirror surface reflectivity is 88% nominally for visible illumination (420-700nm). For 780nm wavelength, it is in between 86-87%. You have to be aware that TI does not guarantee the same performance beyond the values specified in the DLP3000 datasheet .
Regards,
Divya