Hi community member,
I have a question about the description in datasheet.
The datasheet of C5535 is described it as below.
-----------------------------------------------------------------------------------------------
> 6.3.1 Power-Supply Sequencing
>
> Note: If the device is powered up with the USB cable connected to
> an active USB host and the USB PHY (USB_VDDA3P3) is powered up
> before the USB Core (USB_VDD1P3, USB_VDDA1P3), the USB Core must
> be powered within 100 ms after the USB host detects the device has
> been attached.
-----------------------------------------------------------------------------------------------
I do not understand that "the USB host detects the device has been attached".
Which the timing does this description pointed out?
1) USB_DP will be Pull-up.
2) The voltage of USB_VBUS will be exceeded the threshold of settings values in host.
3) Others case.
If other case, would you please explain the timing?
If you have any questions, please let me know.
Best regards.