This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320c6474 can not ping through

Hi,everyone!

 I am using the einfochips evm, TMDSEVM6474L.

MCSDK  1.0.0.8

CSL:sprc975-csl6474.zip    03.04.00.01

NDK:2.0  Version 2.00.00 Release

CCS:5.3.0.00090  compiler:7.4.1

BIOS: 5.42.0.7

src_6474.rar

[C64XP] Core Number on which NDK is running = 0
EFUSED MAC Address = 0c-22-38-4e-0c-22
Only on CORE 0: SGMII reset successful........
Only on CORE 0: SGMII config successful........
Only on CORE 0: SerDes should be up and running
EMAC has been started successfully
Registeration of the EMAC Successful
Network Added: If-1:192.168.1.88
EchoSrv Initialized
Link Status: 100Mb/s Full Duplex on PHY 1
Link Status: No Link on PHY 1
Link Status: 100Mb/s Full Duplex on PHY 1

I can not ping through. Please help me, or who can give me an example which can use PC ping the TMDSEVM6474 through? Thank you!