When I build and run the HUA or Image Processing Demos from the MCSDK, I am not getting an IP address displayed. However, the out-of-box HUA demo that loads from the board's NOR flash works correctly. I have already looked at this page and I don't think it is a problem. I am using DHCP. http://processors.wiki.ti.com/index.php/MCSDK_HUA_Guide#The_CIO_console_window_does_not_show_the_IP_address I did run gel file prior to connecting to the cores. CCS version: CCS_5.0.3.00028 MCSDK version: mcsdk_2_00_01_12 Jumper settings are below (set to little endien, emif16 + emulator boot): SW3 off on on on SW4 on on on on SW5 on on on off SW6 on on on on SW9 on on ------------------------------------ Console Log is below: MCSDK IMAGE PROCESSING DEMONSTRATION QMSS successfully initialized CPPI successfully initialized PA successfully initialized Configuring DHCP client PASS successfully initialized Ethernet subsystem successfully initialized Ethernet eventId : 48 and vectId (Interrupt) : 7 Verify_Init: Expected 16 entry count for gTxFreeQHnd queue 736, found 0 entries Verify_Init: Expected 18 entry count for gRxFreeQHnd queue 737, found 20 entries Verify_Init: Expected 0 entry count for gRxQHnd= 704, found 16 entries Verify_Init: Expected 0 entry count for Queue number = 704, found 16 entries Verify_Init: Expected 0 entry count for Queue number = 4095, found 21 entries Warning:Queue handler Verification failed Registration of the EMAC Successful, waiting for link up .. Service Status: DHCPC : Enabled : : 000 Service Status: HTTP : Enabled : : 000 Service Status: DHCPC : Enabled : Running : 000 Service Status: DHCPC : Enabled : Fault : 002 Service Status: DHCPC : Disabled : : 000 Service Status: DHCPC : Enabled : : 000 Service Status: DHCPC : Enabled : Running : 000 Service Status: DHCPC : Enabled : Fault : 002 Service Status: DHCPC : Disabled : : 000 Service Status: DHCPC : Enabled : : 000 Service Status: DHCPC : Enabled : Running : 000 Service Status: DHCPC : Enabled : Fault : 002 Service Status: DHCPC : Disabled : : 000 Service Status: DHCPC : Enabled : : 000 Service Status: DHCPC : Enabled : Running : 000 Service Status: DHCPC : Enabled : Fault : 002 Service Status: DHCPC : Disabled : : 000
When I build and run the HUA or Image Processing Demos from the MCSDK, I am not getting an IP address displayed.
However, the out-of-box HUA demo that loads from the board's NOR flash works correctly.
I have already looked at this page and I don't think it is a problem. I am using DHCP.
http://processors.wiki.ti.com/index.php/MCSDK_HUA_Guide#The_CIO_console_window_does_not_show_the_IP_address
I did run gel file prior to connecting to the cores.
CCS version: CCS_5.0.3.00028
MCSDK version: mcsdk_2_00_01_12
Jumper settings are below (set to little endien, emif16 + emulator boot):
SW3 off on on on
SW4 on on on on
SW5 on on on off
SW6 on on on on
SW9 on on
------------------------------------
Console Log is below:
MCSDK IMAGE PROCESSING DEMONSTRATION
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
Configuring DHCP client
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Verify_Init: Expected 16 entry count for gTxFreeQHnd queue 736, found 0 entries
Verify_Init: Expected 18 entry count for gRxFreeQHnd queue 737, found 20 entries
Verify_Init: Expected 0 entry count for gRxQHnd= 704, found 16 entries
Verify_Init: Expected 0 entry count for Queue number = 704, found 16 entries
Verify_Init: Expected 0 entry count for Queue number = 4095, found 21 entries
Warning:Queue handler Verification failed
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC : Enabled : : 000
Service Status: HTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Hi,
Not sure if your jumper settings are set to run from the Nor Flash and then you are connecting the CCS and loading HUA/Image processing application? If that is the case, then you may want to do system reset before loading and executing the .out file from CCS.
The same is true (system reset is needed) when you execute the HUA and would like to reload the program for next runs.
Summary:
Can you please try system reset before loading and executing the .out file? It appears like the QMSS is not in initial condition.
-Thanks,
Aravind
My jumper settings were correct.
It seems to work if I reset the board every time. Thanks!