Hi,
Is there a way to use VLIB with the C6678 dsp?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I believe that there will be a release of the VLIB object code that is compatible with C66x in the September timeframe. It needs to be ELF format to be compatible with the C66x family and I have been told that there is a C674x ELF release coming in this timeframe that will be compatible. I'd suggest going through the VLIB request form at:
http://www.surveymonkey.com/s.aspx?sm=_2biqVh_2br0FuVP1h5_2fQ0gZdQ_3d_3d
Regards,
Travis
We cannot post the VLIB binary directly on the forums. Can you please send an email to the following email id, requesting the library and we can ship the library to you.
Regards,
Rahul
Hi
We have just purchased two eval boards for the C6678 chips. I was wondering if VLIB was now available for that platform.
thanks.
Azhar,
The VLIB download location is being updated with the new installers that have the ELF version of VLIB that can used on C6678. If the installers are not uploaded by tomorrow, I will send you a separate email with the latest installers. Please understand the ELF version of VLIB is not a C66X optimized version of the library yet, it is merely the library built in the ELF binary format that is compatible with the C66x software stack. You are likely to see the same performance as C64X+ with the current version. An updated C66X version of VLIB library should be available for download early next year..
Thanks and Regards,
Rahul
PS: We have received your email on the developers email list and will respond to your request based on the updates on the VLIB download page.
Hi Rahul
If I check under my myRegistered Software and look for updates for VLIB, I don't see the new version. Can you please email me the installers. Also, there is a fixed path in the *.pjt file for the VLIB test example. We modified the path in the pjt file but it still looks for a CCSV3.3 path:
################################################################################
# Automatically-generated file. Do not edit!
################################################################################
# Add inputs and outputs from these tool invocations to the build variables
LIB_SRCS += \
C:/CCStudio_v3.3/C6000/cgtools_6.0.16/lib/rts6400.lib
Please advise.
thanks
Azhar
I am also looking for the c6678 version of the VLIB. I have access to the standard one for c64 only.
Scott,
The C66x VLIB is not released yet. I'll check to see if I can get a status on when that might happen.
Regards,
Travis
Update - Please see the announcement:
Regards,
Travis