Hi,
We are using TMS320C6657CZH25 and TMS320C6657CZH with LM10011SD.
Both TMS320C6657CZH25 and TMS320C6657CZH output 6-bit VCNTL signals by the reset release after the sequence of the power supplies in our board.
These VCNTL signals are corresponding to VCNTL value of register 0x02350014 in bit 21 to 16.
The value of register 0x02350014 in TMS320C6657CZH25 is 0x0FFF0000. This is same value in every TMS320C6657CZH25.
In TMS320C6657CZH, the value is different in every device. One of them is 0x07DF0000.
CVDD for TMS320C6657CZH is controlled to about 0.9V. But CVDD for TMS320C6657CZH25 is 1.1V, It doesn't change from an initial voltage.
Power consumption of TMS320C6657CZH is from beginning to end steady.
It of TMS320C6657CZH25 keeps increasing depending at the own temperature. It is saturated with about 6-watt.
We think that we have appropriately cooled it.
1. Do we keep using TMS320C6657CZH25 in CVDD is 1.1V?
2. How much is appropriate power consumption of TMS320C6657CZH25?
3. Should I control CVDD for TMS320C6657CZH25?
My best regards.