This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 spi boot to rapid io boot

Hello,

Using c6678 evm is it possible to:

- use nor writer to write a srio boot parameter table to the nor flash which confis srio to 4 lanes

- confiig the evm switch to spi boot

- power cycle the board and  than see the board eventually ready to rapid io boot in 4 lanes

help needed in:

- for spi boot, is it enough to write the flash with a single srio boot parameter table ?

- how to correctly write the srio parameter table to the flash

Thanks