This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Generating MSI interrupts



The PCIe User Guide (SPRUGS6C) on page 87 describes the MSI_IRQ register: 'This register is written to by the remote device (value = 0-FFFFFFFFh). Writes initiated by an EP over PCIe link that target BAR0 of the RC land to this register if the offset matches. To generate MSI Interrupt 0, the EP should write 0x0000_0000 to this register. It will result in a pulse on bit zero triggering the MSI interrupt from PCIESS to the external processor.'

Is the actual meaning of the value written to this register documented anywhere?

How would I generate MSI Interrupt 1, for example?

Is there an error in the document and the written value should be (1<<n)  to generate MSI int n?

In section 2.14.2.2, the same document gives a procedure for generating an MSI interrupt (which surprisingly does not mention the MSI_IRQ register at all), step 5 states 'Depending upon the number of MSI interrupts allocated, issue a memory write transaction with the address the same as MSI Address Register and the data the same as the MSI Data Register. In the data, the LSBs can be modified to reflect the appropriate MSI event that needs to be notified to root complex'

What does 'Depending on the number of MSI interrupts allocated mean'? Surely the number of interrupts allocated (handled?) determines the interrupts you wish to generate, not how you generate them.

How exactly are the LSBs modified to reflect (select? determine? choose?) the MSI event? I assume that the MSI Address register references the target's MSI_IRQ register (32 bits) but only 16 bits of the data register are valid. How do these two match?

  • There are 8 groups of MSI interrupts (MSI 0~7) and each group has 4 vectors (MSI vector 0-31). You should write MSI vector value into MSI_IRQ to trigger corresponding interrupt, such as write 0x0 to trigger MSI vector 0 (MSI_0 event), write 0x1 to trigger MSI vector (MSI_1 event), etc.

    Section 2.14.2.2 describes the general rule of generating MSI interrupt from EP to RC. RC will put the MSI_IRQ offset to the MSI Address register and assign vector value to MSI DATA register for each EP during the enumeration/initialization process. 

    There are several threads discussing about PCIe MSI interrupt. Please take a look and hope they could cover your questions.

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/166202.aspx

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/194406/717007.aspx#717007

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/199151/711351.aspx#711351

  • Thank you for that information.

    I would be grateful if you would let me know exactly where in the User Guide it makes clear that ' You should write MSI vector value into MSI_IRQ to trigger corresponding interrupt, such as write 0x0 to trigger MSI vector 0 (MSI_0 event), write 0x1 to trigger MSI vector (MSI_1 event), etc.'

  • Peter,

    It is based on our experiments. And we will make it clear in the MSI_IRQ description in the next release of PCIe user guide.Thanks.

  • Unfortunately, there are far too many occasions when the only way to discover of how a TI device works is to experiment. Your users would be saved a great deal of wasted effort if the documentation were completely rewritten with the aim of making it possible for users to understand unambiguously how to use the hardware. Far too much is assumed or described in an inadequate way.

  • On further reflection, I am not much further forward than when I started.

    You wrote 'There are 8 groups of MSI interrupts (MSI 0~7) and each group has 4 vectors (MSI vector 0-31)'. I assume that you are using the term 'vector' in two contexts: 'vector' meaning one of the 4 items in each group and 'MSI vector' meaning the (unspecified) combination of group and 'vector'.

    So we have 32 possible values.

    You then write 'You should write MSI vector value into MSI_IRQ to trigger corresponding interrupt, such as write 0x0 to trigger MSI vector 0 (MSI_0 event), write 0x1 to trigger MSI vector (MSI_1 event), etc.'.

    The value written to the MSI_IRQ register is therefore a value in the range 0..31. This would suggest that only 5 bits of the register are used, yet the User Guide says 'This register is written to by the remote device (value = 0-FFFFFFFFh)'.  Is this another error in the User Guide?

    What happens if I write the value 14 to MSI_IRQ? Is that group 3 vector 2 or group 6 vector 1?


    I also note this gem in section 2.14.5.1: 'In addition, the software drivers for downstream devices must ensure that the data transaction that is expected to complete before interrupt is triggered in RC device's CPU has completed. Because PCIe write transactions are posted, it is not necessary that a write from EP to system memory in RC has completed before a write to MSI interrupt generation register has completed. This could create a potential race condition.'

    As interrupts are the mechanism usually used to indicate the completion of an operation, how would you suggest that software ensures the transaction has completed? I note that I have been unable to find an example of PSIe transfers that uses interrupts and polling is used instead. This would be intolerable in real code.

  • Please take a look at Table 2-10 in PCIe user guide. If you are writing value 14 (0xE) into MSI_IRQ, the MSI6_IRQ will be generated since MSI 6 includes vectors 6/14/22/30.

    The section 2.14.5.1 talks about the possibility that the PCIe Root Complex or switches could reorder the memory write transactions just posted ahead of previously posted memory write transactions or message transactions. Similarly, message transactions just posted may be ordered ahead of previously posted memory write or message transactions due to the relax ordering feature in PCIe.

     Memory write and Message transactions are treated the same in most respects: both are handled as posted operations, both are received into the same Posted buffer, and both are subject to the same ordering requirements.

     So if the “relaxed ordering” is enabled, the Root Complex or switches are given the permission to move this transaction ahead of others, whereas the action is normally prohibited in strongly ordering case.

     The relaxed ordering could improve the performance of the post transactions while it could potentially cause issues if the reordering is not permitted in some circumstances.

     In the RC mode, the user could disable the relaxed ordering feature by clearing the “RELAXED” field (bit4) to 0 in “DEV_STAT_CTRL” register. The RC could also clear “RELAXED” field (bit1) to 0 in “TLPCFG” register to disable the reordering request for all outgoing TLPs.

     For more details, please take a look at the PCIe standard specification from PCISIG, such as section 2.4 "Transaction Ordering" in PCI_Express_Base_Rev_2.0 document.

    Hope the above info helps.

  • Thank you for the explanation; your life could have meen made much easier had the documentation been adequate.

    I find it difficult to see how I could be expected to work out what you wrote from the descriptions in the User Guide.

    Table 2-10 includes a column simply labelled 'Interrupt'; does this column and its values have any meaning at all?

    Your description shows that only the bottom 3 bits of MSI_IRQ are relevant. Why doesn't the documentation say this? Is the actual value written to MSI_IRQ (all 32 bits) readable by the interrupted processor? In other words, if I generate interrupt 1 by writing 1 or 9 to MSI_IRQ, can the interrupted processor read MSI_IRQ to determine which was used? Also, why make any mention of interrupts 8-31 as from a practical point of view they don't exist?

    Similarly, how am I supposed to make the leap from 'software drivers for downstream devices must ensure...' to 'clear the RELAXED bit in DEV_STAT_CTRL'? Don't you think it might be a little bit helpful to reference that bit in the place where its use is crucial? Even then, the description of RELAXED isn't particularly helpful. The actual description is probably in yet another document, but it wouldn't take much thought to make the description of the race condition and the solution quite clear.

    Not only is the documentation incomplete, it is actually misleading.

  • 1. The interrupt column number in Table 2-10 is used in IRQ_EOI register to clear the interrupt. For example, in order to clear interrupt event triggered by MSI0 vector 0, the user needs to write 1 to bit 0 in MSI0_IRQ_STATUS register and also write 4 (MSI_0 is interrupt 4 in table 2-10) to IRQ_EOI register to indicate the end of this interrupt, which will enable the same event to be triggered again.

    2. MSI_IRQ will be written only, read will return all zeros. Please read the MSIn_IRQ_STATUS register for the status of the interrupt event. Again, we will update the description of MSI_IRQ register in the user guide. Sorry for the confusion.

    3. We will try to connect the race condition and "relaxed" bit description in the user guide as well. You may notice that there are lots of PCIe standard terms or register descriptions are not expanded in this TI PCIe user guide. The user will have to refer to the PCIe standard specification as well. But we will try to describe TI specific PCIe usage clearly in this document and make the user guide more complete and user friendly. Thanks for your suggestions.

  • It is good to hear that you will be revising the documentation, but I fear it will simply be a few tweaks here and there. The actual problem is that there are far too many assumptions built into the text. Once you have discovered what the text means, it's usually obvious, but until then it is open to interpretation. The whole point of documentation is to make things unambiguously clear.

    For example, the clearing of the interrupt status you refer to is described as: 'Each bit indicates status of MSI vector (24, 16, 8, 0) associated with the bit. Each of the bits can be written with 1 to clear the respective interrupt status bit.'. This assumes that you will guess that (24, 16, 8, 0) associates 24 with bit 3, 16 with bit 2, 8 with bit 1 and 0 with bit 0 (rather than 24 with bit 0 and so on). Simply labelling the four bits in question in the diagram above would remove any possibility of misunderstanding and allow a simpler description.

    The documentation needs to be completey rethought with the aim of making it clearly describe the device and how it is used (it is a User Guide after all), rather than leaving it in the current form which is essentially a list of separate features with little describing their interaction. As another example, try to find where the 'Interrupt Support' section mentions anything at all about interrupt acknowledgement. For that, you just have to know you should write to the IRQ_EOI register (fairly obvious) and, not so obviously, also write to the MSIx_IRQ_STATUS register. Who would suspect that you write to a status register?