This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
Environment description:Evm C6670, no IBL not EVM, boot from spi directly, the norflash is connected to the DSP via CS0. The norflash can read and write correctly. Now we have success on booting a dummy project(Hello World and LED flash).But we failed on booting our own project, parts of codes need to be load to DDR in our project and we guess the reason is the DDR is not config before loading the codes. Our project needs to use DDR to store some of the codes. According to my understand, maybe we should use boot configuration table to config the DDR before loading codes to L2 and DDR. Here are my question, I hope someone can help because it is urgent and has block for couple weeks.
1)Here is my .bat file , .map file and .rmd file. These three files can create the correct image if there is no need to use DDR(like my dummy project). I want to know if there are any parts I should modified when I use boot configurantion table to config DDR?Especially the options part in the spi.map file.
runscript.bat
..\utilities\hex6x -order L ..\utilities\boot_script.rmd bootcode.out
..\utilities\b2i2c boot_code.btbl boot_code.btbl.i2c
..\utilities\b2ccs boot_code.btbl.i2c boot_code.btbl.i2c.ccs
..\utilities\romparse ..\utilities\spi.map
ren i2crom.ccs spirom.ccs
copy spirom.ccs spirom_le.dat
echo generate the dat file from spirom_dat.ccs
..\utilities\byteswapccs spirom.ccs spirom_le.swap.dat
echo generate 2 bin files from spirom.ccs
..\utilities\ccs2bin spirom.ccs spirom_le.bin
..\utilities\ccs2bin -swap spirom.ccs spirom_le.swap.bin
bootscript.rmd
-a
-boot
-e _c_int00
ROMS
{
ROM1: org = 0x800000, memwidth = 32, romwidth = 32
files = { boot_code.btbl }
}
spi.map
section {
param_index = 0
boot_mode = 50
sw_pll_prediv = 1
sw_pll_mult = 20
sw_pll_postdiv = 2
sw_pll_flags = 1
options = 1
core_freq_mhz = 1000
next_dev_addr_ext = 0x0
c2t_delay = 0
bus_freq_mhz = 20
bus_freq_khz = 0
addr_width = 24
n_pins = 4
mode = 1
csel = 0
exe_file = "boot_code.btbl.i2c.ccs"
}
2)According to my understanding, we should use the boot configurantion table to config the DDR.And we know what the boot configurantion table like and what each section of boot configuration table means. But we have no idea how to append the boot configurantion table to the boot table, which mentioned in the Bootloader's users' guild. Can someone gives us some examples or some advices and suggestions?Thank you! Expect for your help or support!
Best Regards,
Karlphy
As the boot loader user guide suggests, the romparse utility was created to append boot parameter table and boot configuration table to the boot table. However in the current form the romparse is only used to append boot parameter tables. For DDR configurations you will need to create a pragma DATA_Section in your main function that places the DDR configuration table in the DDR config memory space. The boot loader copies this DDR configuration table when it loads the application binary and when it notices the change in the DDR configuration memory section it will proceed to initialize DDR before loading the DDR sections of your application binary.This is demonstrated in the .bat file included in the example attached.
Please look at the example attached. The parameter table in the nysh.spi.map provides the modified SPI boot parameter table. The spiboot.c file and spiboot.cmd demonstrates the placement of the DDR3 configuration table.
Let us know if you have any further questions with this issue.
Regards,
Rahul
Hi, Rahul
We try to modified our working dummy project with DDR config according to the example you attached. And after one day's try, we seem to get more understandings of how to config DDR using the DDR EMIF table. Somehow, we have some new question. We hope you can give us some help.
1)Here is part of "spiboot.map" file from your attached file.
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
DDR_CFG 008ffd20 00000180 00000178 00000008 RWIX
L2MAGIC 008ffffc 00000004 00000000 00000004 RWIX
DDR 80000000 00002000 00000c5c 000013a4 RWIX
Do we need to modified the DDR_CONFIG origin address? We are using C6670. According to the <SPRUGY5B> Table 2-2, the DDR configuration table should be put in (0x8fffff - 0xd23f +0x740) = 0x8f3500.
2)Here is part of "spiboot.c" file from your attached file.
#pragma DATA_SECTION (emif4Cfg, ".emif4Cfg")
const BOOT_EMIF4_TBL_T emif4Cfg = {
BOOT_EMIF4_ENABLE_MSW_pllCtl | \
BOOT_EMIF4_ENABLE_MSW_sdRamTiming1 | \
BOOT_EMIF4_ENABLE_MSW_sdRamTiming2 | \
BOOT_EMIF4_ENABLE_MSW_sdRamTiming3 | \
BOOT_EMIF4_ENABLE_MSW_ddrPhyCtl1 | \
BOOT_EMIF4_ENABLE_MSW_sdRamRefreshCtl | \
BOOT_EMIF4_ENABLE_MSW_sdRamOutImpdedCalCfg | \
BOOT_EMIF4_ENABLE_MSW_sdRamConfig,
BOOT_EMIF_ENABLE_SLSW_config0 | \
BOOT_EMIF_ENABLE_SLSW_config6 | \
BOOT_EMIF_ENABLE_SLSW_config7 | \
BOOT_EMIF_ENABLE_SLSW_config8 | \
BOOT_EMIF_ENABLE_SLSW_config9 | \
BOOT_EMIF_ENABLE_SLSW_config10 | \
BOOT_EMIF_ENABLE_SLSW_config18 | \
BOOT_EMIF_ENABLE_SLSW_config19 | \
BOOT_EMIF_ENABLE_SLSW_config20 | \
BOOT_EMIF_ENABLE_SLSW_config22 | \
BOOT_EMIF_ENABLE_SLSW_config12 | \
BOOT_EMIF_ENABLE_SLSW_config23 | \
BOOT_EMIF_ENABLE_SLSW_config21, /* Config select slsw */
0, /* Config select lsw */
3, /* pllPrediv */
40, /* pllMult */
2, /* pllPostDiv */ --------------------------question 1>
0x62477AB2, /* sdRamConfig */
0, /* sdRamConfig2, dont care*/
0x0000144F, /* sdRamRefreshCtl */
0x1333780C, /* sdRamTiming1 */
0x30717FE3, /* sdRamTiming2 */
0x559F86AF, /* sdRamTiming3 */
0, /* lpDdrNvmTiming, dont care */
0, /* powerManageCtl, dont care */
0, /* iODFTTestLogic, dont care */
0, /* performCountCfg, dont care */
0, /* performCountMstRegSel, dont care */
0, /* readIdleCtl, dont care */
0, /* sysVbusmIntEnSet, dont care */
0x70074c1f, /* sdRamOutImpdedCalCfg, dont care */
0, /* tempAlterCfg, dont care */
0x0010010F, /* ddrPhyCtl1 */
0, /* ddrPhyCtl2, dont care */
0, /* priClassSvceMap, dont care */
0, /* mstId2ClsSvce1Map, dont care */
0, /* mstId2ClsSvce2Map, dont care */
0, /* eccCtl, dont care */
0, /* eccRange1, dont care */
0, /* eccRange2, dont care */
0, /* rdWrtExcThresh, dont care */
0x87A0047F, 0, 0, 0, 0, 0, 0x33, 0x3A,
0x2C, 0x2C, 0x21, 0, 0xAF00002, 0, 0, 0,
0, 0, 0xB7, 0xB1, 0xA4, 0xA4, 0x98, 0x200,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0 ----------------------question 2>
};
1>These three parts seem to take no effect, maybe I'm doing wrong, I hope you could point it out.
When I set this table to 0x8ffd20, we can test the DDR frequency is 66.667MHz whatever we changed these three parts, our input CLK is 66.667MHz.
When I set this table to 0x8f3500, we can test the DDR frequency is 10.08MHz whatever we changed these three parts, our input CLK is 10.08MHz.
This makes us so confuse to get further.
2>What do these 64 32-bit values mean? Do we have to modify these values from your attached?
3>We found some of the annotations in the "emif4cfg table" is with "dont care".Does it means these values can be anything and we don't have to care about them?
Looking forward to your reply cause your advice is very helpful.Thank you!
Karlphy
Hi, Rahul
With your help, we have work out the DDR configuration!Thank you! And now, we are facing the last step: Booting multicores. We hope that you can help us with an example or some advices. I have started a new post and I gave you veryfied answer on this post. Here is the new post link:
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/289371.aspx
Thank you!
Karlphy
Hi, Rahul
I follow this post instead of opening a new post because the question we met has some relationship with this post. I hope you don't mind.
We have finished booting the 4 cores, using a HelloWorld simple project. And we solved the address problem through changing the package and cmd file of the project.
When we boot our own project, we can go into main() funtion. But when the code allocate the DDR memory, a hint was shown: "[C66xx_0] ti.sysbios.heaps.HeapMem: line 307: out of memory: handle=0x10869318, size=1030464
xdc.runtime.Error.raise: terminating execution" We guess there is something wrong with the heap. The shown length is a bit larger than our definition. Something odd is that when we use the emulator to connect the DSP, it runs successfully and there is no error occured. Our gel file is similar to the 6670EVM gel file with some ddr configuration changes. We guess that there is something of the DDR config we have never noticed.
Here is part of "tiboot.h" file from you attached "7080.SPIboot_ddr.zip"
/*******************************************************************************
* Emif4 (DDR3) configuration table
*******************************************************************************/
typedef struct bootEmif4Tbl_s {
UINT32 configSelect_msw; /* Bit map defining which registers to set */
UINT32 configSelect_slsw; /* Bit map defining which registers to set */
UINT32 configSelect_lsw; /* Bit map defining which registers to set */
UINT32 pllPrediv; /* Values of all 0s will disable the pll */
UINT32 pllMult;
UINT32 pllPostDiv;
UINT32 sdRamConfig; /* Controlled by bit 1 of configSelect_msw */
UINT32 sdRamConfig2; /* Bit 2 */
UINT32 sdRamRefreshCtl; /* Bit 3 */
UINT32 sdRamTiming1; /* Bit 4 */
UINT32 sdRamTiming2; /* Bit 5 */
UINT32 sdRamTiming3; /* Bit 6 */
UINT32 lpDdrNvmTiming; /* Bit 7 */
UINT32 powerManageCtl; /* Bit 8 */
UINT32 iODFTTestLogic; /* Bit 9 */
UINT32 performCountCfg; /* Bit 10 */
UINT32 performCountMstRegSel; /* Bit 11 */
UINT32 readIdleCtl; /* Bit 12 */
UINT32 sysVbusmIntEnSet; /* Bit 13 */
UINT32 sdRamOutImpdedCalCfg; /* Bit 14 */
UINT32 tempAlterCfg; /* Bit 15 */
UINT32 ddrPhyCtl1; /* Bit 16 */
UINT32 ddrPhyCtl2; /* Bit 17 */
UINT32 priClassSvceMap; /* Bit 18 */
UINT32 mstId2ClsSvce1Map; /* Bit 19 */
UINT32 mstId2ClsSvce2Map; /* Bit 20 */
UINT32 eccCtl; /* Bit 21 */
UINT32 eccRange1; /* Bit 22 */
UINT32 eccRange2; /* Bit 23 */
UINT32 rdWrtExcThresh; /* Bit 24 */
UINT32 chipConfig[64];
} BOOT_EMIF4_TBL_T;
Here is part of "toboot.h" file from 6670 bootloader source code("C6670_pg10_bootloader.zip")
/*******************************************************************************
* Emif4 (DDR3) configuration table
*******************************************************************************/
typedef struct bootEmif4Tbl_s {
UINT32 configSelect; /* Bit map defining which registers to set */
UINT32 pllPrediv; /* Values of all 0s will disable the pll */
UINT32 pllMult;
UINT32 pllPostDiv;
UINT32 sdRamConfig;
UINT32 sdRamConfig2;
UINT32 sdRamRefreshCtl;
UINT32 sdRamTiming1;
UINT32 sdRamTiming2;
UINT32 sdRamTiming3;
UINT32 lpDdrNvmTiming;
UINT32 powerManageCtl;
UINT32 iODFTTestLogic;
UINT32 performCountCfg;
UINT32 performCountMstRegSel;
UINT32 readIdleCtl;
UINT32 sysVbusmIntEnSet;
UINT32 sdRamOutImpdedCalCfg;
UINT32 tempAlterCfg;
UINT32 ddrPhyCtl1;
UINT32 ddrPhyCtl2;
UINT32 priClassSvceMap;
UINT32 mstId2ClsSvce1Map;
UINT32 mstId2ClsSvce2Map;
UINT32 eccCtl;
UINT32 eccRange1;
UINT32 eccRange2;
UINT32 rdWrtExcThresh;
} BOOT_EMIF4_TBL_T;
We can see there are something different between the two parts. We are using the 6670 bootloader version and it worked till now(DDR can be read and written correctly). Our question is: Should we config the UINT32 chipConfig[64] . part of DDR? If so, how to config? If not, how can we solved this heap problem? We guess there is something wrong with this part because the gel file has do some part of config in UINT32 chipConfig[64] .
Another question: We know that before loading codes to L2 and DDR, we should config the PLL(using boot parameter table) and DDR(in this case, using emif4 config table). Is there anyting we should config before bootloading except for PLL and DDR? If so, how to do the conifg?
Waiting for your reply, it's urgent. Thank you for you patience.
Karlphy
Hi Rahul
As the last reply by Karlphy Fong , I dont think the exsample 7080.SPIboot_ddr.zip is for C6670.
Can you tell me how can I find the DDR_CONFIG address for C6670 and C6678? I can not find out the Table 2-2 in the last Bootloader User Guide (SPRUGY9C). Why is It removed?
Hi Karlphy,
Sorry for interrupting you.
Did you solve the DDR configuration problem?
I'm using C6670 and facing to the DDR configuration problem.
I made a DDR EMIF table as mentioned in this post, but DDR access is unstable.
Are there any additional setting for DDR3 during RBL boot?
I guess DDR3 Configuration Register need to be set during RBL boot,
but I don't know how to configurate the register.
If you have any information, can you please share with me?
best regards,
g.f.
YI Yin,
The DDR config table is being moved from bootloader user guide to the Data manual which is why it is removed. We plan to release the new data sheet soon which should reflect this change. In the mean time you can refer to the ROM code source provided here:
http://processors.wiki.ti.com/index.php/Keystone_Device_Architecture
Regards,
Rahul
PS: Please start a new thread when a thread is closed or verified as it is easier to track
Hi gf,
If you are configuring the DDR to max speed please try to reduce the DDR speed and then re-initialize the DDR from the application code after performing DDR leveling. Currently DDR leveling is not supported in the ROM.
Regards,
Rahul
Hi Rahul,
Thank you for the reply.
Okay, I will reduce the DDR3 speed.
By the way, I have question about re-initializing DDR3.
Do you mean that we need to allocate application code in internal RAM
for re-initializing DDR3?
best regards,
g.f.
HI Karlphy Fong and G.F,
Can you please share how you did DDR3 configuration. I am trying with above steps but I am unable to boot the board.
Thank You,
Nithin