Hello,
There are two types of C66x L2 configuration, 0 wait-states and 2 × 128-bit banks, 1 wait-state and 4 × 128-bit banks. Which one is C6657? I can't find the description in data manual.
Regards,
Kazu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kazu,
There are two types of C66x L2 configuration, 0 wait-states and 2 × 128-bit banks, 1 wait-state and 4 × 128-bit banks.
Please provide the document reference for the above statement.
The L2 memory configuration for the C6655/57 device is as follows:
• Total memory is 1024KB (C6655)
• Total memory is 2048KB (C6657)
As per corepac UG -L2SRAM:
The configuration features 3 wait states for L2SRAM, 8 x 128 bit banks which is made up of two physical banks with four sub-banks each.
Thank you.