This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm365 timer help



hi, all

im new to the timer. I want to use timers and generate 1KHz frequncy from GPIO pins like pwm Using timer IRQs form kernel space driver .

but the interrupt doesnot function and even the counter doesnot change. we are using dvsdk 4 with kernel linux-2.6.32.17-psp03.01.01.38

i have tried with 3timers but i get different value in the readonly register PID12 however:

LCD:PID12:0x0, EMUMGT 0x0                        timer 1

LCD:PID12:0x44722a0b, EMUMGT 0x0        timer 3

LCD:PID12:0x10701, EMUMGT 0x0               timer 4

does it make sense that all of them are different ? i have seen that PID12 is just for timer0,1,2,4. since timer0 is used for the system clock, and timer2 canonly used for WDT,so i can only use timer1,3,4. am i correct ?

here is the code snippets:

00132: struct lcd_dev lcd_devices = {

00133: .fpd = 1,

00134: .period = 100,

00135: .base = IO_ADDRESS(DAVINCI_TIMER3_BASE),

00136: .cmp_off = 0,

00137: .cmp_irq = 0,

00138: .bottom_irq = IRQ_DM365_TINT6, /* 15 INT6 timer 1:2*/

00139: .top_irq = 22, /* 22 INT7 timer 3:4 */

00140: };

 

00032: #define DAVINCI_TIMER1_BASE (0x1c21800)

00033: #define DAVINCI_TIMER3_BASE (0x1c20800)

00034: #define DAVINCI_TIMER4_BASE (0x1c23800)

00035:

00036: #define DAVINCI_ARM_INTC_IO_BASE (IO_ADDRESS(0x01C48000))

 

 

00038: /* Timer register offsets */

00039: #define PID12 0x0

00040: #define TIM12 0x10

00041: #define TIM34 0x14

00042: #define PRD12 0x18

00043: #define PRD34 0x1c

00044: #define TCR 0x20

00045: #define TGCR 0x24

00046: #define WDTCR 0x28

00047: #define INTCTL_STAT 0x44

//...

00401: /***************************************

00402: * init the Clock

00403: ***************************************/

00404: timer_clk = clk_get(NULL, "timer3");

00405: BUG_ON(IS_ERR(timer_clk));

00406: clk_enable(timer_clk);

00407:

00408: /***************************************

00409: * init the registers

00410: ***************************************/

00411: debug("PID12:0x%x, EMUMGT 0x%x\n", __raw_readl(lcd_devices .base + PID12), __raw_readl(

00411: lcd_devices .base + 4));

00412:

00413: /* Disabled, Internal clock source */

00414: __raw_writel(0, lcd_devices .base + TCR);

00415:

00416: /* reset both timers, no pre-scaler for timer34 */

00417: __raw_writel(0, lcd_devices .base + TGCR);

00418:

00419: /* Set both timers to unchained 32-bit */

00420: tgcr = TGCR_TIMMODE_32BIT_UNCHAINED << TGCR_TIMMODE_SHIFT;

00421: __raw_writel(tgcr, lcd_devices .base + TGCR);

00422:

00423: /* Unreset timers */

00424: tgcr |= (TGCR_UNRESET << TGCR_TIM12RS_SHIFT) | (TGCR_UNRESET << TGCR_TIM34RS_SHIFT);

00425: __raw_writel(tgcr, lcd_devices .base + TGCR);

00426:

00427: /* Init both counters to zero */

00428: __raw_writel(0, lcd_devices .base + TIM12);

00429: __raw_writel(0, lcd_devices .base + TIM34);

00430:

00431:

00432: /* period */

00433: __raw_writel(lcd_devices .period, lcd_devices .base + PRD12);

00434: /* first phase duration */

00435: __raw_writel(lcd_devices .fpd, lcd_devices .base + PRD34);

00436:

00437: /* only for time 34 : PSC34 = Prescaler : 1 : like no Prescaler */

00438: __raw_writel(1<<TGCR_PSC34_SHIFT, lcd_devices .base + TGCR);

00439:

00440: /***************************************

00441: * enable the timer

00442: ***************************************/

00443:

00444: /* ENAMODE12/ENAMODE34 = continuously */

00445: tgcr = TCR_ENAMODE_PERIODIC << 6;

00446: tgcr |= TCR_ENAMODE_PERIODIC << 22;

00447: __raw_writel(tgcr, lcd_devices .base + TCR); /* Enable it */

00448:

00449:

00450: /***************************************

00451: * init IRQs

00452: ***************************************/

00454: /* timer prescale counter */

00455: rv = request_irq(lcd_devices .top_irq, timer34_isr, IRQF_DISABLED, DEVICE_NAME, NULL);

00456: if(rv)

00457: {

00458: err("can't get assigned irq %i", lcd_devices .bottom_irq);

00459: goto dev_del;

00460: }

00461:

00462: /* timer counter */

00463: rv = request_irq(lcd_devices .bottom_irq, timer12_isr, IRQF_DISABLED, DEVICE_NAME, NULL);

00464: if(rv)

00465: {

00466: err("can't get assigned irq %i", lcd_devices .bottom_irq);

00467: goto dev_del;

00468: }

00469:

00470: /***************************************

00471: * enable the interrupt mask

00472: ***************************************/

00473: irq_enable(lcd_devices .top_irq);

00474: irq_enable(lcd_devices .bottom_irq);

00475:

00476: /***************************************

00477: * enable interrupt

00478: ***************************************/

00479: addr = lcd_devices .base + INTCTL_STAT;

00480: tgcr = __raw_readl(addr) | BIT(16) | BIT(0);

00481:

00482: __raw_writel(tgcr, addr);

 the code source file is here. 5758.lcd-11.09.16.10.21.10.rar

did i miss anything?

any help will be appreciated.

Thinks in advance.

regards, mike

 

 

  • i found some post here, said that:  "the changes i have made are setting  SUSPSRC reg for the timer0  ( though i am not yet sure that it was the prob )since my timer counter is not getting increamented". and the post said if use timer 4, you need set arm_intmux... but im using timer 3 now..

    i have checked the part 10 about SUSPSRC  reg but just found that the EMUMGT reg and i have also update it to free, see below. but the counter doesnot increament in my situation.(i canot found any other document about SUSPSRC  but the timer & wdt )

     __raw_writel(1, lcd_devices.base + EMUMGT); /* FREE: The timer runs free regardless of the SOFT bit */

    anothe helpfull post is here. (thinks, Jinh)


     ... any idea where is the problem ??

     

    regards, mike

  • Sorry .. Guys. my mistake.

    the problem is here :

    00437: /* only for time 34 : PSC34 = Prescaler : 1 : like no Prescaler */

    00438: __raw_writel(1<<TGCR_PSC34_SHIFT, lcd_devices .base + TGCR);

    -->

     tgcr|= 1<<TGCR_PSC34_SHIFT;
     __raw_writel(tgcr, lcd_devices.base + TGCR);

    regards, Mike