This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Som question about DM368 (Performance & Power Consumption)



Hi all

We use dm368 (arm clock 397Mhz, ddr 340Mhz for Digital Out)

Anybody sucess 30 FPS at 1080P (H.264 Encoding include capture) ?

My Result is about 29.5 FPS (not 30 fps)

I trun off video display & audio function.

and Addtional HDMI out(1080P30) , FPS is 22

(we try arm clock 432Mhz , ddr 340Mhz, it's same)

 

1, Can dm368  encoding 30fps include capture ?

 

We test power consumption by electric current

it's 220mA at boot

and it's 340mA 1080P encoding

and it's 420mA 1080P encoding & HDMI out

 

2. is it normal ? or something wrong ?

 

  • Hi,

    We have got 1080P30 with capture on DM368 IPNC Reference Design. When i say 30 fps, i am talking from overall system perspective (with capture and encoding). With streaming turned on, we are at margin and at times see a little under 30fps (29.8-30) system performance. In all the use cases, codec still performs above 30fps.

    Can you tell me whether you see 29.5 fps across VIDENC1_process function call or across the system level? Also, can you explain the DDR accesses in your capture flow? As you mentioned, changing ARM form 399 to 432 MHz did not improve codec performance, this adds to our theory that it is DDR that is causing the issue. So please help us understand your DDR accesses and any other DMA accesses that you are doing?

    For power numbers, i will get back to you with more details.

    Regards,

    Anshuman

  • thank you Anshuman

    More information is here

    a. Video Encoding Path

        ISIF -> Resize A (1920x1080) -> YUV420 -> H.264 Encoding (8000 Kbps)

                     Resize B(352x240) -> YUV420 (not encoding, no more process)

                     (not use AEWB, Motion Detection, Not streaming)

    b. Audio Path

       Audio External Codec -> I2S -> MBCSP -> Audio Codec(AAC or G..711)

    c. Video Out Path (PreView)

      DMA Copy To Video Outbuffer -> Digital (YCbCr16) -> HDMI Trans

     

    I just turn on A(Video Encoding Path, Other not used) -> 29.6~29.8 FPS (System Performance 29.6, Encoding 29.8)

     

    More detail power information is here

    DM368 36Mzh Xtal , Arm Core:371Mhz, DDR:680Mhz(340Mhz)

    a. 1080P Encoding  video output

         DM368(1.35V):568mA

         DM368(1.8V) + DDR(1.8V):295mA

     

    b. 1080P Encoding

         DM368(1.35V):575mA

         DM368(1.8V) + DDR(1.8V):228mA

     

    c. 720P Encoding  video output

          DM368(1.35V):472mA

         DM368(1.8V) + DDR(1.8V):240mA

     

    d. 720P Encoding

          DM368(1.35V):435mA

         DM368(1.8V) + DDR(1.8V):150mA


  • Sungil,

    The power numbers that were measured look reasonable.  They are in the range of power consumption that I expect for DM368.

    Regards,

    -phil

  • Hi,

    In the below encoding path, you have enabled RSZ B. What is it intended for? We do not add any extra resize option in our capture flow. I think if you disable RSZB, then i am sure you should be able to comfortably get encode performance of above 30 fps and system performance around 30fps.

    Sungil Kim said:

    a. Video Encoding Path

        ISIF -> Resize A (1920x1080) -> YUV420 -> H.264 Encoding (8000 Kbps)

                     Resize B(352x240) -> YUV420 (not encoding, no more process)

                     (not use AEWB, Motion Detection, Not streaming)

    The RSZB output to DDR is unnecessary DDR bandwidth consumption.

    For your display path, we have not evaluated how much would be the impact of extra DDR on codec, but i assume that the performance numbers you are seeing are reasonable. You are adding 1920x1080x1.5x30x3 Bytes/sec DDR read and write operations, which surely is a huge DDR load.

    Regards,

    Anshuman

    PS: Please mark this post as verified if you think it has answered your question. Thanks.

     

  • I've tried speeding up our DM368 to run the DDR at 340MHz but the board locks when UBL loads the PLL and DDR parameters.  I feel that it's the DDR parameters that are at fault.  Could you post the DDR setup code in your UBL?

    Thanks,

    John A

  • Hi John

     

    Here is  our code

     

    Uint32 DEVICE_DDR2Init()
    {
        DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);

        SYSTEM->VTPIOCR = (SYSTEM->VTPIOCR) & 0xFFFF9F3F;

        // Set bit CLRZ (bit 13)
        SYSTEM->VTPIOCR = (SYSTEM->VTPIOCR) | 0x00002000;

        // Check VTP READY Status
        while( !(SYSTEM->VTPIOCR & 0x8000));    

        // Set bit VTP_IOPWRDWN bit 14 for DDR input buffers)
        //SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00004000;        

        // Set bit LOCK(bit7) and PWRSAVE (bit8)
        SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00000080;    

        // Powerdown VTP as it is locked (bit 6)
        // Set bit VTP_IOPWRDWN bit 14 for DDR input buffers)
        SYSTEM->VTPIOCR = SYSTEM->VTPIOCR | 0x00004040;

        // Wait for calibration to complete
        UTIL_waitLoop( 150 );

        // Set the DDR2 to synreset, then enable it again
        DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_SYNCRESET);
        DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);

        DDR->DDRPHYCR = 0x000000C6;

        DDR->SDBCR = 0x00D34A32;        //Program SDRAM Bank Config Register
        DDR->SDBCR = 0x0053CA32;

        DDR->SDTIMR  =0x576D7D12;         //Program SDRAM Timing Control Register1
        DDR->SDTIMR2 =0x422EC742;         //Program SDRAM Timing Control Register2

        DDR->PBBPR = 0x000000FE;

        DDR->SDBCR = 0x08534832;         //Program SDRAM Bank Config Register

        DDR->SDRCR = 0xA5C;            //Program SDRAM Refresh Control Register     

        DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_SYNCRESET);
        DEVICE_LPSCTransition(LPSC_DDR2,0,PSC_ENABLE);

        return E_PASS;
    }

     

    good luck

  • Thanks Sungil,

    I did find some code for running the DDR at 340MHZ and got it working.  It's very close to what you posted. One thing that's interesting is the code for setting the SDBCR (SDCR in the documentation) is setting a reserved bit to 1 for apparently no reason.

    So while your code shows...

    DDR->SDBCR = 0x00D34A32

    The code supplied would be...

    DDR->SDBCR = 0x08D34A32

    John A