Dear All,
I have ran the demo application dvsdk/encodedecode successfully before I changed the kernel for IPNC of Appro.
There is error if I run the encodedecode in EVM. I guess the error becasue of the wrong capture device be selected.
Where is the document to describe the capture device setup for DM365? Or could someone tell me the advice for understanding the capture device setting?
How let demo AP to run?
root@192.168.3.106:/opt/dvsdk/dm365# ./encodedecode
Encodedecode demo started.
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 736,
layer.pix_fmt.width = 720,
layer.pix_fmt.height = 480,
layer.pix_fmt.sizeimage =529920
DavinciDisplay DavinciDisplay.1: pixfmt->width = 720,
layer->layer_info.config.line_length= 736
davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:0:1:108
davinci_previewer davinci_previewer.2: ipipe_set_preview_config
davinci_previewer davinci_previewer.2: ipipe_set_preview_config
vpfe ccdc capture vpfe ccdc capture.1: IMP chained
vpfe ccdc capture vpfe ccdc capture.1: Resizer present
vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 480, bpp = 1
vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 480, bpp = 1
IRQ handler type mismatch for IRQ 0
vpfe ccdc capture vpfe ccdc capture.1: Error in requesting VINT0 <3>vpfe ccdc capture vpfe ccdc capture.1: Error in attaching interrupt handle
Trying to free already-free IRQ 0
Error: Failed to create capture device
Process one buffer to figure out buffer requirements
my bootarg=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.3.220:/home/person/workdir/filesys,nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4
Best Regards,
Person