Hi,
The version of DVSDK is 4.0 and the H.264 encoder is 02_10_00_06.
I created two instances of H.264 encoder. One is for CIF input and another is for D1 input.
At about 50% channce the encoder will hangup in VIDENC1_process. During hang up, with the ps command:
ps H -eo user,pid,ppid,tid,time,%cpu,cmd,wchan
I got:
root 1478 1447 1481 00:00:01 7.8 ./elss down_interruptible
The 1481 is the thread no. of the CIF encoder. So it seems the encoder is waiting for an interrupt?
I can't reproduce this problem when only one encoder instance is used.
Edit: attached the log file with CE_DEBUG=3
Regards,
lcj