This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel boot issue on DM814x EVM



Hello,

I'm using EZSDK DM814x 5.02.02.60 and DM814x EVM with 512MB memory.

I modified the memory map as given in http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_Map_For_512MB_Board wiki page.

Bootargs I'm using is: console=ttyO0,115200n8 rootwait rw mem=176M earlyprintk notifyk.vpssm3_sva=0x9F900000 vram=50M ti814xfb.vram=0:16M,1:16M,2:6M root=/dev/
nfs nfsroot=10.10.38.39:/home/admin1/targetfs/ ip=dhcp

When I boot the system , kernel hangs after some time. Please see the boot log

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (root@admin1-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #6 Mon Oct 17 16:50:33 IST 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
bootconsole [earlycon0] enabled
vram size = 52428800 at 0
reserved size = 52428800 at 0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 1.0
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 31904
Kernel command line: console=ttyO0,115200n8 rootwait rw mem=176M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.vram=0:16M,1:16M,2:6M root=/dev/
nfs nfsroot=10.10.38.39:/home/admin1/targetfs/ ip=dhcp
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 126MB = 126MB total
Memory: 122228k/122228k available, 57996k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xcb800000 - 0xf8000000   ( 712 MB)
    lowmem  : 0xc0000000 - 0xcb000000   ( 176 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .init : 0xc0008000 - 0xc0037000   ( 188 kB)
      .text : 0xc0037000 - 0xc04a6000   (4540 kB)
      .data : 0xc04a6000 - 0xc04e9400   ( 269 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy: 
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
registered ti814x_vpss device
registered TI814x on-chip HDMI device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
pcf857x: probe of 1-0021 failed with error -121
i2c i2c-1: Failed to register i2c client PCF_8575 at 0x21 (-16)
i2c i2c-1: Can't create device at 0x21
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at cb80c000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at cb81e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 238
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst 
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffd
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
qt602240_ts 1-004a: __qt602240_read_reg: i2c transfer failed
qt602240_ts: probe of 1-004a failed with error -5
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbf900000
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
  #0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Detected MACID=0:0:0:0:0:0
ata1: SATA link down (SStatus 0 SControl 300)
mmc0: new SD card at address e624
mmcblk0: mmc0:e624 SD01G 968 MiB 
 mmcblk0: p1 p2

CPSW phy found : id is : 0x282f014
Sending DHCP requests .
PHY: 0:01 - Link is Up - 100/Full
....., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 10.10.38.57
IP-Config: Complete:
     device=eth0, addr=10.10.38.57, mask=255.255.255.0, gw=10.10.38.1,
     host=10.10.38.57, domain=kpit.com, nis-domain=(none),
     bootserver=0.0.0.0, rootserver=10.10.38.39, rootpath=
VFS: Mounted root (nfs filesystem) on device 0:14.
devtmpfs: mounted
Freeing init memory: 188K
INIT: version 2.86 booting
Error opening /dev/fb0: No such file or directory
Please wait: booting...
Starting udev
udevd (78): /proc/78/oom_adj is deprecated, please use /proc/78/oom_score_adj instead.
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
EXT3-fs (mmcblk0): error: can't find ext3 filesystem on dev mmcblk0.
EXT2-fs (mmcblk0): error: can't find an ext2 filesystem on dev mmcblk0.
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
ISOFS: Unable to identify CD-ROM format.
EXT3-fs: barriers not enabled
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
Root filesystem already rw, not remounting
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
NOT configuring network interfaces: / is an NFS mount
hwclock: can't open '/dev/misc/rtc': No such file or directory
Thu Sep  8 17:37:00 UTC 2011
hwclock: can't open '/dev/misc/rtc': No such file or directory
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
        PRCM for IVHD0 is in Progress, Please wait.....  
                        BW Phy Addr : 0x48180600 Data : 0x00000002
                        AW Phy Addr : 0x48180600 Data : 0x00000002
                        Phy Addr : 0x48180c04 Data : 0x00000037
                        BW Phy Addr : 0x48180620 Data : 0x00070000
                        AW Phy Addr : 0x48180620 Data : 0x00070002
                        BW Phy Addr : 0x48180624 Data : 0x00030000
                        AW Phy Addr : 0x48180624 Data : 0x00010002
                        Phy Addr : 0x48180600 Data : 0x00000102
                        BW Phy Addr : 0x48180c10 Data : 0x00000007
                        AW Phy Addr : 0x48180c10 Data : 0x00000003
                        Phy Addr : 0x48180c14 Data : 0x00000004
                        BW Phy Addr : 0x58088000 Data : 0x7f5adc32
                        AW Phy Addr : 0x58088000 Data : 0xeafffffe
                        BW Phy Addr : 0x58098000 Data : 0x0cceba81
                        AW Phy Addr : 0x58098000 Data : 0xeafffffe
                        BW Phy Addr : 0x48180c10 Data : 0x00000003
                        AW Phy Addr : 0x48180c10 Data : 0x00000000
                        Phy Addr : 0x48180c14 Data : 0x00000007
        PRCM for IVHD0 is Done Successfully  
PRCM Initialization completed 
FATAL: Module syslink not found.
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1
OsalDrv driver open: /dev/syslinkipc_Osal: No such file or directory
OsalDrv driver close: /dev/syslinkipc_Osal: Bad file descriptor
/dev/syslinkipc_MultiProc: No such file or directory
MultiProc driver close: : Bad file descriptor
SharedRegion driver open: : No such file or directory
SharedRegion driver close: : Bad file descriptor
/dev/syslinkipc_GateMP: No such file or directory
/dev/syslinkipc_MessageQ: No such file or directory
MessageQ driver close: : Bad file descriptor
Notify driver open: /dev/syslinkipc_Notify: No such file or directory
Notify driver close: /dev/syslinkipc_Notify: Bad file descriptor
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
/dev/syslinkipc_HeapBufMP: No such file or directory
/dev/syslinkipc_HeapMemMP: No such file or directory
/dev/syslinkipc_ListMP: No such file or directory
/dev/syslinkipc_RingIO: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_RingIOShm: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_ClientNotifyMgr: No such file or directory
ClientNotifyMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQBufMgr: No such file or directory
FrameQBufMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQ: No such file or directory
FrameQ driver close: : Bad file descriptor
/dev/syslinkipc_Ipc: No such file or directory
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
FIRMWARE: Could not open ProcMgr: ProcMgr status 0xfffffff8
Starting telnet daemon.
Loading HDVPSS Firmware
FATAL: Module syslink not found.
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1
OsalDrv driver open: /dev/syslinkipc_Osal: No such file or directory
OsalDrv driver close: /dev/syslinkipc_Osal: Bad file descriptor
/dev/syslinkipc_MultiProc: No such file or directory
MultiProc driver close: : Bad file descriptor
SharedRegion driver open: : No such file or directory
SharedRegion driver close: : Bad file descriptor
/dev/syslinkipc_GateMP: No such file or directory
/dev/syslinkipc_MessageQ: No such file or directory
MessageQ driver close: : Bad file descriptor
Notify driver open: /dev/syslinkipc_Notify: No such file or directory
Notify driver close: /dev/syslinkipc_Notify: Bad file descriptor
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
/dev/syslinkipc_HeapBufMP: No such file or directory
/dev/syslinkipc_HeapMemMP: No such file or directory
/dev/syslinkipc_ListMP: No such file or directory
/dev/syslinkipc_RingIO: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_RingIOShm: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_ClientNotifyMgr: No such file or directory
ClientNotifyMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQBufMgr: No such file or directory
FrameQBufMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQ: No such file or directory
FrameQ driver close: : Bad file descriptor
/dev/syslinkipc_Ipc: No such file or directory
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
FIRMWARE: Could not open ProcMgr: ProcMgr status 0xfffffff8
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
ti81xxfb ti81xxfb: no grpxs
ti81xxfb: probe of ti81xxfb failed with error -22
Configuring fb0 to LCD
/etc/init.d/rc: /etc/rc5.d/S15load-hdvpss-firmware.sh: line 60: can't create /sys/devices/platform/vpss/graphics0/nodes: nonexistent directory
/etc/init.d/rc: /etc/rc5.d/S15load-hdvpss-firmware.sh: line 60: can't create /sys/devices/platform/vpss/display1/enabled: nonexistent directory
/etc/init.d/rc: /etc/rc5.d/S15load-hdvpss-firmware.sh: line 60: can't create /sys/devices/platform/vpss/display1/timings: nonexistent directory
/etc/init.d/rc: /etc/rc5.d/S15load-hdvpss-firmware.sh: line 60: can't create /sys/devices/platform/vpss/display1/output: nonexistent directory
/etc/init.d/rc: /etc/rc5.d/S15load-hdvpss-firmware.sh: line 60: can't create /sys/devices/platform/vpss/display1/enabled: nonexistent directory
open /dev/fb0: No such file or directory
open /dev/fb0: No such file or directory
cat: write error: No space left on device
cat: write error: No space left on device


.

Please let me know if need to add/modify some settings.

 

Regards,

Mitul

  • Hi Mitul,

    FATAL: Module syslink not found.

    I see this error in the boot log. Is the filesystem correctly setup? On the EZSDK filesystem, syslink should be under /lib/modules
  • Hi Siddharth,

    syslink module is present at "/lib/modules/2.6.37/kernel/drivers/dsp/" location in filesystem. So modprobe should find this module. Any idea why modprobe can't find syslink? I checked /etc/modprobe.conf and /etc/modprobe.d files, but all configurations looks okay.

    Anyway, I replaced "modprobe syslink" with "insmod /lib/modules/2.6.37/kernel/drivers/dsp/syslink.ko". So now the kernel boot is working fine.

    Regards,

    Mitul

  • I've had similiar modprobe problems with minix and ipv6. I had to run "depmod -a" on the target. Of course to do that, the target has to boot up to the console login. Init scripts that fail on modprobe will prvent getting that far. Never did figure out how to do a "depmod -a" while the target filesystem is mounted on the host.

     

  • Thanks Norman. "dempod -a" worked for me.

    I removed those startup scripts to boot the kernel & once kernel is up I ran "depmode -a". This updated modules.dep file on my file-system. So after this modprobe works & kernel boots properly with all scripts restored.

  • I've been running into the same exact problems described here (and a few other threads) with the EZSDK 5.03.01.15.

    I simply tried to rebuild the kernel with inotify support, and then wound up with the error about an invalid syslink.ko.  At that point, attempting to run 'make linux_install syslink syslink_install' from the top level EZSDK directory resulted in a bunch of broken moddep files, and an error about the syslink kernel module not being found.

    Has anyone figured out a procedure by which you can update the kernel and rootfs without ever needing to boot the target and run depmod? While this does seem to work, I'd prefer something that I could use when preparing rootfs images for mass programming.

    Thanks!

  • Looks like Hiroto Shibuya has a solution in his thread here:

    http://e2e.ti.com/support/embedded/linux/f/354/t/54366.aspx

    He uses the Arago toolchain. Don't know it the same tool is available with the CodeSourcery toolchain. I should probably switch as CodeSourcery is now owned by Mentor and they data-mine you to download the free version. Maybe on the next project.

  • Hi,

    a simple "depmod -b /path/to/your/targetfs 2.6.37 -v" does it.

  • /sbin/depmod -b /path/to/your/targetfs/ -v 2.6.37

    did it for me - but it is frustrating to see what TI is offering here as official SDK at all. If you are going to rebuild linux (make linux and make linux_install) you are running into those troubles as even make cmem / make cmem_install and make syslink / make syslink_instal won't update the targetfs module dependencies. TI could have fixed this by just inserting a depmod -a as early as possible in their startup scripts...or even by integrating the above command in their make install?

  • There is a "depmod -ae" in TI's udev script - but it only runs when modules.dep is missing.  So another half-baked manual fix is to delete the modules.dep in the targetfs area during installation, and letting the udev start script regenerate the modules.dep on the next reboot.

    Of course, depmod complains because -e needs -E or -F - but it still runs.

  • My solution was to rebuild everything step-by-step according to the DM816x EZ Software Developers Guide:

    source $EZSDK/linux-devkit/environment-setup

    cd $EZSDK

    make clean

    make components

    make all

    make install

    Then modify the kernel:

    cd board-support/linux-2.6.37-psp04.04.00.01/

    make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_evm_defconfig

    make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm menuconfig

    make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm uImage

    REMAKE the module

    make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm modules

    sudo cp -r ${HOME}/targetfs/home/root/dm816x-evm/lib/modules ${HOME}/targetfs/lib

    etc...