This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding Two DEI Components in DM8148

Hi Vimal,

I am working on DM8148EVM .I am using EZSDK 5_03_01_15 .I have got a few questions regarding creating two DEI  component instances .

1 . Can I create two DEI component instances  in DM8148 ?

2.  Can I connect output of one DEI component to the input of another DEI Component ?

3.  In the omx_vfpc.h ,there are two DEI components OMX.TI.VPSSM3.VFPC.DEIMDUALOUT(DEI-M) and OMX.TI.VPSSM3.VFPC.DEIHDUALOUT (DEI-H)

       Can i Connect  DEI-M to DEI-H on DM8148 without any problem ?

4. If i create two DEI-M component instances on DM8148 and connect the output of one DEI component to another ,will there be a performance issue ?since one DEI hardware block has to manage two DEI-M componenet instances and process the data serially  .

Can you please help me out in the understanding the above problem clearly .any help is appreciated .

Thanks,

N Sivaramkrishna .