This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 about IPIPE、IPIPEIF and ISIF mode input size

Genius 3400 points


Hi,all!
DM8127 run ipnc2.8 in the lowpower M2M mode,the camera outputs H264(5M)+D1+MJPEG(5M).
About RSZE、IPIPEIF and ISIF mode input size,we have three questions.

1、In the issdrv_ispApi.c file Iss_ispControl() function.

Set rszA and rezB input size,the code are as folloes:

rszASetOutConfig(pRszCfg->inWidth - 2,pRszCfg->inHeight - 4,pRszCfg->outWidth0,pRszCfg->outHeight0);
rszBSetOutConfig(pRszCfg->inWidth - 2,pRszCfg->inHeight - 4,pRszCfg->outWidth0,pRszCfg->outHeight0);

Q1: Why the input size are inWidth-2 and inHeight-4 ?
     When we set input size are inWidth and inHeight,the camera can not output streams.
     When we set input size are smaller than inWidth-2 and inHeight-4,the camera can output streams, and the streams become smaller.

2、In the issdrv_ispApi.c file Iss_ispControl() function.

Set ipipeif PPLN and LPFR,the code are as folloes:

Iss_ispWriteReg(&ipipeif_reg->PPLN,((pRszCfg->inWidth + 16) - 1),0,13);
Iss_ispWriteReg(&ipipeif_reg->LPFR,((pRszCfg->inHeight + 16) - 1),0,13);

Q2: Why the PPLN and LPFR are (inWidth + 16)-1 and (inHeight + 16)-1? Is it because the follow said:

But when we set PPLN = inWidth + 10 and LPFR = inHeight + 10,the camera can output streams.

3、In the issdrv_captureApi.c file Iss_captCreate() function.

Set isif regesiter, the code are as follows:

if (pObj->createArgs.scParams[0].inHeight == 1920)
{
    isif_reg->HDW = 2577;
    isif_reg->VDW = 1923;
    isif_reg->PPLN = 2577;
    isif_reg->LPFR = 3847;
    isif_reg->LNH = 2563;
    isif_reg->LNV = 1921;
}

Q3: Why are these value? The value must be these?

But when we modify the value are as follows,the camera can also output streams.
isif_reg->HDW = 2563;
isif_reg->VDW = 1921;
isif_reg->PPLN = 2563;
isif_reg->LPFR = 3843;
isif_reg->LNH = 2559;
isif_reg->LNV = 1919;

Thanks a lot!