Hi ,
For DM81XX the USB MMC's power control issue.Please help confirm, thank you
1.Why EVM Board schematic for USB-side and MMC-side power switch not the same? can use the same?ex:TPS2065DR
2. if the MMC1_POW not in use, direct floating it?
3.mmc port if only used to store images, and do not use to boot, it is suggest which port?