This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet port 1 in MII mode in DM8107

Other Parts Discussed in Thread: DM8107

Hi All,

We are using Ethernet port 1 in MII mode in DM8107.We are using LAN8700 PHY.

we have take UDWORKS DM8107 as reference design.(only we use MII mode while in UDWORKS board its RMII)

We have done changes in u-boot but unable ping.

We have done below changes for it.

1)Pin Mux Setting in PINCNTL register(reg:PAD204, PAD219, PAD220, PAD221, PAD222, PAD227, PAD205, PAD206,PAD207, PAD208,PAD209, PAD210,PAD211, PAD212)

2)GMII_SEL=0x00

when i ping from u-boot

]ping 192.168.102.55

link up on port1, speed 100, full duplex

ping failed: 192.168.102.55 not alive

Is any other setting require other than pin mux and GMII_SEL

Regards,

Bharat Gohil