Hi All,
> We have two different hardware boards for TI netra processor.
>
> 1) Spectrum Digital EVM HW Rev F.
> 2) UDWORKS RDK HW Rev 0.5
>
> These two boards have direct SATA ports from DM8168. On EVM there are
> two direct SATA ports and RDK have one direct SATA port.
>
> We have Seagate harddisk which is not detected on SATA ports which is
> directly connected to Netra DM8168. RDK have one SATA multiplier from
> silicon image have four SATA ports.
>
> Seagate harddisk which is not detected on direct port of Netra DM8168
> but this same harddisk is detected on all the four ports of SATA
> multiplier form silicon image.
>
> So we don’t understand why it is so?
>
> Any harddisk should detect on direct SATA port.
Regards,
Bharat Gohil