This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omaplfb won't load

I've been trying to install the Graphics SDK (4.05.00.01) on a Z3 DM8168 board.

After installing to the target file system I run "rc.pvr start" and the response is "Loaded PowerVR consumer services" which seems correct.

However, if I run lsmod, the omaplfb module has not been loaded. Here is the output ...

root@arago:/etc/init.d# lsmod
Module                  Size  Used by    Not tainted
pvrsrvkm              155098  0
ti81xxhdmi             14478  0
ti81xxfb               21771  0
vpss                   72346  2 ti81xxhdmi,ti81xxfb
ipv6                  209855 10
syslink              1108763  0

If I then try and manually load omaplfb, I get the following output ...

root@arago:/etc/init.d# insmod /lib/modules/2.6.37/kernel/drivers/char/omaplfb.ko
insmod: can't insert '/lib/modules/2.6.37/kernel/drivers/char/omaplfb.ko': Invalid argument

I built the Graphics SDK according the instructions and everything seemed to build correctly.

I wonder if anyone has seen the problem and knows what is the solution?

Thx, Steve