This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 alsa underrun problem



We are using DM8168 board with EzSDK software.

We are seeing random underruns on alsa playback although we are providing more than enough PCM samples to the playback device (always filled with more than a second's worth of data).

We found the following known issue mentioned in EZSDK 5.05 release notes 

SDOCM00096174 - snd_pcm_avail() returns a negative number of available words due to
non-sequential value read by edma_get_position()


It seems we are seeing this very issue on our boards.

Is there any work around for this problem? Is the fix available through some patch?


Thanks

George

  • I believe that I am also seeing this problem.  We have an application which is running at the highest priority.  I have code which checks to see how often audio data is written to the playback device.  I never see time between writes much larger than the period time (period time is 10ms and the wait time varies between 9.997ms to 10.067 ms).  I can see that audio data is buffered out to the playback device at all times, yet now and again between 4 to 10 minutes I will see an XRUN.  The XRUN never corresponds to any large delay or reduced amount of data in the audio stream.

    I have changed our driver to use EVENTQ_0 and a fifo size of 32.  This seems to have reduced the frequency of XRUNs, but I still see them now and again.

    Is there any solution to this?

  • We fixed the problem by modifying davinci-pcm.c to not use edma_get_position. The modified code is attached. There are some unrelated changes also in this code, you can pick the relevant changes. (added a new variable offset in in struct davinci_runtime_data to keep track of dma position)

    /*
     * ALSA PCM interface for the TI DAVINCI processor
     *
     * Author:      Vladimir Barinov, <vbarinov@embeddedalley.com>
     * Copyright:   (C) 2007 MontaVista Software, Inc., <source@mvista.com>
     * added SRAM ping/pong (C) 2008 Troy Kisky <troy.kisky@boundarydevices.com>
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    #include <linux/module.h>
    #include <linux/init.h>
    #include <linux/platform_device.h>
    #include <linux/slab.h>
    #include <linux/dma-mapping.h>
    #include <linux/kernel.h>
    
    #include <sound/core.h>
    #include <sound/pcm.h>
    #include <sound/pcm_params.h>
    #include <sound/soc.h>
    
    #include <asm/dma.h>
    
    #ifndef CONFIG_ARCH_TI81XX
    #include <mach/edma.h>
    #include <mach/sram.h>
    #else
    #include <asm/hardware/edma.h>
    #endif
    
    
    #include "davinci-pcm.h"
    
    #define AMAGI_DEBUG 1
    #ifdef AMAGI_DEBUG
    
    #define DEBUG 1
    static int print_edma_flag = 0;
    
    #endif //AMAGI_DEBUG
    
    #ifdef DEBUG
    static void print_buf_info(int slot, char *name)
    {
    	struct edmacc_param p;
    	if (slot < 0)
    		return;
    	edma_read_slot(slot, &p);
    	printk(KERN_DEBUG "%s: 0x%x, opt=%x, src=%x, a_b_cnt=%x dst=%x\n",
    			name, slot, p.opt, p.src, p.a_b_cnt, p.dst);
    	printk(KERN_DEBUG "    src_dst_bidx=%x link_bcntrld=%x src_dst_cidx=%x ccnt=%x\n",
    			p.src_dst_bidx, p.link_bcntrld, p.src_dst_cidx, p.ccnt);
    }
    #else
    static void print_buf_info(int slot, char *name)
    {
    }
    #endif
    
    static struct snd_pcm_hardware pcm_hardware_playback = {
    	.info = (SNDRV_PCM_INFO_INTERLEAVED | SNDRV_PCM_INFO_BLOCK_TRANSFER |
    		 SNDRV_PCM_INFO_MMAP | SNDRV_PCM_INFO_MMAP_VALID |
    		 SNDRV_PCM_INFO_PAUSE | SNDRV_PCM_INFO_RESUME),
    	.formats = (SNDRV_PCM_FMTBIT_S16_LE),
    	.rates = (SNDRV_PCM_RATE_8000 | SNDRV_PCM_RATE_16000 |
    		  SNDRV_PCM_RATE_22050 | SNDRV_PCM_RATE_32000 |
    		  SNDRV_PCM_RATE_44100 | SNDRV_PCM_RATE_48000 |
    		  SNDRV_PCM_RATE_88200 | SNDRV_PCM_RATE_96000 |
    		  SNDRV_PCM_RATE_KNOT),
    	.rate_min = 8000,
    	.rate_max = 96000,
    	.channels_min = 2,
    	.channels_max = 2,
    	.buffer_bytes_max = 2 * 1024 * 1024,
    	.period_bytes_min = 32,
    	.period_bytes_max = 8 * 1024,
    	.periods_min = 16,
    	.periods_max = 4096,
    	.fifo_size = 0,
    };
    
    static struct snd_pcm_hardware pcm_hardware_capture = {
    	.info = (SNDRV_PCM_INFO_INTERLEAVED | SNDRV_PCM_INFO_BLOCK_TRANSFER |
    		 SNDRV_PCM_INFO_MMAP | SNDRV_PCM_INFO_MMAP_VALID |
    		 SNDRV_PCM_INFO_PAUSE),
    	.formats = (SNDRV_PCM_FMTBIT_S16_LE),
    	.rates = (SNDRV_PCM_RATE_8000 | SNDRV_PCM_RATE_16000 |
    		  SNDRV_PCM_RATE_22050 | SNDRV_PCM_RATE_32000 |
    		  SNDRV_PCM_RATE_44100 | SNDRV_PCM_RATE_48000 |
    		  SNDRV_PCM_RATE_88200 | SNDRV_PCM_RATE_96000 |
    		  SNDRV_PCM_RATE_KNOT),
    	.rate_min = 8000,
    	.rate_max = 96000,
    	.channels_min = 2,
    	.channels_max = 8,
    	.buffer_bytes_max = 2 * 1024 * 1024,
    	.period_bytes_min = 32,
    	.period_bytes_max = 8 * 1024,
    	.periods_min = 16,
    	.periods_max = 2048,
    	.fifo_size = 0,
    };
    
    /*
     * How ping/pong works....
     *
     * Playback:
     * ram_params - copys 2*ping_size from start of SDRAM to iram,
     * 	links to ram_link2
     * ram_link2 - copys rest of SDRAM to iram in ping_size units,
     * 	links to ram_link
     * ram_link - copys entire SDRAM to iram in ping_size uints,
     * 	links to self
     *
     * asp_params - same as asp_link[0]
     * asp_link[0] - copys from lower half of iram to asp port
     * 	links to asp_link[1], triggers iram copy event on completion
     * asp_link[1] - copys from upper half of iram to asp port
     * 	links to asp_link[0], triggers iram copy event on completion
     * 	triggers interrupt only needed to let upper SOC levels update position
     * 	in stream on completion
     *
     * When playback is started:
     * 	ram_params started
     * 	asp_params started
     *
     * Capture:
     * ram_params - same as ram_link,
     * 	links to ram_link
     * ram_link - same as playback
     * 	links to self
     *
     * asp_params - same as playback
     * asp_link[0] - same as playback
     * asp_link[1] - same as playback
     *
     * When capture is started:
     * 	asp_params started
     */
    struct davinci_runtime_data {
    	spinlock_t lock;
    	int period;		/* current DMA period */
        unsigned int offset;
    	int asp_channel;	/* Master DMA channel */
    	int asp_link[2];	/* asp parameter link channel, ping/pong */
    	struct davinci_pcm_dma_params *params;	/* DMA params */
    	int ram_channel;
    	int ram_link;
    	int ram_link2;
    	struct edmacc_param asp_params;
    	struct edmacc_param ram_params;
    };
    
    /*
     * Not used with ping/pong
     */
    static void davinci_pcm_enqueue_dma(struct snd_pcm_substream *substream)
    {
    	struct davinci_runtime_data *prtd = substream->runtime->private_data;
    	struct snd_pcm_runtime *runtime = substream->runtime;
    	int link = prtd->asp_link[0];
    	unsigned int period_size;
    	unsigned int dma_offset;
    	dma_addr_t dma_pos;
    	dma_addr_t src, dst;
    	unsigned short src_bidx, dst_bidx;
    	unsigned short src_cidx, dst_cidx;
    	unsigned int data_type;
    	unsigned short acnt;
    	unsigned int count;
    	unsigned int fifo_level = 1;
    
    	period_size = snd_pcm_lib_period_bytes(substream);
    	dma_offset = prtd->period * period_size;
    	dma_pos = runtime->dma_addr + dma_offset;
    
        /* Amagi: Changed fifo level runtime based on the number of output channels
         * */
        if(substream->runtime->channels == 8)
        {
            fifo_level = 4;
        }
        else if(substream->runtime->channels == 6)
        {
            fifo_level = 3;
        }
        else if(substream->runtime->channels == 4)
        {
            fifo_level = 2;
        }
        else if(substream->runtime->channels == 2)
        {
            fifo_level = 1;
        }
    #if 0
        if(substream->runtime->channels == 4 &&
                substream->stream == SNDRV_PCM_STREAM_PLAYBACK)
        {
            fifo_level = 2;
        }
        else if(substream->runtime->channels == 2 &&
                substream->stream == SNDRV_PCM_STREAM_PLAYBACK)
        {
            fifo_level = 1;
        }
    #endif //0
    	//fifo_level = prtd->params->fifo_level;
    
    #ifdef AMAGI_DEBUG
        if(print_edma_flag)
        {
            printk("davinci_pcm: davinci_pcm_enqueue_dma channel = %d "
                "dma_ptr = %x period_size=%x\n", link, dma_pos, period_size);
        }
    #endif //AMAGI_DEBUG
    
    	data_type = prtd->params->data_type;
    	count = period_size / data_type;
    	if (fifo_level)
    		count /= fifo_level;
    
    	if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    		src = dma_pos;
    		dst = prtd->params->dma_addr;
    		src_bidx = data_type;
    		dst_bidx = 0;
    		src_cidx = data_type * fifo_level;
    		dst_cidx = 0;
    	} else {
    		src = prtd->params->dma_addr;
    		dst = dma_pos;
    		src_bidx = 0;
    		dst_bidx = data_type;
    		src_cidx = 0;
    		dst_cidx = data_type * fifo_level;
    	}
    
    	acnt = prtd->params->acnt;
    	edma_set_src(link, src, INCR, W8BIT);
    	edma_set_dest(link, dst, INCR, W8BIT);
    
    	edma_set_src_index(link, src_bidx, src_cidx);
    	edma_set_dest_index(link, dst_bidx, dst_cidx);
    
    	if (!fifo_level)
    		edma_set_transfer_params(link, acnt, count, 1, 0, ASYNC);
    	else
    		edma_set_transfer_params(link, acnt, fifo_level, count,
    							fifo_level, ABSYNC);
    
    #ifdef AMAGI_DEBUG
        pr_debug("print_edma_flag=%d link=%d\n", print_edma_flag, link);
        if(print_edma_flag)
        {
            print_buf_info(link, "asp_channel");
        }
    #endif //AMAGI_DEBUG
    
    	prtd->period++;
    	if (unlikely(prtd->period >= runtime->periods))
        {
    		prtd->period = 0;
    #ifdef AMAGI_DEBUG
            print_edma_flag = 0;
    #endif //AMAGI_DEBUG
        }
    }
    
    static void davinci_pcm_dma_irq(unsigned link, u16 ch_status, void *data)
    {
    	struct snd_pcm_substream *substream = data;
    	struct davinci_runtime_data *prtd = substream->runtime->private_data;
    	unsigned int period_size;
    	period_size = snd_pcm_lib_period_bytes(substream);
    
    	//print_buf_info(prtd->ram_channel, "i ram_channel");
    	/*printk("In %s: link=%d, status=0x%x, stream=%d\n", __func__, link,
                ch_status, substream->stream);*/
    
    	if (unlikely(ch_status != DMA_COMPLETE))
    		return;
    
    	if (snd_pcm_running(substream)) {
    		if (prtd->ram_channel < 0) {
    			/* No ping/pong must fix up link dma data*/
    			spin_lock(&prtd->lock);
    			davinci_pcm_enqueue_dma(substream);
    			spin_unlock(&prtd->lock);
    		}
    		snd_pcm_period_elapsed(substream);
            prtd->offset += period_size;
            prtd->offset %= period_size * substream->runtime->periods;
    
    	}
    }
    
    static int allocate_sram(struct snd_pcm_substream *substream, unsigned size,
    		struct snd_pcm_hardware *ppcm)
    {
    	struct snd_dma_buffer *buf = &substream->dma_buffer;
    #if !defined(CONFIG_ARCH_TI81XX)	/* No SRAM support on TI81xx */
    	struct snd_dma_buffer *iram_dma = NULL;
    	dma_addr_t iram_phys = 0;
    	void *iram_virt = NULL;
    #endif
    	if (buf->private_data || !size)
    		return 0;
    
    #if !defined(CONFIG_ARCH_TI81XX)	/* No SRAM support on TI81xx */
    	ppcm->period_bytes_max = size;
    	iram_virt = sram_alloc(size, &iram_phys);
    	if (!iram_virt)
    		goto exit1;
    	iram_dma = kzalloc(sizeof(*iram_dma), GFP_KERNEL);
    	if (!iram_dma)
    		goto exit2;
    	iram_dma->area = iram_virt;
    	iram_dma->addr = iram_phys;
    	memset(iram_dma->area, 0, size);
    	iram_dma->bytes = size;
    	buf->private_data = iram_dma;
    	return 0;
    exit2:
    	if (iram_virt)
    		sram_free(iram_virt, size);
    exit1:
    	return -ENOMEM;
    #else
    	return 0;
    #endif
    }
    
    /*
     * Only used with ping/pong.
     * This is called after runtime->dma_addr, period_bytes and data_type are valid
     */
    static int ping_pong_dma_setup(struct snd_pcm_substream *substream)
    {
    	unsigned short ram_src_cidx, ram_dst_cidx;
    	struct snd_pcm_runtime *runtime = substream->runtime;
    	struct davinci_runtime_data *prtd = runtime->private_data;
    	struct snd_dma_buffer *iram_dma =
    		(struct snd_dma_buffer *)substream->dma_buffer.private_data;
    	struct davinci_pcm_dma_params *params = prtd->params;
    	unsigned int data_type = params->data_type;
    	unsigned int acnt = params->acnt;
    	/* divide by 2 for ping/pong */
    	unsigned int ping_size = snd_pcm_lib_period_bytes(substream) >> 1;
    	int link = prtd->asp_link[1];
    	unsigned int fifo_level = prtd->params->fifo_level;
    	unsigned int count;
    	if ((data_type == 0) || (data_type > 4)) {
    		printk(KERN_ERR "%s: data_type=%i\n", __func__, data_type);
    		return -EINVAL;
    	}
    	if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    		dma_addr_t asp_src_pong = iram_dma->addr + ping_size;
    		ram_src_cidx = ping_size;
    		ram_dst_cidx = -ping_size;
    		edma_set_src(link, asp_src_pong, INCR, W8BIT);
    
    		link = prtd->asp_link[0];
    		edma_set_src_index(link, data_type, data_type * fifo_level);
    		link = prtd->asp_link[1];
    		edma_set_src_index(link, data_type, data_type * fifo_level);
    
    		link = prtd->ram_link;
    		edma_set_src(link, runtime->dma_addr, INCR, W32BIT);
    	} else {
    		dma_addr_t asp_dst_pong = iram_dma->addr + ping_size;
    		ram_src_cidx = -ping_size;
    		ram_dst_cidx = ping_size;
    		edma_set_dest(link, asp_dst_pong, INCR, W8BIT);
    
    		link = prtd->asp_link[0];
    		edma_set_dest_index(link, data_type, data_type * fifo_level);
    		link = prtd->asp_link[1];
    		edma_set_dest_index(link, data_type, data_type * fifo_level);
    
    		link = prtd->ram_link;
    		edma_set_dest(link, runtime->dma_addr, INCR, W32BIT);
    	}
    
    	if (!fifo_level) {
    		count = ping_size / data_type;
    		edma_set_transfer_params(prtd->asp_link[0], acnt, count,
    				1, 0, ASYNC);
    		edma_set_transfer_params(prtd->asp_link[1], acnt, count,
    				1, 0, ASYNC);
    	} else {
    		count = ping_size / (data_type * fifo_level);
    		edma_set_transfer_params(prtd->asp_link[0], acnt, fifo_level,
    				count, fifo_level, ABSYNC);
    		edma_set_transfer_params(prtd->asp_link[1], acnt, fifo_level,
    				count, fifo_level, ABSYNC);
    	}
    
    	link = prtd->ram_link;
    	edma_set_src_index(link, ping_size, ram_src_cidx);
    	edma_set_dest_index(link, ping_size, ram_dst_cidx);
    	edma_set_transfer_params(link, ping_size, 2,
    			runtime->periods, 2, ASYNC);
    
    	/* init master params */
    	edma_read_slot(prtd->asp_link[0], &prtd->asp_params);
    	edma_read_slot(prtd->ram_link, &prtd->ram_params);
    	if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    		struct edmacc_param p_ram;
    		/* Copy entire iram buffer before playback started */
    		prtd->ram_params.a_b_cnt = (1 << 16) | (ping_size << 1);
    		/* 0 dst_bidx */
    		prtd->ram_params.src_dst_bidx = (ping_size << 1);
    		/* 0 dst_cidx */
    		prtd->ram_params.src_dst_cidx = (ping_size << 1);
    		prtd->ram_params.ccnt = 1;
    
    		/* Skip 1st period */
    		edma_read_slot(prtd->ram_link, &p_ram);
    		p_ram.src += (ping_size << 1);
    		p_ram.ccnt -= 1;
    		edma_write_slot(prtd->ram_link2, &p_ram);
    		/*
    		 * When 1st started, ram -> iram dma channel will fill the
    		 * entire iram.  Then, whenever a ping/pong asp buffer finishes,
    		 * 1/2 iram will be filled.
    		 */
    		prtd->ram_params.link_bcntrld =
    			EDMA_CHAN_SLOT(prtd->ram_link2) << 5;
    	}
    	return 0;
    }
    
    /* 1 asp tx or rx channel using 2 parameter channels
     * 1 ram to/from iram channel using 1 parameter channel
     *
     * Playback
     * ram copy channel kicks off first,
     * 1st ram copy of entire iram buffer completion kicks off asp channel
     * asp tcc always kicks off ram copy of 1/2 iram buffer
     *
     * Record
     * asp channel starts, tcc kicks off ram copy
     */
    static int request_ping_pong(struct snd_pcm_substream *substream,
    		struct davinci_runtime_data *prtd,
    		struct snd_dma_buffer *iram_dma)
    {
    	dma_addr_t asp_src_ping;
    	dma_addr_t asp_dst_ping;
    	int link;
    	struct davinci_pcm_dma_params *params = prtd->params;
    
    	/* Request ram master channel */
    	link = prtd->ram_channel = edma_alloc_channel(EDMA_CHANNEL_ANY,
    				  davinci_pcm_dma_irq, substream,
    				  prtd->params->ram_chan_q);
    	if (link < 0)
    		goto exit1;
    
    	/* Request ram link channel */
    	link = prtd->ram_link = edma_alloc_slot(
    			EDMA_CTLR(prtd->ram_channel), EDMA_SLOT_ANY);
    	if (link < 0)
    		goto exit2;
    
    	link = prtd->asp_link[1] = edma_alloc_slot(
    			EDMA_CTLR(prtd->asp_channel), EDMA_SLOT_ANY);
    	if (link < 0)
    		goto exit3;
    
    	prtd->ram_link2 = -1;
    	if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    		link = prtd->ram_link2 = edma_alloc_slot(
    			EDMA_CTLR(prtd->ram_channel), EDMA_SLOT_ANY);
    		if (link < 0)
    			goto exit4;
    	}
    	/* circle ping-pong buffers */
    	edma_link(prtd->asp_link[0], prtd->asp_link[1]);
    	edma_link(prtd->asp_link[1], prtd->asp_link[0]);
    	/* circle ram buffers */
    	edma_link(prtd->ram_link, prtd->ram_link);
    
    	if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    		asp_src_ping = iram_dma->addr;
    		asp_dst_ping = params->dma_addr;	/* fifo */
    	} else {
    		asp_src_ping = params->dma_addr;	/* fifo */
    		asp_dst_ping = iram_dma->addr;
    	}
    	/* ping */
    	link = prtd->asp_link[0];
    	edma_set_src(link, asp_src_ping, INCR, W16BIT);
    	edma_set_dest(link, asp_dst_ping, INCR, W16BIT);
    	edma_set_src_index(link, 0, 0);
    	edma_set_dest_index(link, 0, 0);
    
    	edma_read_slot(link, &prtd->asp_params);
    	prtd->asp_params.opt &= ~(TCCMODE | EDMA_TCC(0x3f) | TCINTEN);
    	prtd->asp_params.opt |= TCCHEN | EDMA_TCC(prtd->ram_channel & 0x3f);
    	edma_write_slot(link, &prtd->asp_params);
    
    	/* pong */
    	link = prtd->asp_link[1];
    	edma_set_src(link, asp_src_ping, INCR, W16BIT);
    	edma_set_dest(link, asp_dst_ping, INCR, W16BIT);
    	edma_set_src_index(link, 0, 0);
    	edma_set_dest_index(link, 0, 0);
    
    	edma_read_slot(link, &prtd->asp_params);
    	prtd->asp_params.opt &= ~(TCCMODE | EDMA_TCC(0x3f));
    	/* interrupt after every pong completion */
    	prtd->asp_params.opt |= TCINTEN | TCCHEN |
    		EDMA_TCC(EDMA_CHAN_SLOT(prtd->ram_channel));
    	edma_write_slot(link, &prtd->asp_params);
    
    	/* ram */
    	link = prtd->ram_link;
    	edma_set_src(link, iram_dma->addr, INCR, W32BIT);
    	edma_set_dest(link, iram_dma->addr, INCR, W32BIT);
    	pr_debug("%s: audio dma channels/slots in use for ram:%u %u %u,"
    		"for asp:%u %u %u\n", __func__,
    		prtd->ram_channel, prtd->ram_link, prtd->ram_link2,
    		prtd->asp_channel, prtd->asp_link[0],
    		prtd->asp_link[1]);
    	return 0;
    exit4:
    	edma_free_channel(prtd->asp_link[1]);
    	prtd->asp_link[1] = -1;
    exit3:
    	edma_free_channel(prtd->ram_link);
    	prtd->ram_link = -1;
    exit2:
    	edma_free_channel(prtd->ram_channel);
    	prtd->ram_channel = -1;
    exit1:
    	return link;
    }
    
    static int davinci_pcm_dma_request(struct snd_pcm_substream *substream)
    {
    	struct snd_dma_buffer *iram_dma;
    	struct davinci_runtime_data *prtd = substream->runtime->private_data;
    	struct davinci_pcm_dma_params *params = prtd->params;
    	int link;
    
    	if (!params)
    		return -ENODEV;
    
    	/* Request asp master DMA channel */
    	link = prtd->asp_channel = edma_alloc_channel(params->channel,
    			davinci_pcm_dma_irq, substream,
    			prtd->params->asp_chan_q);
    	if (link < 0)
    		goto exit1;
    
    
    
    	/* Request asp link channels */
    	link = prtd->asp_link[0] = edma_alloc_slot(
    			EDMA_CTLR(prtd->asp_channel), EDMA_SLOT_ANY);
    	if (link < 0)
    		goto exit2;
    
    	iram_dma = (struct snd_dma_buffer *)substream->dma_buffer.private_data;
    	if (iram_dma) {
    		if (request_ping_pong(substream, prtd, iram_dma) == 0)
    			return 0;
    		printk(KERN_WARNING "%s: dma channel allocation failed,"
    				"not using sram\n", __func__);
    	}
    
    	/* Issue transfer completion IRQ when the channel completes a
    	 * transfer, then always reload from the same slot (by a kind
    	 * of loopback link).  The completion IRQ handler will update
    	 * the reload slot with a new buffer.
    	 *
    	 * REVISIT save p_ram here after setting up everything except
    	 * the buffer and its length (ccnt) ... use it as a template
    	 * so davinci_pcm_enqueue_dma() takes less time in IRQ.
    	 */
    	edma_read_slot(link, &prtd->asp_params);
    	prtd->asp_params.opt |= TCINTEN |
    		EDMA_TCC(EDMA_CHAN_SLOT(prtd->asp_channel));
    	prtd->asp_params.link_bcntrld = EDMA_CHAN_SLOT(link) << 5;
        edma_write_slot(link, &prtd->asp_params);
    
    	return 0;
    exit2:
    	edma_free_channel(prtd->asp_channel);
    	prtd->asp_channel = -1;
    exit1:
    	return link;
    }
    
    static int davinci_pcm_trigger(struct snd_pcm_substream *substream, int cmd)
    {
    	struct davinci_runtime_data *prtd = substream->runtime->private_data;
    	int ret = 0;
    
    	spin_lock(&prtd->lock);
    
    	switch (cmd) {
    	case SNDRV_PCM_TRIGGER_START:
    	case SNDRV_PCM_TRIGGER_RESUME:
    	case SNDRV_PCM_TRIGGER_PAUSE_RELEASE:
    		edma_resume(prtd->asp_channel);
    		break;
    	case SNDRV_PCM_TRIGGER_STOP:
    	case SNDRV_PCM_TRIGGER_SUSPEND:
    	case SNDRV_PCM_TRIGGER_PAUSE_PUSH:
    		edma_pause(prtd->asp_channel);
    		break;
    	default:
    		ret = -EINVAL;
    		break;
    	}
    
    	spin_unlock(&prtd->lock);
    
    	return ret;
    }
    
    static int davinci_pcm_prepare(struct snd_pcm_substream *substream)
    {
    	struct davinci_runtime_data *prtd = substream->runtime->private_data;
        int ret;
    
    #ifdef AMAGI_DEBUG
        printk("amagi: In %s, substream=0x%x, num_channels=%d, num_frame_bits=%d, strm_dir=%d\n",
                __func__, (unsigned int)substream, substream->runtime->channels, substream->runtime->frame_bits,
                substream->stream);
        print_edma_flag = 1;
    #endif //AMAGI_DEBUG
    	if (prtd->ram_channel >= 0) {
            printk("Calling ping_pong_dma_setup\n");
    		ret = ping_pong_dma_setup(substream);
    		if (ret < 0)
    			return ret;
    
    		edma_write_slot(prtd->ram_channel, &prtd->ram_params);
    		edma_write_slot(prtd->asp_channel, &prtd->asp_params);
    
    		print_buf_info(prtd->ram_channel, "ram_channel");
    		print_buf_info(prtd->ram_link, "ram_link");
    		print_buf_info(prtd->ram_link2, "ram_link2");
    		print_buf_info(prtd->asp_channel, "asp_channel");
    		print_buf_info(prtd->asp_link[0], "asp_link[0]");
    		print_buf_info(prtd->asp_link[1], "asp_link[1]");
    
    		if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    			/* copy 1st iram buffer */
    			edma_start(prtd->ram_channel);
    		}
    		edma_start(prtd->asp_channel);
    		return 0;
    	}
    	prtd->period = 0;
        prtd->offset = 0;
    	davinci_pcm_enqueue_dma(substream);
    
    	/* Copy self-linked parameter RAM entry into master channel */
    	edma_read_slot(prtd->asp_link[0], &prtd->asp_params);
    	edma_write_slot(prtd->asp_channel, &prtd->asp_params);
    	davinci_pcm_enqueue_dma(substream);
    	edma_start(prtd->asp_channel);
    
    	return 0;
    }
    
    static snd_pcm_uframes_t
    davinci_pcm_pointer(struct snd_pcm_substream *substream)
    {
    	struct snd_pcm_runtime *runtime = substream->runtime;
    	struct davinci_runtime_data *prtd = runtime->private_data;
    	unsigned int offset;
    	int asp_count;
    	dma_addr_t asp_src, asp_dst;
    
    	spin_lock(&prtd->lock);
    	if (prtd->ram_channel >= 0) {
    		int ram_count;
    		int mod_ram;
    		dma_addr_t ram_src, ram_dst;
    		unsigned int period_size = snd_pcm_lib_period_bytes(substream);
    		if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) {
    			/* reading ram before asp should be safe
    			 * as long as the asp transfers less than a ping size
    			 * of bytes between the 2 reads
    			 */
    			edma_get_position(prtd->ram_channel,
    					&ram_src, &ram_dst);
    			edma_get_position(prtd->asp_channel,
    					&asp_src, &asp_dst);
    			asp_count = asp_src - prtd->asp_params.src;
    			ram_count = ram_src - prtd->ram_params.src;
    			mod_ram = ram_count % period_size;
    			mod_ram -= asp_count;
    			if (mod_ram < 0)
    				mod_ram += period_size;
    			else if (mod_ram == 0) {
    				if (snd_pcm_running(substream))
    					mod_ram += period_size;
    			}
    			ram_count -= mod_ram;
    			if (ram_count < 0)
    				ram_count += period_size * runtime->periods;
    		} else {
    			edma_get_position(prtd->ram_channel,
    					&ram_src, &ram_dst);
    			ram_count = ram_dst - prtd->ram_params.dst;
    		}
    		asp_count = ram_count;
    	} else {
    		//edma_get_position(prtd->asp_channel, &asp_src, &asp_dst);
    		//if (substream->stream == SNDRV_PCM_STREAM_PLAYBACK)
    	//		asp_count = asp_src - runtime->dma_addr;
    	//	else
    	//		asp_count = asp_dst - runtime->dma_addr;
    		asp_count = prtd->offset;
    
    	}
    	spin_unlock(&prtd->lock);
    
    	offset = bytes_to_frames(runtime, asp_count);
    	if (offset >= runtime->buffer_size)
    		offset = 0;
    
    	return offset;
    }
    
    static int davinci_pcm_open(struct snd_pcm_substream *substream)
    {
    	struct snd_pcm_runtime *runtime = substream->runtime;
    	struct davinci_runtime_data *prtd;
    	struct snd_pcm_hardware *ppcm;
    	int ret = 0;
    	struct snd_soc_pcm_runtime *rtd = substream->private_data;
    	struct davinci_pcm_dma_params *pa;
    	struct davinci_pcm_dma_params *params;
    
    	pa = snd_soc_dai_get_dma_data(rtd->cpu_dai, substream);
    	if (!pa)
    		return -ENODEV;
    	params = &pa[substream->stream];
    
    	ppcm = (substream->stream == SNDRV_PCM_STREAM_PLAYBACK) ?
    			&pcm_hardware_playback : &pcm_hardware_capture;
    	allocate_sram(substream, params->sram_size, ppcm);
    	snd_soc_set_runtime_hwparams(substream, ppcm);
    
    	/* ensure that buffer size is a multiple of period size */
    	ret = snd_pcm_hw_constraint_integer(runtime,
    						SNDRV_PCM_HW_PARAM_PERIODS);
    	if (ret < 0)
    		return ret;
    
    	prtd = kzalloc(sizeof(struct davinci_runtime_data), GFP_KERNEL);
    	if (prtd == NULL)
    		return -ENOMEM;
    
    	spin_lock_init(&prtd->lock);
    	prtd->params = params;
    	prtd->asp_channel = -1;
    	prtd->asp_link[0] = prtd->asp_link[1] = -1;
    	prtd->ram_channel = -1;
    	prtd->ram_link = -1;
    	prtd->ram_link2 = -1;
    
    	runtime->private_data = prtd;
    
    	ret = davinci_pcm_dma_request(substream);
    	if (ret) {
    		printk(KERN_ERR "davinci_pcm: Failed to get dma channels\n");
    		kfree(prtd);
    	}
    	return ret;
    }
    
    static int davinci_pcm_close(struct snd_pcm_substream *substream)
    {
    	struct snd_pcm_runtime *runtime = substream->runtime;
    	struct davinci_runtime_data *prtd = runtime->private_data;
    
    	if (prtd->ram_channel >= 0)
    		edma_stop(prtd->ram_channel);
    	if (prtd->asp_channel >= 0)
    		edma_stop(prtd->asp_channel);
    	if (prtd->asp_link[0] >= 0)
    		edma_unlink(prtd->asp_link[0]);
    	if (prtd->asp_link[1] >= 0)
    		edma_unlink(prtd->asp_link[1]);
    	if (prtd->ram_link >= 0)
    		edma_unlink(prtd->ram_link);
    
    	if (prtd->asp_link[0] >= 0)
    		edma_free_slot(prtd->asp_link[0]);
    	if (prtd->asp_link[1] >= 0)
    		edma_free_slot(prtd->asp_link[1]);
    	if (prtd->asp_channel >= 0)
    		edma_free_channel(prtd->asp_channel);
    	if (prtd->ram_link >= 0)
    		edma_free_slot(prtd->ram_link);
    	if (prtd->ram_link2 >= 0)
    		edma_free_slot(prtd->ram_link2);
    	if (prtd->ram_channel >= 0)
    		edma_free_channel(prtd->ram_channel);
    
    	kfree(prtd);
    
    	return 0;
    }
    
    static int davinci_pcm_hw_params(struct snd_pcm_substream *substream,
    				 struct snd_pcm_hw_params *hw_params)
    {
    	return snd_pcm_lib_malloc_pages(substream,
    					params_buffer_bytes(hw_params));
    }
    
    static int davinci_pcm_hw_free(struct snd_pcm_substream *substream)
    {
    	return snd_pcm_lib_free_pages(substream);
    }
    
    static int davinci_pcm_mmap(struct snd_pcm_substream *substream,
    			    struct vm_area_struct *vma)
    {
    	struct snd_pcm_runtime *runtime = substream->runtime;
    
    	return dma_mmap_writecombine(substream->pcm->card->dev, vma,
    				     runtime->dma_area,
    				     runtime->dma_addr,
    				     runtime->dma_bytes);
    }
    
    static struct snd_pcm_ops davinci_pcm_ops = {
    	.open = 	davinci_pcm_open,
    	.close = 	davinci_pcm_close,
    	.ioctl = 	snd_pcm_lib_ioctl,
    	.hw_params = 	davinci_pcm_hw_params,
    	.hw_free = 	davinci_pcm_hw_free,
    	.prepare = 	davinci_pcm_prepare,
    	.trigger = 	davinci_pcm_trigger,
    	.pointer = 	davinci_pcm_pointer,
    	.mmap = 	davinci_pcm_mmap,
    };
    
    static int davinci_pcm_preallocate_dma_buffer(struct snd_pcm *pcm, int stream,
    		size_t size)
    {
    	struct snd_pcm_substream *substream = pcm->streams[stream].substream;
    	struct snd_dma_buffer *buf = &substream->dma_buffer;
    
    	buf->dev.type = SNDRV_DMA_TYPE_DEV;
    	buf->dev.dev = pcm->card->dev;
    	buf->private_data = NULL;
    	buf->area = dma_alloc_writecombine(pcm->card->dev, size,
    					   &buf->addr, GFP_KERNEL);
    
    	pr_debug("davinci_pcm: preallocate_dma_buffer: area=%p, addr=%p, "
    		"size=%d\n", (void *) buf->area, (void *) buf->addr, size);
    
        printk("allocating size %d\n", size);
    
    	if (!buf->area){
    		printk("dma_alloca_writecombine failed \n");
    		return -ENOMEM;
    	}
    
    	buf->bytes = size;
    	return 0;
    }
    
    static void davinci_pcm_free(struct snd_pcm *pcm)
    {
    	struct snd_pcm_substream *substream;
    	struct snd_dma_buffer *buf;
    	int stream;
    
    	for (stream = 0; stream < 2; stream++) {
    		struct snd_dma_buffer *iram_dma;
    		substream = pcm->streams[stream].substream;
    		if (!substream)
    			continue;
    
    		buf = &substream->dma_buffer;
    		if (!buf->area)
    			continue;
    
    		dma_free_writecombine(pcm->card->dev, buf->bytes,
    				      buf->area, buf->addr);
    		buf->area = NULL;
    		iram_dma = buf->private_data;
    		if (iram_dma) {
    #if !defined(CONFIG_ARCH_TI81XX)	/* No SRAM support on TI81xx */
    			sram_free(iram_dma->area, iram_dma->bytes);
    			kfree(iram_dma);
    #endif
    		}
    	}
    }
    
    static u64 davinci_pcm_dmamask = 0xffffffff;
    
    static int davinci_pcm_new(struct snd_card *card,
    			   struct snd_soc_dai *dai, struct snd_pcm *pcm)
    {
    	int ret;
    
    	if (!card->dev->dma_mask)
    		card->dev->dma_mask = &davinci_pcm_dmamask;
    	if (!card->dev->coherent_dma_mask)
    		card->dev->coherent_dma_mask = 0xffffffff;
    
    	if (dai->driver->playback.channels_min) {
    		ret = davinci_pcm_preallocate_dma_buffer(pcm,
    			SNDRV_PCM_STREAM_PLAYBACK,
    			pcm_hardware_playback.buffer_bytes_max);
    		if (ret)
    			return ret;
    	}
    
    	if (dai->driver->capture.channels_min) {
    		ret = davinci_pcm_preallocate_dma_buffer(pcm,
    			SNDRV_PCM_STREAM_CAPTURE,
    			pcm_hardware_capture.buffer_bytes_max);
    		if (ret)
    			return ret;
    	}
    
    	return 0;
    }
    
    static struct snd_soc_platform_driver davinci_soc_platform = {
    	.ops =		&davinci_pcm_ops,
    	.pcm_new = 	davinci_pcm_new,
    	.pcm_free = 	davinci_pcm_free,
    };
    
    static int __devinit davinci_soc_platform_probe(struct platform_device *pdev)
    {
    	return snd_soc_register_platform(&pdev->dev, &davinci_soc_platform);
    }
    
    static int __devexit davinci_soc_platform_remove(struct platform_device *pdev)
    {
    	snd_soc_unregister_platform(&pdev->dev);
    	return 0;
    }
    
    static struct platform_driver davinci_pcm_driver = {
    	.driver = {
    			.name = "davinci-pcm-audio",
    			.owner = THIS_MODULE,
    	},
    
    	.probe = davinci_soc_platform_probe,
    	.remove = __devexit_p(davinci_soc_platform_remove),
    };
    
    static int __init snd_davinci_pcm_init(void)
    {
    	return platform_driver_register(&davinci_pcm_driver);
    }
    module_init(snd_davinci_pcm_init);
    
    static void __exit snd_davinci_pcm_exit(void)
    {
    	platform_driver_unregister(&davinci_pcm_driver);
    }
    module_exit(snd_davinci_pcm_exit);
    
    MODULE_AUTHOR("Vladimir Barinov");
    MODULE_DESCRIPTION("TI DAVINCI PCM DMA module");
    MODULE_LICENSE("GPL");
    

  • Thank you.  I've inserted your changes associated with the offset variable into our davinci-pcm.c and have been running it for about 30 minutes without any underruns so far.  Normally I would see underruns every 4 to 10 minutes.  Looks good so far.  I'll continue testing.  Thank you again.

  • Ran it for over 24 hours.  No underruns seen.  Looks like it's fixed.  Thank you very much.

  • We also run into this problem and fixed it by fixing edma_get_position(). The root problem is that edma_get_position() reads the whole PaRAM descriptor into a temporary buffer using edma_read_slot() and this function uses memcpy_fromio() to do the copy, which in turn simply does a byte by byte copy.

    Doing a byte by byte copy is racy as the EDMA engine may update the PaRAM in between the byte reads done by the ARM. The issue with edma_get_position() occurs when the PaRAM is updated by the EDMA engine after a few bytes of dst or src, but not all, have been read by the ARM, so the read dst or src value is a half the old value and half the new value, which often shows as a wraparound in the buffer position.

    The fix is simple and consists in doing 4-byte read accesses in edma_get_position() to read src and/or dst as necessary. As the 4-byte reads are atomic the race is gone. BTW, this is what the EDMA driver does in the mainline kernel.

    Patch is attached (with extension .txt as .diff cannot be uploaded).

    Index: arch/arm/common/edma.c
    ===================================================================
    --- arch/arm/common/edma.c	(revision 26593)
    +++ arch/arm/common/edma.c	(revision 26594)
    @@ -944,17 +944,19 @@
      */
     void edma_get_position(unsigned slot, dma_addr_t *src, dma_addr_t *dst)
     {
    -	struct edmacc_param temp;
     	unsigned ctlr;
    +	void __iomem *pbase;
     
     	ctlr = EDMA_CTLR(slot);
     	slot = EDMA_CHAN_SLOT(slot);
     
    -	edma_read_slot(EDMA_CTLR_CHAN(ctlr, slot), &temp);
    +	if (slot >= edma_info[ctlr]->num_slots)
    +		return;
    +	pbase = edmacc_regs_base[ctlr] + PARM_OFFSET(slot);
     	if (src != NULL)
    -		*src = temp.src;
    +		*src = (dma_addr_t) __raw_readl(pbase + PARM_SRC);
     	if (dst != NULL)
    -		*dst = temp.dst;
    +		*dst = (dma_addr_t) __raw_readl(pbase + PARM_DST);
     }
     EXPORT_SYMBOL(edma_get_position);