This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NO DISPLAY Run mcfw cap_dis demo (8168EVM+EIO card )

Other Parts Discussed in Thread: TVP7002

hi,everybody

i use DVRRDK4.0 and 8168 evm+eio card ,but when i run cap_dis demo ,the hdmi can not output, the hdmi screen print“NO INPUT SINGAL”。the cap_dis link is not complex,code as follow:

CaptureLink_CreateParams capturePrm;
DisplayLink_CreateParams displayPrm;
CaptureLink_VipInstParams *pCaptureInstPrm;
CaptureLink_OutParams *pCaptureOutPrm;

MULTICH_INIT_STRUCT(DisplayLink_CreateParams,displayPrm);

MultiCh_detectBoard();

System_linkControl(
SYSTEM_LINK_ID_M3VPSS,
SYSTEM_M3VPSS_CMD_RESET_VIDEO_DEVICES,
NULL,
0,
TRUE
);
gVcapModuleContext.captureId = SYSTEM_LINK_ID_CAPTURE;
gVdisModuleContext.displayId[0] = SYSTEM_LINK_ID_DISPLAY_0;


CaptureLink_CreateParams_Init(&capturePrm);
capturePrm.numVipInst = 1;
capturePrm.outQueParams[0].nextLink = gVdisModuleContext.displayId[0];;
capturePrm.tilerEnable = FALSE;
capturePrm.enableSdCrop = FALSE;

pCaptureInstPrm = &capturePrm.vipInst[0];
pCaptureInstPrm->vipInstId = SYSTEM_CAPTURE_INST_VIP0_PORTA;
pCaptureInstPrm->videoDecoderId = 0;// not 5158
pCaptureInstPrm->inDataFormat = SYSTEM_DF_YUV422P;
pCaptureInstPrm->standard = SYSTEM_STD_720P_60;
pCaptureInstPrm->numOutput = 1;
pCaptureInstPrm->inScanFormat = SYSTEM_SF_PROGRESSIVE;

pCaptureOutPrm = &pCaptureInstPrm->outParams[0];
pCaptureOutPrm->dataFormat = SYSTEM_DF_YUV422I_YUYV;
pCaptureOutPrm->scEnable = FALSE;
pCaptureOutPrm->scOutWidth = 0;
pCaptureOutPrm->scOutHeight = 0;
pCaptureOutPrm->outQueId = 0;


displayPrm.inQueParams[0].prevLinkId = gVcapModuleContext.captureId;
displayPrm.inQueParams[0].prevLinkQueId = 0;
displayPrm.displayRes = gVdisModuleContext.vdisConfig.deviceParams[VDIS_DEV_HDMI].resolution;

//capturePrm.isPalMode = Vcap_isPalMode();
capturePrm.isPalMode = FALSE;
System_linkCreate (gVcapModuleContext.captureId, &capturePrm, sizeof(capturePrm));
System_linkCreate(gVdisModuleContext.displayId[0], &displayPrm, sizeof(displayPrm));
MultiCh_memPrintHeapStatus();

 when running the demo,output information in log.txt,it seems like that the capture does caputured videos.

1154698: SYSTEM: ListElem Shared Addr = 0x406a2900
 1154699: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
 1154701: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
 1154703: SYSTEM: ListElem Shared Addr = 0x406d9700
 1154704: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
 1154707: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
 1154709: SYSTEM: ListElem Shared Addr = 0x40753580
 1154710: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
 1154712: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
 1154714: SYSTEM: ListElem Shared Addr = 0x40796880
 1154715: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
 1154718: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
 1154720: SYSTEM: ListElem Shared Addr = 0x407d9600
 1154736: SYSTEM: System Common Init Done !!!
 [host] HDMI Ctrl :Initializing
[HOST] 
ThreadName:Vdis_hdmiControlThread_0,ThreadID:783
 [host] HDMI Ctrl :Initialized
 [host] HDMI Ctrl :Sink Connected
 [FBDEV] 
 [FBDEV] FB: Starting !!!
 [FBDEV] ERROR: FB: Could not open device [/dev/fb0] !!! 
 1154740: MCFW  : CPU Revision [ES1.0] !!! 
 [m3vpss ]  1162771: CAPTURE: Create in progress !!!
 [m3vpss ]  1162800: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!! 
 [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 58 (58)
 [m3vpss ]  UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
 [m3vpss ]  UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
 [m3vpss ]  UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
 [m3vpss ]  UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
 [m3vpss ] CAPTURE::HEAPID:0    USED:328
 [m3vpss ] CAPTURE::HEAPID:4    USED:24422400
 [m3vpss ]  1162897: CAPTURE: Create Done !!!
 [m3vpss ]  1162897: DISPLAY: Create in progress !!!
 [m3vpss ]  1162898: DISPLAY: Create Done !!!
 [m3vpss ]  1162899: DISPLAY: Start in progress !!!
 [m3vpss ]  1162937: DISPLAY: Start Done !!!
 [m3vpss ]  1162937: DISPLAY: HDDAC(BP0) : 52 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) DropCount:0 DispLatency (Min / Max) = ( 7811 / 
 [m3vpss ]  1162937: DISPLAY DRV: HDDAC(BP0) : Q:[2] Display:[2], Repeat:[1], DQ:[0]
 [m3vpss ]  1162937: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 0, HDDAC(BP0) 0, DVO2(BP1) 0, SDDAC(SEC1) 0 
 [m3vpss ]  1162937: SYSTEM  : FREE SPACE : System Heap      = 68048 B, Mbx = 10239 msgs) 
 [m3vpss ]  1162937: SYSTEM  : FREE SPACE : SR0 Heap         = 8682112 B (8 MB) 
 [m3vpss ]  1162937: SYSTEM  : FREE SPACE : Frame Buffer     = 249926528 B (238 MB) 
 [m3vpss ]  1162937: SYSTEM  : FREE SPACE : Bitstream Buffer = 210763648 B (200 MB) 
 [m3vpss ] TILER_STATS: CNT :8BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    16384 x 8192
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 8188
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134152192 (99 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ] TILER_STATS: CNT :16BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    32768 x 3072
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 3072
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   100663296 (100 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ]  1162939: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134152192 B (127 MB)  - TILER ON 
 [m3vpss ]  1162939: SYSTEM  : FREE SPACE : Tiler 16-bit     = 100663296 B (96 MB)  - TILER ON 
 [m3vpss ]  1164761: CAPTURE: Start in progress !!!
[HOST] 
ThreadName:Demo_run,ThreadID:757

 =============
 Run-Time Menu
 =============

 1: Capture Settings
 2: Encode  Settings
 3: Decode  Settings
 4: Display Settings
 5: Audio Capture <TVP5158> & Encode <AAC-LC, G711> demo
 6: Change Playback Channel <valid only if capture/playback is active>
 7: Audio encode demo <File In/Out>
 8: Audio decode demo <File In/Out>

 i: Print detailed system information
 s: Core Status: Active/In-active
 f: Switch IVA Channel Map

 e: Stop Demo

 Enter Choice:  [m3vpss ]  1164860: CAPTURE: Enabled Time Stamping !!!
 [m3vpss ]  1164863: CAPTURE: Start Done !!!
[HOST] 
ThreadName:SystemLink_tskMain_3000003f,ThreadID:782
 DEMO: HDMI TV/Monitor connected !!!
 DEMO: TV Detected - HDMI interface !!!
 DEMO: INFO : Resolution set to 1080P60 !!!
i
 
 
 [m3vpss ]  
 [m3vpss ]  *** Capture Driver Advanced Statistics *** 
 [m3vpss ]  
 [m3vpss ]  VIP Parser Reset Count : 0
 [m3vpss ]  
 [m3vpss ]      |   Total    Even     Odd  Total  Even   Odd  Min /  Max  Min /  Max Dropped Fid Repeat Frame Error Y/C
 [m3vpss ]  CH  |  Fields  Fields  Fields    FPS   FPS   FPS       Width      Height  Fields      Count (Desc Error Y/C)
 [m3vpss ]  ------------------------------------------------------------------------------------------------------------
 [m3vpss ]  000 |     491     491       0     61    61     0 1280 / 1280  720 /  720       1          0 0/0 (0/0)
 [m3vpss ]  
 [m3vpss ]  VIP Capture Port 0 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0 
 [m3vpss ]  
 [m3vpss ]  *** Capture List Manager Advanced Statistics *** 
 [m3vpss ]  
 [m3vpss ]  List Post Count        : 144397 
 [m3vpss ]  List Stall Count       : 0 
 [m3vpss ]  List Post Time (ms)    : Max = 0, Min = 0, Avg = 0, Total = 0 
 [m3vpss ]  INTC Timeout Count     : (0, 1) (Min timeout value = 980, 0) 
 [m3vpss ]  Descriptor miss found count : 0 
 [m3vpss ]  
 [m3vpss ]  
 [m3vpss ]  VIP and VPDMA registers, 
 [m3vpss ]  VIP0 : FIQ_STATUS  : 0x4810551c = 0x00000000
 [m3vpss ]  VIP1 : FIQ_STATUS  : 0x48105a1c = 0x00000000
 [m3vpss ]  VPDMA: LIST_BUSY   : 0x4810d00c = 0x00020000
 [m3vpss ]  
 [m3vpss ]  
 [m3vpss ]  1173072: CAPTURE: Fields = 489 (fps = 59, CPU Load = 0)
 [m3vpss ]  1173072: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
 [m3vpss ]  1173072: SYSTEM  : FREE SPACE : System Heap      = 68048 B, Mbx = 10238 msgs) 
 [m3vpss ]  1173072: SYSTEM  : FREE SPACE : SR0 Heap         = 8682112 B (8 MB) 
 [m3vpss ]  1173073: SYSTEM  : FREE SPACE : Frame Buffer     = 249926528 B (238 MB) 
 [m3vpss ]  1173073: SYSTEM  : FREE SPACE : Bitstream Buffer = 210763648 B (200 MB) 
 [m3vpss ] TILER_STATS: CNT :8BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    16384 x 8192
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 8188
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134152192 (99 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ] TILER_STATS: CNT :16BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    32768 x 3072
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 3072
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   100663296 (100 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ]  1173074: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134152192 B (127 MB)  - TILER ON 
 [m3vpss ]  1173074: SYSTEM  : FREE SPACE : Tiler 16-bit     = 100663296 B (96 MB)  - TILER ON 
 [m3vpss ]  1173074: DISPLAY: HDDAC(BP0) : 59 fps, Latency (Min / Max) = ( 74 / 92 ), Callback Interval (Min / Max) = ( 16 / 17 ) DropCount:0 DispLatency (Min / Max) = ( 49 / 6 
 [m3vpss ]  1173074: DISPLAY DRV: HDDAC(BP0) : Q:[491] Display:[610], Repeat:[121], DQ:[488]
 [m3vpss ]  1173075: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 608, HDDAC(BP0) 1123, DVO2(BP1) 1123, SDDAC(SEC1) 1123 
 [m3vpss ]  1173075: SYSTEM  : FREE SPACE : System Heap      = 68048 B, Mbx = 10239 msgs) 
 [m3vpss ]  1173075: SYSTEM  : FREE SPACE : SR0 Heap         = 8682112 B (8 MB) 
 [m3vpss ]  1173075: SYSTEM  : FREE SPACE : Frame Buffer     = 249926528 B (238 MB) 
 [m3vpss ]  1173075: SYSTEM  : FREE SPACE : Bitstream Buffer = 210763648 B (200 MB) 
 [m3vpss ] TILER_STATS: CNT :8BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    16384 x 8192
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 8188
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134152192 (99 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ] TILER_STATS: CNT :16BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    32768 x 3072
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 3072
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   100663296 (100 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ]  1173076: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134152192 B (127 MB)  - TILER ON 
 [m3vpss ]  1173076: SYSTEM  : FREE SPACE : Tiler 16-bit     = 100663296 B (96 MB)  - TILER ON 
 [m3vpss ]  
 [m3vpss ]  1182077: LOAD: CPU: 3.5% HWI: 0.6%, SWI:0.7% 
 [m3vpss ]  
 [m3vpss ]  1182077: LOAD: TSK: CAPTURE             : 0.9% 
 [m3vpss ]  1182077: LOAD: TSK: DISPLAY0            : 0.3% 
 [m3vpss ]  1182077: LOAD: TSK: MISC                : 1.0% 
 [m3vpss ]  
 [m3video]  
 [m3video]  1182578: LOAD: CPU: 0.5% HWI: 0.2%, SWI:0.1% 
 [m3video]  
 [m3video]  1182578: LOAD: TSK: MISC                : 0.2% 
 [m3video]  
 [c6xdsp ]  
 [c6xdsp ]  1182441: LOAD: CPU: 0.2% HWI: 0.0%, SWI:0.0% 
 [c6xdsp ]  
 [c6xdsp ]  1182441: LOAD: TSK: MISC                : 0.2% 
 [c6xdsp ]  
[HOST] 
ThreadName:Demo_run,ThreadID:757

 =============
 Run-Time Menu
 =============

 1: Capture Settings
 2: Encode  Settings
 3: Decode  Settings
 4: Display Settings
 5: Audio Capture <TVP5158> & Encode <AAC-LC, G711> demo
 6: Change Playback Channel <valid only if capture/playback is active>
 7: Audio encode demo <File In/Out>
 8: Audio decode demo <File In/Out>

 i: Print detailed system information
 s: Core Status: Active/In-active
 f: Switch IVA Channel Map

 e: Stop Demo

 Enter Choice: 

in the log,it print 

[host] HDMI Ctrl :Initializing
[HOST]
ThreadName:Vdis_hdmiControlThread_0,ThreadID:783
[host] HDMI Ctrl :Initialized
[host] HDMI Ctrl :Sink Connected
[FBDEV]
[FBDEV] FB: Starting !!!
[FBDEV] ERROR: FB: Could not open device [/dev/fb0] !!!

does it cause there is no display?

but i dont know where is wrong.

so, can you help me ?

thank you 

dv

  • Have you inserted FB modules in the kernel? If inserted, can you check if /dev/fb entries are present in devfs.

     

    Regards,

    Brijesh

  • hi,Brijesh

      Thank you for reply

      Is ti81xxfb.ko not inserted?after execute load.sh,the ti81xxfb.ko have been inserted.

      I checked /dev/, but there dont have fb

      And how to fix it?

      Regards

      dv

  • The logs shows display is running. Make sure you are connected to correct on chip HDMI .Also log shows silicon version is 1.0. Check your uboot/kernel boot up logs to confirm silcion revision . 1.0 silicon is not supported.

  • hi,Badri

        yes,silicon is 1.0.My evm is TI8168 with DIMM(DDR2). 

        You mean the 1.0 silicon is not supported for display? or encode? 

        in ezsdk,by v4l2 or HDVPSS,it can capture and display.

        Does it supprot encode?

        thank you 

    dv

  • There are numerous issues with PG1.0.Migrate to PG2.0 or PG2.1 for any further development.Encode will work on PG1.0.

  • hi,Badri

    thank you 

    i modify load.sh (ti81xxfb.ko the last param set to 4M )and success open /dev/fb0

    but there are still nothing on my screen...

    Regards

    dv

  • hi,Bresh

    now it can open /dev/fb0 by modify load.sh.

    but it still can not work.

    my video source is 720P30,in the cap_dsi.c,i set the 

    pCaptureInstPrm->standard = SYSTEM_STD_720P_60

    displayPrm.displayRes = gVdisModuleContext.vdisConfig.deviceParams[VDIS_DEV_HDMI].resolution

    maybe  the display params is not  correct?

    but if it is not correct,there are also something on the screen.

    so ,what could i do to fix it ?

    thank you 

    dv

  • Hi,

     

    Is your display device detecting the input signal and saying that it is receiving some resolution? Can you check you display device?

    You could even try 720p60 display resolution by setting,

    displayPrm.displayRes = SYSTEM_STD_720P_60

     

    Regards,

    Brijesh

  • Hi,Brijesh

    The HDMI output interface I used is on TI8168 EVM,and is this interface that be called "hdmi on chip"?

    The HDMI screen and cable can work well.

    when the demo began running,in 5 or 6 secs,the screen display white color and a balck line (I am sure this is not my video source),then the screen print “NO INPUT SIGNAL”

    and the FB LOGs as follow:

     [host] HDMI Ctrl :Initializing
    [HOST]
    ThreadName:Vdis_hdmiControlThread_0,ThreadID:948
     [host] HDMI Ctrl :Initialized
     [host] HDMI Ctrl :Sink Connected
     [FBDEV]
     [FBDEV] FB: Starting !!!
     [FBDEV] FB: Opened device [/dev/fb0] (fd=22) !!!
     [FBDEV]
     [FBDEV] Fix Screen Info
     [FBDEV] ---------------
     [FBDEV] Line Length - 2560
     [FBDEV] Physical Address = 8ea00000
     [FBDEV] Buffer Length = 8388608
     [FBDEV]
     [FBDEV]
     [FBDEV] Var Screen Info
     [FBDEV] ---------------
     [FBDEV] Xres - 1280
     [FBDEV] Yres - 720
     [FBDEV] Xres Virtual - 1280
     [FBDEV] Yres Virtual - 720
     [FBDEV] Bits Per Pixel - 16
     [FBDEV] Pixel Clk - 6734
     [FBDEV] Rotation - 0
     [FBDEV]
     [FBDEV]
     [FBDEV] Reg Params Info
     [FBDEV] ---------------
     [FBDEV] region 0, postion 0 x 0, prioirty 1
     [FBDEV] first 1, last 1
     [FBDEV] sc en 1, sten en 0
     [FBDEV] tran en 1, type 0, key 16777215
     [FBDEV] blend 0, alpha 0
     [FBDEV] bb en 0, alpha 0
     [FBDEV]
     [FBDEV]
     [FBDEV] ### BUF SIZE = 1843200 Bytes !!!
     [FBDEV]
     [FBDEV]
     [FBDEV] Fix Screen Info
     [FBDEV] ---------------
     [FBDEV] Line Length - 2560
     [FBDEV] Physical Address = 8ea00000
     [FBDEV] Buffer Length = 8388608
     [FBDEV]
     [FBDEV]
     [FBDEV] Var Screen Info
     [FBDEV] ---------------
     [FBDEV] Xres - 1280
     [FBDEV] Yres - 720
     [FBDEV] Xres Virtual - 1280
     [FBDEV] Yres Virtual - 720
     [FBDEV] Bits Per Pixel - 16
     [FBDEV] Pixel Clk - 6734
     [FBDEV] Rotation - 0
     [FBDEV]
     [FBDEV]
     [FBDEV] Reg Params Info
     [FBDEV] ---------------
     [FBDEV] region 0, postion 0 x 0, prioirty 1
     [FBDEV] first 1, last 1
     [FBDEV] sc en 1, sten en 0
     [FBDEV] tran en 1, type 0, key 16777215
     [FBDEV] blend 0, alpha 0
     [FBDEV] bb en 0, alpha 0
     [FBDEV]
     [FBDEV]
     [FBDEV] ### BUF SIZE = 1843200 Bytes !!!
     [FBDEV]
     [FBDEV] grpx_fb_draw ...
     [FBDEV] grpx_fb_draw ... Done !!!
     [FBDEV] FB: Start DONE !!!
     [FBDEV]

     thank you

    dv

  • Hi,

     

    When it switches off, can you give me address at the location 0x48106000?

     

    regards,

    Brijesh

  • Hi,Brejesh

    I use this way to get address:

    telnet 127.0.0.1

    sh init.sh

    sh load.sh

    after sh load.sh,the hdmi screen is dark,but it is displaying.

    ./mem_rdwr.out --rd 0x48106000

    output is 44023013

    then i run the demo,when the screen is off

    ctrl+]

    exit the telnet

    and read the 0x48106000 again

    the output is still 44023013

    i am thinking about that maybe i have link the hdmi cable with a wrong interface?

    in the demo,there are some xxx_init before vsys_creat,maybe somewhere need modify?

    I modify the vcap and vdis,make extenddecoder =Fasle.i dont modify any init expect this.

    thank you

    dv

  • Hi,Brijesh

    i set 0x48106000 as 4420B013

    then the hdmi screen dipaly as follow:

    my video source is 720p30 but i use the 720p60.sh to configure TVP7002,maybe i made a mistake ?

    but from the log,the capture seems like captured videos.

    Regards

    dv

  • Hi,Brijesh

    I use cap-nsf-enc link to test the that vin0 is capturing video source.

    And the H264 file was been created and can be decoded by Video Player.

    The resolution is 1280x720.But its color and format is not correct.

    contrast the video source ,A little left part (the part which red line point to  )of the image attached to the right part.

    this is video source and screenshot of the H264 file as follow:

    video source (photograph by my phone )

    h264 file decode play by video player:

    and the output log at here:

    root@dm816x:/opt/dvr_rdk/ti816x# sh tvp7002_720p60.sh                           
    root@dm816x:/opt/dvr_rdk/ti816x# ./test.out                                     
                                                                                    
     =========                                                                      
     Main Menu                                                                      
     =========                                                                      
                                                                                    
     1: VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode                 
     2: VCAP + VENC        + VDIS  - SD Encode ONLY                                 
     3: VCAP + VENC + VDEC + VDIS  - Progressive HD Encode + Decode                 
     4:               VDEC + VDIS  - SD/HD Decode ONLY                              
     6: VCAP + VENC + VDEC + VDIS  - Progressive HD+SD Encode + Decode              
     a: 960H DVR usecase                                                            
     b: 36CH Hybrid enc usecase                                                     
     c: 4CH Car DVR usecase                                                         
     d: 5CH SD+HD (Interlaced<->Progressive switch) usecase                         
                                                                                    
     e: Exit                                                                        
                                                                                    
     Enter Choice: 2                                                                
    --------------- CHANNEL DETAILS-------------                                    
    Capture Channels => 1                                                           
    Enc Channels => Primary 1, Secondary 1                                          
    Disp Channels => 1                                                              
    -------------------------------------------                                     
     0: SYSTEM: System Common Init in progress !!!                                  
     0: SYSTEM: IPC init in progress !!!                                            
     14: SYSTEM: CPU [DSP] syslink proc ID is [0] !!!                               
     14: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!!                          
     14: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!!                           
     14: SYSTEM: CPU [HOST] syslink proc ID is [3] !!!                              
     14: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...                       
     16: SYSTEM: Creating MsgQ [HOST_MSGQ] ...                                      
     18: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...                                  
     20: SYSTEM: Opening MsgQ [DSP_MSGQ] ...                                        
     21: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...                                   
     21: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...                                    
     22: SYSTEM: Notify register to [DSP] line 0, event 15 ...                      
     23: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...                 
     24: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...                  
     25: SYSTEM: IPC init DONE !!!                                                  
     26: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...                  
     28: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...                   
     30: SYSTEM: ListElem Shared Addr = 0x406b4680                                  
     31: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...                  
     33: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...                   
     35: SYSTEM: ListElem Shared Addr = 0x406eb480                                  
     36: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...                  
     38: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...                   
     40: SYSTEM: ListElem Shared Addr = 0x40722280                                  
     41: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...                  
     44: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...                   
     45: SYSTEM: ListElem Shared Addr = 0x40765580                                  
     46: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...                  
     49: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...                   
     50: SYSTEM: ListElem Shared Addr = 0x407a8880                                  
     67: SYSTEM: System Common Init Done !!!                                        
     [host] HDMI Ctrl :Initializing                                                 
    [HOST]                                                                          
    ThreadName:Vdis_hdmiControlThread_0,ThreadID:790                                
     [host] HDMI Ctrl :Initialized                                                  
                                                                                    
     Enable file write (YES - y / NO - n) : y                                       
                                                                                    
     File write ENABLED !!!                                                         
                                                                                    
                                                                                    
     Enter file write path : .                                                      
                                                                                    
     Selected file write path [.]                                                   
                                                                                    
                                                                                    
     Select File Write CH ID [0 .. 0] : 0                                           
                                                                                    
     Selected CH ID = 0                                                             
                                                                                    
                                                                                    
     [host] MCFW_IPCFRAMES:VcapVenc_ipcFramesSendRecvFxn:Entered... 3962: MCFW  : C 
     [m3vpss ]  61959: CAPTURE: Create in progress !!!                              
     Opened file [./VID_CH00.h264] for writing CH0                                  
     [m3vpss ]  61989: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedde 
     [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 58 (58)                            
     [m3vpss ]  UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)               
     [m3vpss ]  UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)               
     [m3vpss ]  UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)               
     [m3vpss ]  UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)               
     [m3vpss ] CAPTURE::HEAPID:0    USED:328                                        
     [m3vpss ] CAPTURE::HEAPID:4    USED:24422400                                   
     [m3vpss ]  62084: CAPTURE: Create Done !!!                                     
     [m3vpss ]  62085: NSF: Create in progress !!!                                  
     [m3video]  62127: IPC_IN_M3   : Create in progress !!!                         
     [m3video]  62127: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...               
     [m3video]  62127: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...                
     [m3vpss ] NSF::HEAPID:0        USED:128                                        
     [m3video]  62130: IPC_IN_M3   : Create Done !!!                                
     [m3vpss ] NSF::HEAPID:1        USED:4928                                       
     [m3video]  62130: ENCODE: Create in progress ... !!!                           
     [m3vpss ] NSF::HEAPID:4        USED:8478720                                    
     [m3vpss ]  62125: NSF: Create Done !!!                                         
     [m3vpss ]  62126: IPC_OUT_M3   : Create in progress !!!                        
     [m3vpss ]  62127: IPC_OUT_M3   : Create Done !!!                               
     [m3video]  62146: ENCODE: Creating CH0 of 1280 x 720, pitch = (1280, 1280) [PR 
                                                                                    
     [host] IpcBitsInLink_tskMain:Entered[HOST]                                     
    ThreadName:IpcBitsInLink_tskMain_3000001a,ThreadID:780                          
                                                                                    
     [host]  4173: IPC_BITS_IN   : Create in progress !!!                           
                                                                                    
     [host]  4173: IPC_BITS_IN   : ListMPOpen start !!!                             
                                                                                    
     [host]  4173: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_24] ...                 
     4175: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_24] ...                          
                                                                                    
     [host]  4177: IPC_BITS_IN   : ListMPOpen done !!!                              
                                                                                    
     [host]  4177: IPC_BITS_IN   : System_linkGetInfo done !!!                      
                                                                                    
     [host]  4178: IPC_BITS_IN   : Create Done !!!                                  
    [HOST]                                                                          
    ThreadName:IpcBitsInLink_periodicTaskFxn_3000001a,ThreadID:793                  
    pass                                                                            
    ******************************************************                          
     [m3vpss ]  62174: CAPTURE: Start in progress !!!                               
     [m3video] ENCLINK_H264:HEAPID:0        USED:13808                              
     [m3video] ENCLINK_H264:HEAPID:3        USED:3383296                            
     [m3video]  62163: ENCODE: All CH Create ... DONE !!!                           
     [m3video] ENCLINK:HEAPID:0     USED:13928                                      
     [m3video] ENCLINK:HEAPID:2     USED:2764800                                    
     [m3video] ENCLINK:HEAPID:3     USED:3383296                                    
     [m3video]  62165: ENCODE: Create ... DONE !!!                                  
     [m3video]  62165: IPC_BITS_OUT   : Create in progress !!!                      
     [m3video]  62167: IPC_BITS_OUT   : Create Done !!!                             
     [m3vpss ]  62273: CAPTURE: Enabled Time Stamping !!!                           
                                                                                    
     Channel Selected: 0[HOST]                                                      
    ThreadName:Demo_run,ThreadID:777                                                
                                                                                    
     =============                                                                  
     Run-Time Menu                                                                  
     =============                                                                  
                                                                                    
     1: Capture Settings                                                            
     2: Encode  Settings                                                            
     3: Decode  Settings                                                            
     4: Display Settings                                                            
     5: Audio Capture <TVP5158> & Encode <AAC-LC, G711> demo                        
     6: Change Playback Channel <valid only if capture/playback is active>          
     7: Audio encode demo <File In/Out>                                             
     8: Audio decode demo <File In/Out>                                             
                                                                                    
     i: Print detailed system information                                           
     s: Core Status: Active/In-active                                               
     f: Switch IVA Channel Map                                                      
                                                                                    
     e: Stop Demo                                                                   
                                                                                    
     Enter Choice:  [m3vpss ]  62281: CAPTURE: Start Done !!!                       
                                                                                    
    [HOST]                                                                          
    ThreadName:Demo_run,ThreadID:777                                                
                                                                                    
     =============                                                                  
     Run-Time Menu                                                                  
     =============                                                                  
                                                                                    
     1: Capture Settings                                                            
     2: Encode  Settings                                                            
     3: Decode  Settings                                                            
     4: Display Settings                                                            
     5: Audio Capture <TVP5158> & Encode <AAC-LC, G711> demo                        
     6: Change Playback Channel <valid only if capture/playback is active>          
     7: Audio encode demo <File In/Out>                                             
     8: Audio decode demo <File In/Out>                                             
                                                                                    
     i: Print detailed system information                                           
     s: Core Status: Active/In-active                                               
     f: Switch IVA Channel Map                                                      
                                                                                    
     e: Stop Demo                                                                   
                                                                                    
     Enter Choice: i                                                                
                                                                                    
                                                                                    
     [m3vpss ]                                                                      
     [m3vpss ]  *** Capture Driver Advanced Statistics ***                          
     [m3vpss ]                                                                      
     [m3vpss ]  VIP Parser Reset Count : 0                                          
     [m3vpss ]                                                                      
     [m3vpss ]      |   Total    Even     Odd  Total  Even   Odd  Min /  Max  Min /C
     [m3vpss ]  CH  |  Fields  Fields  Fields    FPS   FPS   FPS       Width      H)
     [m3vpss ]  --------------------------------------------------------------------
     [m3vpss ]  000 |     350     350       0     70    70     0 1280 / 1280  720 /)
     [m3vpss ]                                                                      
     [m3vpss ]  VIP Capture Port 0 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescM 
     [m3vpss ]                                                                      
     [m3vpss ]  *** Capture List Manager Advanced Statistics ***                    
     [m3vpss ]                                                                      
     [m3vpss ]  List Post Count        : 731                                        
     [m3vpss ]  List Stall Count       : 0                                          
     [m3vpss ]  List Post Time (ms)    : Max = 0, Min = 0, Avg = 0, Total = 0       
     [m3vpss ]  INTC Timeout Count     : (0, 0) (Min timeout value = 993, 1000)     
     [m3vpss ]  Descriptor miss found count : 0                                     
     [m3vpss ]                                                                      
     [m3vpss ]                                                                      
     [m3vpss ]  VIP and VPDMA registers,                                            
     [m3vpss ]  VIP0 : FIQ_STATUS  : 0x4810551c = 0x00000000                        
     [m3vpss ]  VIP1 : FIQ_STATUS  : 0x48105a1c = 0x00000000                        
     [m3vpss ]  VPDMA: LIST_BUSY   : 0x4810d00c = 0x00100000                        
     [m3vpss ]                                                                      
     [m3vpss ]                                                                      
     [m3vpss ]  68126: CAPTURE: Fields = 349 (fps = 59, CPU Load = 0)               
     [m3vpss ]  68126: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)                 
     [m3vpss ]  68126: SYSTEM  : FREE SPACE : System Heap      = 67984 B, Mbx = 102 
     [m3vpss ]  68126: SYSTEM  : FREE SPACE : SR0 Heap         = 8683520 B (8 MB)   
     [m3vpss ]  68126: SYSTEM  : FREE SPACE : Frame Buffer     = 238064512 B (227 M 
     [m3vpss ]  68126: SYSTEM  : FREE SPACE : Bitstream Buffer = 207998848 B (198 M 
     [m3vpss ]  68127: SYSTEM  : FREE SPACE : Tiler Buffer     = 224 B (0 MB)  - TI 
     [m3vpss ]                                                                      
     [m3vpss ]  *** [NSF0] NSF Statistics ***                                       
     [m3vpss ]                                                                      
     [m3vpss ]  Elasped Time           : 6 secs                                     
     [m3vpss ]  Total Fields Processed : 349                                        
     [m3vpss ]  Total Fields FPS       : 251 FPS                                    
     [m3vpss ]                                                                      
     [m3vpss ]                                                                      
     [m3vpss ]  CH  | In Recv In Reject In Process Out User Out Out                 
     [m3vpss ]  Num | FPS     FPS       FPS        FPS Skip FPS Skip FPS            
     [m3vpss ]  ------------------------------------------------                    
     [m3vpss ]    0 |      58         0         58  58        0        0            
     [m3vpss ]                                                                      
     [m3video]      74128: HDVICP-ID:0                                              
     [m3video] All percentage figures are based off totalElapsedTime                
     [m3video]               totalAcquire2wait :5 %                                 
     [m3video]               totalWait2Isr :29 %                                    
     [m3video]               totalIsr2Done :0 %                                     
     [m3video]               totalWait2Done :29 %                                   
     [m3video]               totalDone2Release :0 %                                 
     [m3video]               totalAcquire2Release :35 %                             
     [m3video]               totalAcq2acqDelay :64 %                                
     [m3video]               totalElapsedTime in msec :   11797                     
     [m3video]               numAccessCnt:     707                                  
     [m3video]              IVA-FPS :      64                                       
     [m3video]              Average time spent per frame in microsec:    4838       
     [m3video]      74129: HDVICP-ID:1                                              
     [m3video] All percentage figures are based off totalElapsedTime                
     [m3video]               totalAcquire2wait :0 %                                 
     [m3video]               totalWait2Isr :0 %                                     
     [m3video]               totalIsr2Done :0 %                                     
     [m3video]               totalWait2Done :0 %                                    
     [m3video]               totalDone2Release :0 %                                 
     [m3video]               totalAcquire2Release :0 %                              
     [m3video]               totalAcq2acqDelay :0 %                                 
     [m3video]               totalElapsedTime in msec :       0                     
     [m3video]               numAccessCnt:       0                                  
     [m3video]              IVA-FPS :       0                                       
     [m3video]              Average time spent per frame in microsec:       0       
     [m3video]      74129: HDVICP-ID:2                                              
     [m3video] All percentage figures are based off totalElapsedTime                
     [m3video]               totalAcquire2wait :0 %                                 
     [m3video]               totalWait2Isr :0 %                                     
     [m3video]               totalIsr2Done :0 %                                     
     [m3video]               totalWait2Done :0 %                                    
     [m3video]               totalDone2Release :0 %                                 
     [m3video]               totalAcquire2Release :0 %                              
     [m3video]               totalAcq2acqDelay :0 %                                 
     [m3video]               totalElapsedTime in msec :       0                     
     [m3video]               numAccessCnt:       0                                  
     [m3video]              IVA-FPS :       0                                       
     [m3video]              Average time spent per frame in microsec:       0       
     [m3video]                                                                      
     [m3video]  *** ENCODE Statistics ***                                           
     [m3video]                                                                      
     [m3video]  Elasped Time           : 11 secs                                    
     [m3video]                                                                      
     [m3video]                                                                      
     [m3video]  CH  | In Recv In Skip In User  Out Latency                          
     [m3video]  Num | FPS     FPS     Skip FPS FPS Min / Max                        
     [m3video]  --------------------------------------------                        
     [m3video]    0 |      63       0        0  63 255 / 58093                      
     [m3video]                                                                      
     [m3video] Multi Channel Encode Average Submit Batch Size                       
     [m3video] Max Submit Batch Size : 24                                           
     [m3video] IVAHD_0 Average Batch Size : 1                                       
     [m3video] IVAHD_0 Max achieved Batch Size : 1                                  
     [m3video] IVAHD_1 Average Batch Size : 0                                       
     [m3video] IVAHD_1 Max achieved Batch Size : 0                                  
     [m3video] IVAHD_2 Average Batch Size : 0                                       
     [m3video] IVAHD_2 Max achieved Batch Size : 0                                  
     [m3video]                                                                      
     [m3video] Multi Channel Encode Batch break Stats                               
     [m3video] Total Number of Batches created: 704                                 
     [m3video] All numbers are based off total number of Batches created            
     [m3video]       Batch breaks due to batch sizeexceeding limit: 0 %             
     [m3video]       Batch breaks due to ReqObj Que being empty: 100 %              
     [m3video]       Batch breaks due to changed resolution class: 0 %              
     [m3video]       Batch breaks due to interlace and progressivecontent mix: 0 %  
     [m3video]       Batch breaks due to channel repeat: 0 %                        
     [m3video]       Batch breaks due to different codec: 0 %                       
     [m3video] Total Number of Batches created: 0                                   
     [m3video] All numbers are based off total number of Batches created            
     [m3video]       Batch breaks due to batch sizeexceeding limit: 0 %             
     [m3video]       Batch breaks due to ReqObj Que being empty: 0 %                
     [m3video]       Batch breaks due to changed resolution class: 0 %              
     [m3video]       Batch breaks due to interlace and progressivecontent mix: 0 %  
     [m3video]       Batch breaks due to channel repeat: 0 %                        
     [m3video]       Batch breaks due to different codec: 0 %                       
     [m3video] Total Number of Batches created: 0                                   
     [m3video] All numbers are based off total number of Batches created            
     [m3video]       Batch breaks due to batch sizeexceeding limit: 0 %             
     [m3video]       Batch breaks due to ReqObj Que being empty: 0 %                
     [m3video]       Batch breaks due to changed resolution class: 0 %              
     [m3video]       Batch breaks due to interlace and progressivecontent mix: 0 %  
     [m3video]       Batch breaks due to channel repeat: 0 %                        
     [m3video]       Batch breaks due to different codec: 0 %                       
     [m3vpss ]                                                                      
     [m3vpss ]  77133: LOAD: CPU: 4.3% HWI: 0.7%, SWI:0.9%                          
     [m3vpss ]                                                                      
     [m3vpss ]  77133: LOAD: TSK: IPC_OUT_M30         : 0.4%                        
     [m3vpss ]  77133: LOAD: TSK: CAPTURE             : 0.4%                        
     [m3vpss ]  77134: LOAD: TSK: NSF0                : 0.9%                        
     [m3vpss ]  77134: LOAD: TSK: MISC                : 1.0%                        
     [m3vpss ]                                                                      
     [m3video]                                                                      
     [m3video]  77634: LOAD: CPU: 4.7% HWI: 0.5%, SWI:0.6%                          
     [m3video]                                                                      
     [m3video]  77634: LOAD: TSK: IPC_IN_M30          : 0.3%                        
     [m3video]  77634: LOAD: TSK: IPC_BITS_OUT0       : 0.5%                        
     [m3video]  77635: LOAD: TSK: ENC0                : 1.1%                        
     [m3video]  77635: LOAD: TSK: ENC_PROCESS_TSK_0   : 1.4%                        
     [m3video]  77635: LOAD: TSK: MISC                : 0.3%                        
     [m3video]                                                                      
     [c6xdsp ]                                                                      
     [c6xdsp ]  77453: LOAD: CPU: 0.2% HWI: 0.0%, SWI:0.0%                          
     [c6xdsp ]                                                                      
     [c6xdsp ]  77453: LOAD: TSK: MISC                : 0.2%                        
     [c6xdsp ]                                                                      
                                                                                    
                                                                                    
     *** Encode Bitstream Received Statistics ***                                   
                                                                                    
     Elased time =   16.4 secs                                                      
                                                                                    
     CH | Bitrate (Kbps) | FPS | Key-frame FPS | Width (max/min) | Height (max/min))
     -------------------------------------------------------------------------------
      0 |        3146.49 | 59.7 |           2.0 |  1280 /   1280 |    720 /    720 5
                                                                                    
     [host]                                                                         
                                                                                    
     *** SCD Frame Results Received Statistics ***                                  
                                                                                    
     Elased time =   20.6 secs                                                      
                                                                                    
     CH | Bitrate (Kbps) | FPS | Width (max/min) | Height (max/min)                 
     -------------------------------------------------------------------------------
    
    

    look forward to your help

    thank you

    dv

  • Hi,

     

    Can you dump the frames from the capture and check if the captured frames are correct? Display is correct, so only if The capture is not capturing frames correctly, it will be a problem.

     

    Regards,

    Brijesh

  • Hi,

     

    It does not look like contrast problem, but it looks like either Cb and Cr are swapped. I am assuming here that the problem here is the the change in the building color. In the previous image, it was red, whereas in the decoder image it is changed. Is this the problem you are facing? What is the format of the capture from the Vip? Is YUV422I or YUV420?

     

    Regards,

    Brijesh

  • Hi,Brijesh

    Yes,you are right,i checked the pr \pr cables and swapped them to the right interface,the right color comed back.

    The output format of the cpature  YUV422I.If i configure the output format as 420sp_uv,the demo stuck at creat capture process.So i use cap-nsf-enc to test the format of captured date.

    The question is :

    1.In the decoded picture,the part which red line point to should be attached to the left part.And the cap-dis demo still can not work.I dont know why the video can be captured,encoded,but  not display?

    2.The decoded image could demonstrate that the capture module captured video with wrong format.Maybe the wrong format video come from TVP7002.My video source is 720p30,but i use the configuration of 720p60 to configure TVP7002.so,how to configure the tvp7002 to 720p30?

    Regards

    dv

  • Hi,

     

    I think display expects YUV422I data format, so with the YUV420 capture format, you cannot connect capture directly to display. You will need to convert YUV420 format to YUV422 using one of the scalar and then connect to display.

    Could you use Linux Driver to get the TVP7002 settings?

     

    Regards,

    Brijesh

  • Hi,Brijesh

    I use this link now:

    cap-nfs-smws-display

    and failed again.

    I had used link as cap(output format is 420sp_uv)-enc ,but stuck at creating capture module.it is strange.

    The tvp7002 driver in v4l2 (tvp7002.c in ezsdk). I found that it don't have 720p30,and its' 720p60 configuration does not as same as my configuration(support by   http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/315097.aspx)

    thank you for giving some guidance.

    Regards

    dv

  • Hi,Brijesh

    Now,i am still confused by “DISPLAY”.

    This time i use dec_dis demo,the HDMI device still shutdown by Powe saving mode.

    how to fix it ?

    Thank you

    dv

  • Hi,

     

    Could you tell what the problem you are facing?

     

    Is the display not displaying 720p30 resolution? or is it capture not capturing 720p30 resolution? or capture link is assrting?

     

    Regards,

    Brijesh

  • Hi,Brijesh

    I am facing the problem about displaying.

    Use the dec-dis demo to decode and display 720p30 h264 file,the HDMI does not output data as cap-dis demo that we talk about before.

    i have ever doubt that the issue was caused by tvp7002 configuration,but it is not.

    and i will shutdown this post and welcome to guide me at the another post:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/328294.aspx

     thank you

    dv