hi, folks
My project is follow xdais(xdm) software architecture.
I try to implement GMM background subtraction with VLIB 2.0 on DM6467. The arm-core operation frequence is 337MHz and C64 processor operation frequency is twice of arm-core. Now I measure the VLIB GMM background subtraction execution time,it seem not good. The resolution of test video sequence is 384x288, it only achieves about 8 fps. The performace is far from real-time requirement. Is it possible to realize real-time background subtraction with VLIB 2.0.