This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSL questions

Anonymous
Anonymous


Hi All,

I would like to ask some questions on chip-suppor library.

There is a Chip-support library for C6000, described in SPRU401J. However,

In both

  1. http://focus.ti.com/docs/toolsw/folders/print/sprc090.html
  2. http://processors.wiki.ti.com/index.php/Chip_support_library

DM6437 or DM6431 are not listed. Does this mean C6000 CSL doesn't support them?

What is the relationship between C6000 and DavinCi chips? If DavinCi chips, in particular, DM6437/6431, are members of the C6000 family/class, why the document titled as "TMS320C6000 Chip Support Library API Reference Guide" doesn't support them?


Another question is that is CSL a must-to-use? Take the instance of I2C controlling for example, my EVM uses functions like:

I2C functions said:


Int16 EVMDM6437_I2C_write( Uint16 i2c_addr, Uint8* data, Uint16 len )
{
Int32 timeout, i;

I2C_ICCNT = len; // Set length
I2C_ICSAR = i2c_addr; // Set I2C slave address
I2C_ICMDR = ICMDR_STT // Set for Master Write
| ICMDR_TRX
| ICMDR_MST
| ICMDR_IRS
| ICMDR_FREE;

_wait( 10 ); // Short delay

for ( i = 0 ; i < len ; i++ )
{
I2C_ICDXR = data[i]; // Write

timeout = i2c_timeout;
do
{
if ( timeout-- < 0 )
{
EVMDM6437_I2C_reset( );
return -1;
}
} while ( ( I2C_ICSTR & ICSTR_ICXRDY ) == 0 );// Wait for Tx Ready
}

I2C_ICMDR |= ICMDR_STP; // Generate STOP

return 0;
}

and

Int16 EVMDM6437_I2C_read( Uint16 i2c_addr, Uint8* data, Uint16 len )
{
Int32 timeout, i;

I2C_ICCNT = len; // Set length
I2C_ICSAR = i2c_addr; // Set I2C slave address
I2C_ICMDR = ICMDR_STT // Set for Master Read
| ICMDR_MST
| ICMDR_IRS
| ICMDR_FREE;

_wait( 10 ); // Short delay

for ( i = 0 ; i < len ; i++ )
{
timeout = i2c_timeout;
do
{
if ( timeout-- < 0 )
{
EVMDM6437_I2C_reset( );
return -1;
}
} while ( ( I2C_ICSTR & ICSTR_ICRRDY ) == 0 );// Wait for Rx Ready

data[i] = I2C_ICDRR; // Read
}

I2C_ICMDR |= ICMDR_STP; // Generate STOP

return 0;
}



They work well and I didn't see any other I2C related code in my projects. Actually, it seems that CSL is entirely missing in all examples but these examples could still work well.


So the question finally is: Do I have to use CSL or not? Ultimately all on-chip peripherals (including I2C) can be configured and controlled by register read/write, therefore programmer's "raw code", as long as correctly written, is sufficient for all purposes. So is CSL provided simply to give some ease of programming to programmers that are not so familiar with the work of register configuration?

In fact, the I2C code in CSL looks to me quite similar to the code in Spectrum's EVM examples:

CSL reset said:

void I2C_reset(I2C_Handle hI2c) {

Uint32 gie;

gie = IRQ_globalDisable();

if (hI2c == INV) {
I2C_reset((I2C_Handle)(&(_I2C_deviceTable[0])));
#if (CHIP_6713 | CHIP_DA610 | CHIP_6413 | CHIP_6418 | CHIP_6410)
I2C_reset((I2C_Handle)(&(_I2C_deviceTable[1])));
#endif
} else {
I2C_RSETH(hI2c,I2COAR,I2C_I2COAR_DEFAULT);
I2C_RSETH(hI2c,I2CIER,I2C_I2CIER_DEFAULT);
I2C_RSETH(hI2c,I2CSTR,I2C_I2CSTR_DEFAULT);
I2C_RSETH(hI2c,I2CCLKL,I2C_I2CCLKL_DEFAULT);
I2C_RSETH(hI2c,I2CCLKH,I2C_I2CCLKH_DEFAULT);
I2C_RSETH(hI2c,I2CCNT,I2C_I2CCNT_DEFAULT);
I2C_RSETH(hI2c,I2CSAR,I2C_I2CSAR_DEFAULT);
I2C_RSETH(hI2c,I2CPSC,I2C_I2CPSC_DEFAULT);
I2C_RSETH(hI2c,I2CDXR,I2C_I2CDXR_DEFAULT);

while(I2C_RGETH(hI2c,I2CISRC)) /* Reading I2CISRC clears the interrupt flag */
;

I2C_RSETH(hI2c,I2CMDR,I2C_I2CMDR_DEFAULT); /* I2C is reset mode IRS=0 */

#if (CHIP_6413 | CHIP_6418 | CHIP_6410)
I2C_RSETH(hI2c,I2CEMDR,I2C_I2CEMDR_DEFAULT);
I2C_RSETH(hI2c,I2CPFUNC,I2C_I2CPFUNC_DEFAULT);
I2C_RSETH(hI2c,I2CPDIR,I2C_I2CPDIR_DEFAULT);
I2C_RSETH(hI2c,I2CPDOUT,I2C_I2CPDOUT_DEFAULT);
#endif
IRQ_reset(hI2c->eventId);
}

IRQ_globalRestore(gie);

return;
}


Spectrum EVM init() and reset() said:

Int16 EVMDM6437_I2C_init( )
{
I2C_ICMDR = 0; // Reset I2C
I2C_ICPSC = 13; // Config prescaler for 27MHz
I2C_ICCLKL = 5; // Config clk LOW for 100 kHz
I2C_ICCLKH = 5; // Config clk HIGH for 100 kHz
I2C_ICMDR |= ICMDR_IRS; // Release I2C from reset
return 0;
}

Int16 EVMDM6437_I2C_reset( )
{
EVMDM6437_I2C_close( );
EVMDM6437_I2C_init( );
return 0;
}


The commonality is that they all configure

  1. ICMDR
  2. ICCLKL, ICCLKH
  3. ICPSC


and the difference is only that CSL are more comprehensive, most likely due to its need to support multiple devices. So can I understand CSL's I2C fun ctions as a generalist's repertoire, and Spectrum EVMDM6437's I2C functions as a specialist's? Therefore as long as I have the EVM's function, there is no need for the CSL. Is this correct?

Does this apply to all CSL functions? Chapter 2-28:
Cache
Chip
...
DMA
...
GPIO
...
I2C
...
PCI
...
VP
...
XBUS
...



Looking forward to answers on this.


Zheng