Hi All,
I would like to ask a question JTAG connection.
In EVM6437, the JTAG return clock signal TCKRET is
1. First connect to mux/demux U539
2. Then connect to the output of OR gate U37
But not connected to DSP.
So in this way it is not used? Then why still connect or even provide it? Why connect it to the output of an OR gate?
Thanks,
Zheng