This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6A8167 (Davinci Processor) HD

Other Parts Discussed in Thread: TVP5158

Customer is interested in the C6a8167 or whatever the highest powered Davinci processor is at this time.  There are many questions about the C6A8167 that needs to be addressed initially:

1) What is the video interface, can we feed hdmi, if not then what (not withstanding tvp700x) for component, we want digital.

2) Can we do 2 simulatneous HD compressions (what res?).

3) Can we do vmux (ie security system Quad screen or split screen).

4) What is the max usb xfer rate.

5) Do you have video libraries for mpeg4/h.264 (is this davinci)

6) Do you have a streaming video server for the Arm

7) How many standard def channels can be input

8) How many standard def compressions can we do at the same time

9) Average power consumption

10) Can we do Dual Analog output?, dual TV outputs (I know it has 3 DACs).

11) How many HD outputs can we do (hdmi?).

12) how much osd ram is available.

13) How fast can the vmux be reconfigured (ie speed to go from SD to HD, Dual to single, etc.)

14) How do we do OSD, is this in sw, are there libs?

15) When the arm isnt doing our SW is idle 100%

16) Is there an fpu on the ARM?

17) Who could we use as an HD camera supplier? What format (hdmi, component)?

18) Is there an internal temp sensor on di.

19) Does fire work for a digital camera?

Thank you.