Hi
I need to implement this fragmented Ethernet frame structure in my project (with customized fragment size). But when i give the descriptor as in fragment 1 (SOP,OWNER) & fragment packet (OWNER) &End of fragment (EOP,OWNER) MACSTATUS is showing SOP error and TX0PEND is not showing HIGH. How can i solve this issue to send a fragment frame in EMAC. Single fragment frames are transmitting correctly with the descriptor i initialized. I didn't find any examples from TI on fragmented memory transmission in BSL or NDK's.
I also have doubts like;
1. whether the linked list should be initialized before transmitting the frames?
2. As in the pic, is there any need to send a non fragmented frames before and after fragmented frames?
I request someones help to solve this issue. Kindly use this post also
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/207730.aspx
Thank you