I'm hoping someone from TI can
a) confirm, from first hand knowledge, that the AM1808 does support USB host (mass storage) in 03.22, with USB2.0
b) explain how to enable USB2.0 in mass storage mode
Using the older 03_20 PSP we have been successful in getting USB2.0 operational in host mode, using a USB attached hard drive.
However on the 03_22 PSP we are not successful in attaching a USB2.0 hard disk - again using the LogicPD devboard (which was modified with the register 133, pulled low, and the type A connector). This board functions correctly with the 03_20 PSP. USB1.1 does operate as it did in 03_20, using the second 1.1 connector on the LogicPD.
to recap
a) we need USB2.0 in host mode on the 03_22 PSP, the stock uImage does not have an operational USB stack
b) we need USB 2.0 host, with mass storage
c) we are seeing regressions between 03_20 and 03_22 PSP
d) the wiki is out of date, referencing components that were deprecated between 03_20 and 03_22. further the wiki asks for mutually exclusive components to be selected
I'm growing stressed as this problem has been circling the community for some weeks and I need to sign off on the AM1808 before a production run
my read is that since OTG is not supported that host and gadget are mutually exclusive - however gadget must checked in the config, but "USB Peripheral Controller" needs to be a module? I posted a similar question here, but feedback isnt accurate. http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/246174.aspx
The wiki that is confusing me so badly :)
can I get some guidance - I *think* I need to enable Gadget support? however if I do this the Inventra needed for host disappear? how can this be if host and gadget are mutually exclusive?