Hi everyone !
I am using C6748LCDK
Can I use SPI0 following the pins: SIMO,SOMI,CLK and SCSn_4 (chip selection) ?.
I doubt that SCSn_4 is used for UART0_TX.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Phi tu1,
Thanks for the post.
Please download the schematics of C6748 LCDK from below link. (Download the corresponding Version)
http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_(LCDK)#Online_Resources
Phi tu1: said:Can I use SPI0 following the pins: SIMO,SOMI,CLK and SCSn_4 (chip selection) ?.
I doubt that SCSn_4 is used for UART0_TX.
From my understanding the usage of SPI0 pins as follows. I am referring to Ver. A6
SPI0_CLK/EPWM0_A/MII_RXCLK - SPIO_CLK (J15)
SPI0_SOMI/EPWM0_SYNCI/MII_RXERR - SPIO_SOMI (J15)
SPI0_SIMO/EPWM0_SYNCO/MII_CRS - SPIO_SIMO (J15)
SPI0_ENAn/EPWM0_B/MII_RXDV - SPIO_ENAn (J15)
SPI0_SCSn_4/UART0_TXD/MII_RXD2 - UART0_TX (J15)
SPI0_SCSn_5/UART0_RXD/MII_RXD3 - UART0_RX (J15)
The SPI0 pins are not connected to J15 because the resistors for connection are not populated. The Ethernet chip used those pins. You will need to make some HW changes and maybe power down the Ethernet chip. A discussion here:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/234899.aspx