I've some questions about wakeup the DSP
1. I'd like to wakeup DSP without DSPLINK / C6run, so I follow the <System Ref Guide > and write a linux driver.
But I faild on step 7 : Wait for the STATE bit field in the DSP LPSC module status register (PSC0.MDSTAT15) to change to 3h.
2. How to complile a DSP program, Use CCS? Do I need to convert the out file to bin file? How to?
3. Can I let dsp run in its inner ram, not DDR? Edit the CCS cmd file?