We currently have the AM3517 evaluation module which uses the WL1271 with the Bluetooth PCM connected to the McBSP port. There is a lot of discussion about the McBSP...probably because everyone is using this reference design.
However, we are planning to use the new AM3874 which has only 1 McBSP port. I am trying to make a board with two modular connectors for bluetooth or other audio applications (that can be used simulataneously). Is it possible to do the same thing (PCM / AC97) using the McASP port?
More importantly, what are the key differences between McASP and McBSP? Is it just the built-in buffering on the McBSP? I can't find a clear comparison on the two modules.