This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X SD card - speed class and size supported



Hi All,

We are going to use the MMC0 to boot the system using a SD card.

The AM335X manual mention in chapter 18:

"- SD Host Controller Standard Specification sets as defined in the SD card specification Part A2
v2.00

- up to 192Mbit/sec (24MByte/sec) in High-Speed SD mode 4-bit data transfer

- up to 24Mbit/sec (3MByte/sec) in Default SD mode 1-bit data transfer"

The SD card specification explains the speed classes and respective read speed (MB/s).

Our design will use a 4-bit SD card.

Does anyone know:

- Which is the highest SD speed class supported ?

- What is the size limit supported for a SD card?   (consider AM335X and linux kernel limits)

Thanks

Rodrigo