Hi,
I'm running Version 1.00 of C55BootImage.exe to create a secure boot image so I can boot from an SD Card on my custom C5515 platform. It's working fine (booting an app off the SD Card), but I want to insert some pre-bootloader register configuration information. What is the exact format required for the registers file? I've created a file with the same format as HEX55 ( -reg_config 0xXXXX,0xXXXX) but when I look at the generated .bin file (word 15) the number of registers to configure is zero whatever I try. Any suggestions?
Also, the application I have successfully booting is purely in on-chip memory. The application I'm trying to get to boot also uses off-chip memory, so I'm trying to get the EMIF configuration registers configured with the pre-bootloader configuration (my problem above)... should I be able to do this? (My external to load into is 16 bit wide on CS2 which is what I'm trying to pre-bootloader configure)
Many thanks,
Dave