Hi TI engineers & friends,
I have the board TMS320C5535 eZdsp USB kit come with default Connected Audio Framework installed in the memory stick, when I plug the board into my computer, it throws out a message "This device can perform faster if it was connected to a high speed USB 2.0". However I am sure that all the ports in my computer are USB 2.0, I also tried on another computers as well but no luck at all. This made it a big problem for me since I have another application that need to operate in Hi-speed mode but I cannot manage to do it.
Does anyone have any idea on this?
Thank you very much!