hi everybody,
I am trying to implement audio in/out using mcbsp in ccs 3.1 first, i initialized codec, and set freq, and read data's through mcbsp. But, i am unable to hear my voice. the code is,
#include "imagescfg.h"
#include "dsk6713.h"
#include "dsk6713_aic23.h"
DSK6713_AIC23_Config config={0x0017,0x0017,0x00d8,0x00d8,0x0000,0x0000,0x0011,0x0043,0x0081,0x0001};
/*void main()
{
DSK6713_AIC23_CodecHandle hcodec;
int l_input,r_input,l_output,r_output;
DSK6713_init();
hcodec = DSK6713_AIC23_openCodec(0, &config);
DSK6713_AIC23_setFreq=DSK6713_AIC23_Freq_48KHZ;
while(1)
{
while(!DSK6713_AIC23_read(hcodec,&l_input));
while(!DSK6713_AIC23_read(hcodec,&r_input));
r_output=r_input;
l_output=l_input;
while(!DSK6713_AIC23_write(hcodec,l_output));
while(!DSK6713_AIC23_write(hcodec,r_output));
}
DSK6713_AIC23_closeCodec(hcodec);
}
also, what configuration. is that right or need to modify? please, suggest some ideas friends.
suggestions will be greatful.
regards,
chinny