Hey,
I mounted VM3224K daughter card on 6713 and loaded the example program using CCS V3.3 PLATINUM VERSION. But I cant see any display!
Please tell me what are necessary steps needed to get output on LCD screen of VM3224K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey,
I mounted VM3224K daughter card on 6713 and loaded the example program using CCS V3.3 PLATINUM VERSION. But I cant see any display!
Please tell me what are necessary steps needed to get output on LCD screen of VM3224K
Naveen,
With the VM3224K board removed from the DSK6713, can you build, load, and run example programs that came with the DSK6713?
If you do not have any of those, you can go to the DSK board manufacturer's website www.spectrumdigital.com and find the support page for the DSK6713. Or you can go to the TI Wiki Pages and search for "c6713 workshop" (no quotes) to find the C6x1x workshop that includes some labs you can run while learning to use this board.
Once you have run some of those example programs to confirm that the DSK6713 board is working properly, please contact the manufacturer of the VM3224K board for help with using the VM3224K board.
Regards,
RandyP
Naveen,
If you have done sufficient testing on the DSK6713 to convince yourself that the DSK6713 is operating correctly when the VM3224K is not connected, then you need to contact the VM3224K board vendor for further support.
If you suspect problems with the DSK6713 board, then try your test with the VM3224K connected to a different DSK6713, if you have another available.
Regards,
RandyP