This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART implementation using McBSP and EDMA



I have been implementing UART on 6713DSK in SPI mode.For this I used the sample code in spra633c as reference.The steps involved are as follows

-
1)Enable CSl
2)Enable interrupts and set SRGR
3)Config McBSP
4)Enable EDMA channels
5)transmit data (this fills the recvbuf array)
6)enable McBSP as a receiver
7)enable McBSP as a transmitter
8)enable Fsync
9)data transfer starts
10)close EDMA

When i run the program, the value stored in xmitbuf is correct but that stored in recvbuf is random and changes with each run. I want to know why this occurs and how to solve it. i.e. how to allign both the arrays?? Plz do help , i am stuck with this for a month now.
Thanx.

  • my working code is as follows -

    #define CHIP_6713 1

    /* Include files */
    #include "xyzcfg.h"
    #include <c6713.h>
    #include <csl.h>  
    #include <csl_mcbsp.h>           
    #include <csl_edma.h>
    #include <csl_dma.h>
    #include <csl_irq.h>
    #include <stdio.h>
     
    /* Create buffers and aligning them on an L2 cache line boundary. */
    #pragma DATA_SECTION(xmitbuf,"xmit_buf");
    #pragma DATA_ALIGN(xmitbuf,16);
    unsigned short xmitbuf[0x0400];   

    #pragma DATA_SECTION(recvbuf,"recv_buf");
    unsigned short recvbuf[0x0400];       
    #pragma DTA_ALIGN(recvbuf,16);
    /* Definitions    */
    #define BUFFER_SIZE    2                /* total number of UART data words    */
    #define TRUE 1
    #define FALSE 0

    /* Declare CSL objects */
    MCBSP_Handle hMcbsp1;            /* handle for McBSP1  */
    #if (EDMA_SUPPORT)
        EDMA_Handle hEdma14;            /* handle for EDMA 14 */
        EDMA_Handle hEdma15;            /* handle for EDMA 15 */
    #endif
    #if (DMA_SUPPORT)
        DMA_Handle hDma1;                /* handle for DMA 1 */
        DMA_Handle hDma2;                /* handle for DMA 2 */
    #endif 



    /* Global Variables    */
    volatile int receive_done = FALSE;
    volatile int transmit_done = FALSE;
    char xmit_msg[BUFFER_SIZE] = "M";
    char recv_msg[BUFFER_SIZE] = "T";

    /* Include the vector table to call the IRQ ISRs hookup */
    extern far void vectors();

    /* Prototypes    */
    void ConfigMcBSP(void);
    void ConfigEDMA(void);
    void ConfigDMA(void);
    void ProcessTransmitData(void);
    void ProcessReceiveData(void);
    short VoteLogic(unsigned short);
    int CheckTestCase(void);
    interrupt void c_int11(void);
    interrupt void c_int09(void);
    interrupt void c_int08(void);


    /*******************************************************************/
    /* void main(void)                                                 */
    /*******************************************************************/
    void main(void)
    {
        int i;
        int waittime = 0;
        int works = FALSE;
       
        /* initialize the CSL library */
        CSL_init();

        /* Setup for McBSP */
        ConfigMcBSP();               
       
        /* enable NMI and GI */
        //IRQ_nmiEnable();
        //IRQ_globalEnable();

        /* Start Sample Rate Generator: set /GRST = 1 */
        MCBSP_enableSrgr(hMcbsp1);

        /* inserted wait time for McBSP to get ready */
        for (waittime=0; waittime<0xF; waittime++);

       
        /* point to the IRQ vector table */
        IRQ_setVecs(vectors);

        #if (EDMA_SUPPORT)   
       
            /* disable and clear the event interrupt */
            //IRQ_reset(IRQ_EVT_EDMAINT);        new del
       
            /* clear Parameter RAM of EDMA */
            EDMA_clearPram(0x00000000);
            set_interrupts_edma();             // new add
           
        #endif
       
        #if (DMA_SUPPORT)
       
            DMA_reset(INV);
           
        #endif
       
        ProcessTransmitData();  
      
        #if (EDMA_SUPPORT)   
       
            /* Open the EDMA channels - EDMA 14 for transmit, EDMA 15 for receive    */
            hEdma14 = EDMA_open(EDMA_CHA_XEVT1, EDMA_OPEN_RESET);
            hEdma15 = EDMA_open(EDMA_CHA_REVT1, EDMA_OPEN_RESET);
           
        #endif

        #if (DMA_SUPPORT)
       
            /* Open the DMA channels - DMA 1 for transmit, DMA 2 for receive */
            hDma1 = DMA_open(DMA_CHA1, DMA_OPEN_RESET);
            hDma2 = DMA_open(DMA_CHA2, DMA_OPEN_RESET);
           
        #endif           
       
        /* Open the McBSP channel 1 */
        hMcbsp1 = MCBSP_open(MCBSP_DEV1, MCBSP_OPEN_RESET);
       
        #if (EDMA_SUPPORT)
           
            /* Configure the EDMA channels */
            ConfigEDMA();
       
            /* enable EDMA-CPU interrupt tied to McBSP */
            //IRQ_enable(IRQ_EVT_EDMAINT);
       
           
            /* Enable EDMA channels */
            EDMA_enableChannel(hEdma14);
            EDMA_enableChannel(hEdma15);

        #endif

        #if (DMA_SUPPORT)
       
            /* Configure the DMA channels */
            ConfigDMA();
           
            IRQ_disable(IRQ_EVT_DMAINT1);
            IRQ_disable(IRQ_EVT_DMAINT2);
           
            IRQ_clear(IRQ_EVT_DMAINT1);
            IRQ_clear(IRQ_EVT_DMAINT2);
           
            IRQ_enable(IRQ_EVT_DMAINT1);
            IRQ_enable(IRQ_EVT_DMAINT2);
           
            DMA_start(hDma1);            /*start DMA channel 1*/                           
            DMA_start(hDma2);            /*start DMA channel 2*/
           
        #endif
       
        /* Wake up the McBSP as transmitter and receiver */     
        MCBSP_enableRcv(hMcbsp1);
        MCBSP_enableXmt(hMcbsp1);

        MCBSP_enableFsync(hMcbsp1);
       
        while(!receive_done|| !transmit_done);
       
           
           /* Check to make sure the test case works */
        works = CheckTestCase();
       
        if (works != 0)
         printf("\nTransmission Error....\n");
        else
        printf("\nReceived data matched transmitted data!\n");
                       
        /* process received data */
        printf("Processing Receive string...\n");
       
        ProcessReceiveData();
           
        #if (EDMA_SUPPORT)
       
            //IRQ_disable(IRQ_EVT_EDMAINT);
            //EDMA_RSET(CIER, 0x0);
       
        #endif
       
        #if (DMA_SUPPORT)
       
            IRQ_disable(IRQ_EVT_DMAINT1);
            IRQ_disable(IRQ_EVT_DMAINT2);
           
        #endif
       
        MCBSP_close(hMcbsp1);    /* close McBSP 1 */
       
        #if (EDMA_SUPPORT)
       
            EDMA_close(hEdma14);    /* close EDMA 14 */
            EDMA_close(hEdma15);    /* close EDMA 15 */
       
        #endif   
       
        #if (DMA_SUPPORT)
       
            DMA_close(hDma1);    /* close DMA 1 */
            DMA_close(hDma2);    /* close DMA 2 */
       
        #endif
    }    /* End of main() */
      
             
    /*******************************************************************/
    /* void ConfigEDMA(void): set up EDMA channel 14/15 for UART Xmit  */
    /*******************************************************************/
    #if (EDMA_SUPPORT)

    void ConfigEDMA(void)
    {
        EDMA_configArgs(hEdma14,

            /* OPT Setup */   
            #if (C64_SUPPORT)
                  EDMA_OPT_RMK(
                 EDMA_OPT_PRI_HIGH,        /* 1  */
                 EDMA_OPT_ESIZE_16BIT,            /* 01 */
                    EDMA_OPT_2DS_NO,        /* 0  */
                    EDMA_OPT_SUM_INC,        /* 01 */
                    EDMA_OPT_2DD_NO,        /* 0  */
                    EDMA_OPT_DUM_NONE,        /* 00 */
                    EDMA_OPT_TCINT_YES,        /* 1  */
                    EDMA_OPT_TCC_OF(14),            /* 14 */
                EDMA_OPT_TCCM_DEFAULT,             /* 0  */
                EDMA_OPT_ATCINT_DEFAULT,        /* 0  */
                EDMA_OPT_ATCC_DEFAULT,             /* 0  */
                EDMA_OPT_PDTS_DEFAULT,             /* 0  */
                EDMA_OPT_PDTD_DEFAULT,             /* 0  */
                EDMA_OPT_LINK_NO,        /* 0  */
                    EDMA_OPT_FS_NO            /* 0  */
                  ),
              #else
                  EDMA_OPT_RMK(
                 EDMA_OPT_PRI_HIGH,        /* 1  */
                 EDMA_OPT_ESIZE_16BIT,            /* 01 */
                    EDMA_OPT_2DS_NO,        /* 0  */
                    EDMA_OPT_SUM_INC,        /* 01 */
                    EDMA_OPT_2DD_NO,        /* 0  */
                    EDMA_OPT_DUM_NONE,        /* 00 */
                    EDMA_OPT_TCINT_YES,        /* 1  */
                    EDMA_OPT_TCC_OF(14),            /* 14 */
                    EDMA_OPT_LINK_NO,        /* 0  */
                    EDMA_OPT_FS_NO            /* 0  */
                  ),         
              #endif
           
            /* SRC Setup */             
            EDMA_SRC_RMK((Uint32) xmitbuf),        /*xmitbuf address*/
           
            /* CNT Setup */
            EDMA_CNT_RMK(
                EDMA_CNT_FRMCNT_DEFAULT,
                EDMA_CNT_ELECNT_OF(BUFFER_SIZE*11)
            ),
           
            /* DST Setup */
            EDMA_DST_RMK(MCBSP_getXmtAddr(hMcbsp1)),
           
            /* IDX Setup */
              EDMA_IDX_RMK(0,0),
             
              /* RLD Setup */
              EDMA_RLD_RMK(0,0)
            );

        EDMA_configArgs(hEdma15,
           
            /* OPT Setup */
            #if (C64_SUPPORT)
                EDMA_OPT_RMK(
                 EDMA_OPT_PRI_HIGH,        /* 1  */
                 EDMA_OPT_ESIZE_16BIT,            /* 01 */
                    EDMA_OPT_2DS_NO,        /* 0  */
                    EDMA_OPT_SUM_NONE,        /* 00 */
                    EDMA_OPT_2DD_NO,        /* 0  */
                    EDMA_OPT_DUM_INC,        /* 01 */
                    EDMA_OPT_TCINT_YES,        /* 1  */
                    EDMA_OPT_TCC_OF(15),            /* 15 */
                EDMA_OPT_TCCM_DEFAULT,             /* 0  */
                EDMA_OPT_ATCINT_DEFAULT,        /* 0  */
                EDMA_OPT_ATCC_DEFAULT,             /* 0  */
                EDMA_OPT_PDTS_DEFAULT,             /* 0  */
                EDMA_OPT_PDTD_DEFAULT,             /* 0  */
                    EDMA_OPT_LINK_NO,        /* 0  */
                    EDMA_OPT_FS_NO            /* 0  */
                  ),
              #else
                EDMA_OPT_RMK(
                 EDMA_OPT_PRI_HIGH,            /* 1  */
                 EDMA_OPT_ESIZE_16BIT,            /* 01 */
                    EDMA_OPT_2DS_NO,        /* 0  */
                    EDMA_OPT_SUM_NONE,        /* 00 */
                    EDMA_OPT_2DD_NO,        /* 0  */
                    EDMA_OPT_DUM_INC,        /* 01 */
                    EDMA_OPT_TCINT_YES,        /* 1  */
                    EDMA_OPT_TCC_OF(15),            /* 15 */
                    EDMA_OPT_LINK_NO,        /* 0  */
                    EDMA_OPT_FS_NO            /* 0  */
                  ),
               #endif
             
              /* SRC Setup */
              EDMA_SRC_RMK(MCBSP_getRcvAddr(hMcbsp1)),
             
              /* CNT Setup */
              EDMA_CNT_RMK(0, (BUFFER_SIZE * 11)),
             
              /* DST Setup */
              EDMA_DST_RMK((Uint32) recvbuf),        /*recvbuf address*/
             
              /* IDX Setup */
              EDMA_IDX_RMK(0,0),
             
              /* RLD Setup */
              EDMA_RLD_RMK(0,0)
        );
               
    } /* End of ConfigEDMA() */

    #endif


    /*******************************************************************/
    /* void ConfigDMA(void): set up DMA channels 1 & 2 for UART Xmit   */
    /*******************************************************************/
    #if (DMA_SUPPORT)

    void ConfigDMA(void)
    {
     
        DMA_configArgs(hDma1,
                
            /* PRICTL Setup */
            DMA_PRICTL_RMK(
                DMA_PRICTL_DSTRLD_NONE,
                DMA_PRICTL_SRCRLD_NONE,
                DMA_PRICTL_EMOD_HALT,
                DMA_PRICTL_FS_DISABLE,
                DMA_PRICTL_TCINT_ENABLE,
                DMA_PRICTL_PRI_DMA,
                DMA_PRICTL_WSYNC_XEVT1,
                DMA_PRICTL_RSYNC_NONE,
                DMA_PRICTL_INDEX_NA,
                DMA_PRICTL_CNTRLD_NA,
                DMA_PRICTL_SPLIT_DISABLE,
                DMA_PRICTL_ESIZE_16BIT,
                DMA_PRICTL_DSTDIR_NONE,
                DMA_PRICTL_SRCDIR_INC,
                DMA_PRICTL_START_STOP
            ),

            /* SECCTL Setup */
            DMA_SECCTL_RMK(
                DMA_SECCTL_WSPOL_ACTIVEHIGH,
                DMA_SECCTL_RSPOL_ACTIVEHIGH,
                DMA_SECCTL_FSIG_NORMAL,
                DMA_SECCTL_DMACEN_FRAMECOND,
                DMA_SECCTL_WSYNCCLR_NOTHING,   
                DMA_SECCTL_WSYNCSTAT_CLEAR,    
                DMA_SECCTL_RSYNCCLR_NOTHING,    
                DMA_SECCTL_RSYNCSTAT_CLEAR,       
                DMA_SECCTL_WDROPIE_DISABLE,
                DMA_SECCTL_WDROPCOND_CLEAR,    
                DMA_SECCTL_RDROPIE_DISABLE,
                DMA_SECCTL_RDROPCOND_CLEAR,       
                DMA_SECCTL_BLOCKIE_ENABLE,        /* BLOCK IE=1: enables DMA channel int */
                DMA_SECCTL_BLOCKCOND_CLEAR,
                DMA_SECCTL_LASTIE_DISABLE,
                DMA_SECCTL_LASTCOND_CLEAR,       
                DMA_SECCTL_FRAMEIE_DISABLE,
                DMA_SECCTL_FRAMECOND_CLEAR,       
                DMA_SECCTL_SXIE_DISABLE,
                DMA_SECCTL_SXCOND_CLEAR           
            ),

            /* SRC Setup */
            DMA_SRC_RMK((Uint32) xmitbuf),                /*xmitbuf*/

            /* DST Setup */
            DMA_DST_RMK(MCBSP_getXmtAddr(hMcbsp1)),        /*McBSP DXR */
           
            /* XFRCNT Setup */
            DMA_XFRCNT_RMK(
                DMA_XFRCNT_FRMCNT_OF(1),
                DMA_XFRCNT_ELECNT_OF(BUFFER_SIZE*11)
            )

        );        
               
        DMA_configArgs(hDma2,
           
            /* PRICTL Setup */
            DMA_PRICTL_RMK(
                DMA_PRICTL_DSTRLD_NONE,
                DMA_PRICTL_SRCRLD_NONE,
                DMA_PRICTL_EMOD_HALT,
                DMA_PRICTL_FS_DISABLE,
                DMA_PRICTL_TCINT_ENABLE,
                DMA_PRICTL_PRI_DMA,
                DMA_PRICTL_WSYNC_NONE,
                DMA_PRICTL_RSYNC_REVT1,
                DMA_PRICTL_INDEX_NA,
                DMA_PRICTL_CNTRLD_NA,
                DMA_PRICTL_SPLIT_DISABLE,
                DMA_PRICTL_ESIZE_16BIT,
                DMA_PRICTL_DSTDIR_INC,
                DMA_PRICTL_SRCDIR_NONE,
                DMA_PRICTL_START_STOP
            ), 

            /* SECCTL Setup */
            DMA_SECCTL_RMK(
                DMA_SECCTL_WSPOL_ACTIVEHIGH,
                DMA_SECCTL_RSPOL_ACTIVEHIGH,
                DMA_SECCTL_FSIG_NORMAL,
                DMA_SECCTL_DMACEN_FRAMECOND,
                DMA_SECCTL_WSYNCCLR_NOTHING,   
                DMA_SECCTL_WSYNCSTAT_CLEAR,    
                DMA_SECCTL_RSYNCCLR_NOTHING,    
                DMA_SECCTL_RSYNCSTAT_CLEAR,       
                DMA_SECCTL_WDROPIE_DISABLE,
                DMA_SECCTL_WDROPCOND_CLEAR,    
                DMA_SECCTL_RDROPIE_DISABLE,
                DMA_SECCTL_RDROPCOND_CLEAR,       
                DMA_SECCTL_BLOCKIE_ENABLE,        /* BLOCK IE=1: enables DMA channel int */
                DMA_SECCTL_BLOCKCOND_CLEAR,
                DMA_SECCTL_LASTIE_DISABLE,
                DMA_SECCTL_LASTCOND_CLEAR,       
                DMA_SECCTL_FRAMEIE_DISABLE,
                DMA_SECCTL_FRAMECOND_CLEAR,       
                DMA_SECCTL_SXIE_DISABLE,
                DMA_SECCTL_SXCOND_CLEAR           
            ),                                       
                                
            /* SRC Setup */
            DMA_SRC_RMK(MCBSP_getRcvAddr(hMcbsp1)),        /*McBSP DRR */
           
            /* DST Setup */
            DMA_DST_RMK((Uint32) recvbuf),              /*recvbuf*/

            /* XFRCNT Setup */
            DMA_XFRCNT_RMK(
                DMA_XFRCNT_FRMCNT_OF(1),
                DMA_XFRCNT_ELECNT_OF(BUFFER_SIZE*11)
            )
           
        );        
               
    } /* End of ConfigDMA() */

    #endif
             
    /*******************************************************************/
    /* void ConfigMcBSP(void): Setup for McBSP Configuration           */
    /*******************************************************************/
    void ConfigMcBSP(void)
    {

        MCBSP_Config mcbspCfg1 = {
           
            /* SPCR Setup */
            #if (DMA_SUPPORT)
                MCBSP_SPCR_RMK(       
                    MCBSP_SPCR_FRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_GRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_XINTM_XRDY,            /* 00 */
                    MCBSP_SPCR_XSYNCERR_DEFAULT,            /* 0  */
                    MCBSP_SPCR_XRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_DLB_OFF,            /* 0  */
                    MCBSP_SPCR_RJUST_RZF,            /* 00 */
                    MCBSP_SPCR_CLKSTP_DISABLE,        /* 0x */
                    MCBSP_SPCR_RINTM_RRDY,            /* 00 */
                    MCBSP_SPCR_RSYNCERR_DEFAULT,            /* 0  */
                    MCBSP_SPCR_RRST_DEFAULT            /* 0  */
                ),
            #endif
            #if (EDMA_SUPPORT)
                MCBSP_SPCR_RMK(   
                    MCBSP_SPCR_FREE_YES,            /* 1  */
                    MCBSP_SPCR_SOFT_DEFAULT,        /* 0  */   
                    MCBSP_SPCR_FRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_GRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_XINTM_XRDY,            /* 00 */
                    MCBSP_SPCR_XSYNCERR_DEFAULT,            /* 0  */
                    MCBSP_SPCR_XRST_DEFAULT,        /* 0  */
                    MCBSP_SPCR_DLB_OFF,            /* 0  */
                    MCBSP_SPCR_RJUST_RZF,            /* 00 */
                    MCBSP_SPCR_CLKSTP_DISABLE,        /* 0  */
                    MCBSP_SPCR_DXENA_OFF,            /* 0  */
                    MCBSP_SPCR_RINTM_RRDY,            /* 00 */
                    MCBSP_SPCR_RSYNCERR_DEFAULT,            /* 0  */
                    MCBSP_SPCR_RRST_DEFAULT            /* 0  */
                ),
            #endif
           
            /* RCR Setup */   
            #if (DMA_SUPPORT)
                MCBSP_RCR_RMK(
                    MCBSP_RCR_RPHASE_DUAL,            /* 1     */
                    MCBSP_RCR_RFRLEN2_OF(1),        /* 00010 */
                    MCBSP_RCR_RWDLEN2_8BIT,            /* 000     */
                    MCBSP_RCR_RCOMPAND_MSB,            /* 00     */
                    MCBSP_RCR_RFIG_YES,            /* 1     */
                    MCBSP_RCR_RDATDLY_1BIT,            /* 01     */
                    MCBSP_RCR_RFRLEN1_OF(8),        /* 01000 */
                    MCBSP_RCR_RWDLEN1_16BIT            /* 010     */
                ),
              #endif
            #if (EDMA_SUPPORT)
                MCBSP_RCR_RMK(
                    MCBSP_RCR_RPHASE_DUAL,            /* 1     */
                    MCBSP_RCR_RFRLEN2_OF(1),        /* 00010 */
                    MCBSP_RCR_RWDLEN2_8BIT,            /* 000     */
                    MCBSP_RCR_RCOMPAND_MSB,            /* 00     */
                    MCBSP_RCR_RFIG_YES,            /* 1     */
                    MCBSP_RCR_RDATDLY_1BIT,            /* 01     */
                    MCBSP_RCR_RFRLEN1_OF(8),        /* 01000 */
                    MCBSP_RCR_RWDLEN1_16BIT,        /* 010     */
                    MCBSP_RCR_RWDREVRS_DISABLE         /* 0     */   
                ),
              #endif
         
              /* XCR Setup */
              #if (DMA_SUPPORT)
                  MCBSP_XCR_RMK(
                    MCBSP_XCR_XPHASE_DUAL,            /* 1     */
                    MCBSP_XCR_XFRLEN2_OF(1),        /* 00010 */   
                MCBSP_XCR_XWDLEN2_8BIT,            /* 000     */
                MCBSP_XCR_XCOMPAND_MSB,            /* 00     */
                MCBSP_XCR_XFIG_YES,            /* 1     */
                MCBSP_XCR_XDATDLY_0BIT,            /* 00     */
                MCBSP_XCR_XFRLEN1_OF(8),        /* 01000 */
                MCBSP_XCR_XWDLEN1_16BIT            /* 010     */
                ),
            #endif
              #if (EDMA_SUPPORT)
                  MCBSP_XCR_RMK(
                    MCBSP_XCR_XPHASE_DUAL,            /* 1     */
                    MCBSP_XCR_XFRLEN2_OF(1),        /* 00010 */   
                MCBSP_XCR_XWDLEN2_8BIT,            /* 000     */
                MCBSP_XCR_XCOMPAND_MSB,            /* 00     */
                MCBSP_XCR_XFIG_YES,            /* 1     */
                MCBSP_XCR_XDATDLY_0BIT,            /* 00     */
                MCBSP_XCR_XFRLEN1_OF(8),        /* 01000 */
                MCBSP_XCR_XWDLEN1_16BIT,        /* 010     */
            MCBSP_XCR_XWDREVRS_DISABLE        /* 0     */
                ),
            #endif
                   
            /* SRGR Setup */   
            MCBSP_SRGR_RMK(
                MCBSP_SRGR_GSYNC_FREE,                /* 0      */
                MCBSP_SRGR_CLKSP_RISING,            /* 0      */       
                MCBSP_SRGR_CLKSM_INTERNAL,            /* 1      */
                MCBSP_SRGR_FSGM_DXR2XSR,            /* 0       */
                MCBSP_SRGR_FPER_DEFAULT,            /* 0      */
                MCBSP_SRGR_FWID_DEFAULT,            /* 0      */
     //            MCBSP_SRGR_CLKGDV_OF(40)            /* CLKGDV */
                 MCBSP_SRGR_CLKGDV_OF(731)            /* CLKGDV */            
              ),
           
            /* MCR Setup */
              MCBSP_MCR_DEFAULT,                      /* default values */

            /* RCER Setup */
            #if (C64_SUPPORT)
                MCBSP_RCERE0_DEFAULT,
                MCBSP_RCERE1_DEFAULT,
                MCBSP_RCERE2_DEFAULT,
                MCBSP_RCERE3_DEFAULT,
            #else   
                  MCBSP_RCER_DEFAULT,                     /* default values */
            #endif
           
            /* XCER Setup */
            #if (C64_SUPPORT)
                MCBSP_XCERE0_DEFAULT,
                MCBSP_XCERE1_DEFAULT,
                MCBSP_XCERE2_DEFAULT,
                MCBSP_XCERE3_DEFAULT,
            #else
                  MCBSP_XCER_DEFAULT,                     /* default values */
            #endif
           
            /* PCR Setup */
              MCBSP_PCR_RMK(
                MCBSP_PCR_XIOEN_SP,                /* 0 */
                MCBSP_PCR_RIOEN_SP,                /* 0 */
                MCBSP_PCR_FSXM_INTERNAL,            /* 1 */
                MCBSP_PCR_FSRM_EXTERNAL,            /* 0 */
                MCBSP_PCR_CLKXM_OUTPUT,                /* 1 */
                MCBSP_PCR_CLKRM_OUTPUT,                /* 1 */
                MCBSP_PCR_CLKSSTAT_0,                /* 0 */
                MCBSP_PCR_DXSTAT_0,                /* 0 */
                MCBSP_PCR_FSXP_ACTIVELOW,            /* 1 */
                MCBSP_PCR_FSRP_ACTIVELOW,            /* 1 */
                MCBSP_PCR_CLKXP_RISING,                /* 0 */
            MCBSP_PCR_CLKRP_FALLING                /* 0 */
            )
        };
       
        MCBSP_config(hMcbsp1, &mcbspCfg1);
       
    }    /* end of Config_McBSP(void) */



    /*******************************************************************/
    /* void ProcessTransmitData(void)                                  */
    /*                                                                 */
    /* This function expands each of the 8-bit ASCII characters in the */
    /* transmit string "xmit_msg" into UART transmission 16-bit word   */
    /* and place them in the transmit buffer "xmitbuf".  In addition,  */
    /* 16-bit Start and 8-bit Stop framing words, respectively, are    */
    /* inserted before and after each of the ASCII characters in the   */
    /* buffer.                                                         */
    /*******************************************************************/
    void ProcessTransmitData(void)
    {
        int        i;
        short    cnt = 1;
        unsigned char     xmit_char;
        unsigned short    *xmitbufptr;
       
        /* point to Transmit Buffer    */
        xmitbufptr = (unsigned short *)xmitbuf;

        for (i=0; i<(sizeof(xmitbuf)/sizeof(unsigned int)); i++)
        {
            xmitbufptr[i] = 0x0000;    /* zero fill buffer    */
        }

        xmitbufptr = (unsigned short *)xmitbuf;   
       
        /* Process data BYTES in xmit_msg[] and put in xmit buffer    */
        for (i = 0; i <= BUFFER_SIZE; i++)
        {    
            /*Get transmit character (one byte) from xmit_msg[] and put in xmit buffer*/
            xmit_char    =    xmit_msg[i];
       
            /* Process each BYTE of transmit character    */
            for (cnt = -1; cnt < 10; cnt++)
            {
                if (cnt == -1)
                {
                    *xmitbufptr++     =     0x0000;
               
                 }
                else if (cnt == 8 || cnt ==9)
                {
                    *xmitbufptr++     =     0xFFFF;
                              }
                else if (xmit_char & (1 << cnt))
                {
                    *xmitbufptr++    =    0xFFFF;
               
                }
                else
                {
                    *xmitbufptr++    =    0x0000;
                   
                }
               
                // MCBSP_write(hMcbsp1,*xmitbufptr);               
            }    /* end for cnt    */     
            //MCBSP_write(hMcbsp1,xmit_char);    
           
        }    /* end for i*/
           
        for(i=0;i<=55;i++)
        printf("%x\n",xmitbuf[i]);
       
    }    /* end ProcessTransmitData    */


    /*******************************************************************/
    /* void ProcessReceiveData(void)                                   */
    /*                                                                 */
    /* This function decodes the data in the receive buffer, "recvbuf" */
    /* and strips the framing start (0x0000) and Stop (0xFFFF) words.  */
    /* It calls the subroutine VoteLogic() to determine each bit of    */
    /* the ASCII character.  It then puts the result in recv_msg.      */
    /*******************************************************************/
    void ProcessReceiveData(void)
    {
        int    i;
        unsigned char recv_char = 0;
        short cnt = -1;
        short recv_val;
        unsigned short    raw_data;
        unsigned short    *recvbufptr;    /*receive buffer pointer*/

        /* Point to the receive buffer    */
        recvbufptr    = (unsigned short *)recvbuf;
        /* Process all data in the Receive buffer    */
        for (i = 0; i < BUFFER_SIZE; i++)
        {
            recv_char = 0;
           
            /* Process each UART frame    */
            for (cnt = -1; cnt < 10; cnt++)
            {
                if(cnt == -1 || cnt == 8 || cnt == 9)
                {
                    /* Ignore Start and Stop bits    */
                    *recvbufptr++;
                }
                else
                {
                    /* Get 16-bit data from receive buffer    */
                    raw_data    =    *recvbufptr;
                    recvbufptr++;
                   
                    /* get the value of the majority of the bits    */
                    recv_val    =    VoteLogic(raw_data);
                   
                    /* put received bit into proper place    */
                    recv_char    += recv_val << cnt;
                }   
            }    /* end for cnt    */
       
            /* A full BYTE is decoded. Put in result: recv_msg[i]    */
            recv_msg[i]    =    recv_char;
        //    printf("\n%s",recv_msg);

        }    /* end for i    */
       
    }    /* end ProcessReceiveData() function    */


    /*******************************************************************/
    /* void CheckTestCase(void)                                        */
    /*******************************************************************/
    int CheckTestCase(void)
    {
        unsigned short *source;
        unsigned short *result;
        unsigned int i = 0;
        short cnt = -1;
        int error = 0;
       
        source = (unsigned short *) xmitbuf;
        result = (unsigned short *) recvbuf;
       
        for (i = 0; i < BUFFER_SIZE ; i++)
        {
            for (cnt = -1; cnt < 10; cnt++)
            {
            //    printf("\n%x",*source);
            //    printf("\n%x",*result);
                /* Ignore the start and stop bits */
                if(cnt == -1 || cnt == 8 || cnt ==9)
                {
                    source++;
                    result++;
                }
                else
                {
                    if (*source != *result)
                    {
                        error = i + 1;
                        break;
                    }
                    source++;
                    result++;
                }
            }
        }
        //printf("%d",error);
       
        return(error);
       
    }    /* end CheckTestCase() function */


    /*******************************************************************/
    /* short VoteLogic(unsigned short)                                 */
    /*                                                                 */
    /* This function decoded the received character by testing the     */
    /* center 4 bits of the baud.  A majority rule is used for the     */
    /* decoding.                                                       */
    /*******************************************************************/
    short VoteLogic(unsigned short value)
    {
        short returnvalue;

        switch    ((value    >>    6)    & 0x0F)
        {
            case    0:
            case    1:           
            case    2:   
            case    3:               
            case    4:   
            case    5:   
            case    6:   
            case    8:   
            case    9:                                               
            case    10:
                            returnvalue = 0;
                            break;   
            case    7:   
            case    11:                           
            case    12:   
            case    13:   
            case    14:                           
            case    15:
                            returnvalue = 1 ;
                            break;
        }    /* end switch    */
       
        return (returnvalue);

    }    /* end VoteLogic() funciton    */    


    /*–––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––*/
    /* set_interrupts_edma() */
    /*–––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––––*/
    #if (EDMA_SUPPORT)
    void /* Set the interrupts */
    set_interrupts_edma(void) /* if the device supports EDMA */
    {
    IRQ_nmiEnable();
    IRQ_globalEnable();
    IRQ_reset(IRQ_EVT_EDMAINT);
    IRQ_disable(IRQ_EVT_EDMAINT);
    EDMA_intDisable(14); /* ch 12 for McBSP transmit event XEVT0 */
    EDMA_intDisable(15); /* ch 13 for McBSP receive event REVT0 */
    IRQ_clear(IRQ_EVT_EDMAINT);
    EDMA_intClear(14);
    EDMA_intClear(15);
    IRQ_enable(IRQ_EVT_EDMAINT);
    EDMA_intEnable(14);
    EDMA_intEnable(15);
    return;
    }
    #endif

    /*******************************************************************/
    /* EDMA Data Transfer Completion ISRs                              */
    /*******************************************************************/

     
    interrupt void
    c_int11(void)  /* DMA 2 */
    {
        #if (DMA_SUPPORT)
            transmit_done = TRUE;
        //    printf("Transmit Completed\n");
        #endif
    }

    interrupt void
    c_int09(void)  /* DMA 1 */
    {
        #if (DMA_SUPPORT)
            receive_done = TRUE;
        //    printf("Receive Completed\n");
        #endif
    }


    interrupt void
    c_int08(void)
    {
        #if (EDMA_SUPPORT)
            if (EDMA_intTest(14))
            {
                transmit_done = TRUE;
                EDMA_intClear(14);
            printf("Transmit Completed\n");
            }
       
            if (EDMA_intTest(15))
            {
                receive_done = TRUE;
                EDMA_intClear(15);
                printf("Receive Completed\n\n");
            }
        #endif
        return;
    }


    plz chk the McBSP config part if there is some error!!

  • Avinash,

    Are you able to scope the signals that are being looped back?  Do they look ok?

    -Tommy