Hi All,
I have just successfully got Gingerbread 2.3.4 working on the BeagleBoard XM, thanks to the instructions posted on the Ti WIKI. I am connected to the BeagleBoard via a serial cable, and am looking at the debug messages. I noticed the following messages, and am wondering if other people see the binder messages that are bolded below? Are these normal?
enabling adb
adb_open
# warning: `zygote' uses 32-bit capabilities (legacy support in use)
usb 1-2.4: USB disconnect, address 4
usb 1-2.4: new low speed USB device using ehci-omap and address 5
usb 1-2.4: New USB device found, idVendor=093a, idProduct=2510
usb 1-2.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-2.4: Product: USB Optical Mouse
usb 1-2.4: Manufacturer: PixArt
input: PixArt USB Optical Mouse as /devices/platform/ehci-omap.0/usb1/1-2/1-2.4/1-2.4:1.0/input/input3
generic-usb 0003:093A:2510.0002: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ehci-omap.0-2.4/input0
binder: release 1435:1435 transaction 2686 out, still active
binder: 1122:1529 transaction failed 29189, size 14628-0
binder: send failed reply for transaction 2686, target dead
binder: release 1683:1683 transaction 4115 out, still active
binder: 1122:1122 transaction failed 29189, size 5276-0
binder: send failed reply for transaction 4115, target dead
binder: release 1765:1765 transaction 4318 out, still active
binder: release 1765:1809 transaction 4278 out, still active
binder: release 1765:1810 transaction 4284 out, still active
binder: release 1765:1811 transaction 4312 out, still active
binder: 1409:1568 transaction failed 29189, size 28-4
binder: send failed reply for transaction 4278, target dead
binder: 1409:1424 transaction failed 29189, size 28-4
binder: send failed reply for transaction 4284, target dead
binder: 1409:1427 transaction failed 29189, size 28-4
binder: send failed reply for transaction 4312, target dead
binder: 1409:1812 transaction failed 29189, size 2372-0
binder: send failed reply for transaction 4318, target dead
Thanks a lot again for your help.
Kiran