This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK Raw Ethernet, not really raw?



Can the NDK be used for true raw ethernet with promiscous receive (and send) for all packets regardless of mac header?

if so, what are the api calls to set it up and do it?

These questions were posted over a week ago and so far there are no replies.  Meanwhile, grep and pdf search do not turn up anything on promiscous mode in the documents or source code.  That is a little dissappointing.

 

  • Mitch,

    As we've already discussed via email, I'm posting the solution to this thread so that others may find this if they run into the same problem. Can you please mark this thread as "verified answer?"

    -------------------------------------- original email of solution ------------------------------------------------

    Mitch,

    I think I am getting close to getting the driver in promiscuous mode.  I wanted to share what I know now, in case you wanted to try on your end.

     

    First off, we’ve found the following doc:

     

    http://focus.ti.com/lit/ug/sprufl5b/sprufl5b.pdf

     

    5.21 Receive Multicast/Broadcast/Promiscuous Channel Enable Register

    (RXMBPENABLE)

     

    Looking at the above section, there’s a table that has some bits that we want to set:

     

    The RXPROMCH bit in RXMBPENABLE selects the promiscuous channel to receive frames selected by

    the RXCMFEN, RXCSFEN, RXCEFEN, and RXCAFEN bits. These four bits allow reception of MAC

    control frames, short frames, error frames, and all frames (promiscuous), respectively.

     

    Also from the doc:

     

    2.10.8 Promiscuous Receive Mode

    When the promiscuous receive mode is enabled by setting the RXCAFEN bit in the receive

    multicast/broadcast/promiscuous channel enable register (RXMBPENABLE), nonaddress matching frames

    that would normally be filtered are transferred to the promiscuous channel. Address matching frames that

    would normally be filtered due to errors are transferred to the address match channel when the RXCAFEN

    and RXCEFEN bits in RXMBPENABLE are set. A frame is considered to be an address matching frame

    only if it is enabled to be received on a unicast, multicast, or broadcast channel. Frames received to

    disabled unicast, multicast, or broadcast channels are considered nonaddress matching.

    MAC control frames address match only if the RXCMFEN bit in RXMBPENABLE is set. The RXCEFEN

    and RXCSFEN bits in RXMBPENABLE determine whether error frames are transferred to memory or not,

    but they do not determine whether error frames are address matching or not. Short frames are a special

    type of error frames.

    A single channel is selected as the promiscuous channel by the RXPROMCH bit in RXMBPENABLE. The

    promiscuous receive mode is enabled by the RXCMFEN, RXCEFEN, RXCSFEN, and RXCAFEN bits in

    RXMBPENABLE. Table 5 shows the effects of the promiscuous enable bits. Proper frames are frames

    that are between 64 bytes and the value in the receive maximum length register (RXMAXLEN) bytes in

    length inclusive and contain no code, align, or CRC errors.

    So, given all of this, I’ve tried the following.  I’m having some issues verifying whether or not the driver is actually in promiscuous mode or not, but I though I’d share these steps in case you want to try it on your end:

     

    Here’s the steps:

     

    1. increase the size of the receive buffers by A LOT (in ethdriver.c)

    #define     PKT_MAX                     190          // à  previously this was 64

     

    1. Add this flag EMAC_CONFIG_MODEFLG_PASSALL to ModeFlags (ethdriver.c)

     

        ecfg.ModeFlags             = EMAC_CONFIG_MODEFLG_RXOFFLENBLOCK |

                                     EMAC_CONFIG_MODEFLG_RMII |

                                     EMAC_CONFIG_MODEFLG_PASSALL;

       ecfg.MdioModeFlags         = MDIO_MODEFLG_AUTONEG;

     

    1. Updated the EmacStart() function (nimu_eth.c):

     

            /* Set the 'initial' Receive Filter */

            // ptr_pvt_data->pdi.Filter = ETH_PKTFLT_MULTICAST;  // previous value

            ptr_pvt_data->pdi.Filter = EMAC_RXFILTER_ALL;

     

           setting the above results in the following code being run in EMAC_setReceiveFilter():

     

        if (ReceiveFilter == EMAC_RXFILTER_ALL){

            CSL_FINST(EMAC_REGS->RXMBPENABLE, EMAC_RXMBPENABLE_RXCAFEN, ENABLE);

            CSL_FINS( EMAC_REGS->RXMBPENABLE, EMAC_RXMBPENABLE_RXPROMCH, masterChannel);

        }

    Regards,

     

    Steve

    below is the original files sent from this email:

    8284.promisc01.zip

     

    below contains further updates, however they are unverified by the customer:

    7522.promisc02.zip


  • That's fine, and i marked it verified.  This does put the hardware interface in promiscous mode. Packets with non-matching headers, and also those with matching headers, were received in the raw socket in our test application.

    However there is a caveat or two that should be mentioned.

    1)  The first is that not all packets are passed to the raw socket; packets are filtered by ether type in NIMUReceivePacket() in nimu_eth.c.  If the application needs to get all valid packets (or all packets), some additional patching may be needed.

    2) The second is that the solution includes a patch to EmacStart ()  in nimu.c.   An application that wants to do both non-promisc and promisc will need to patch accordingly.

    Summing up "NDK Raw Ethernet, not really raw?"; the answer is that the hardware can do it, and the NIMU NDK can do it with some patching..