My development enviroment
OMAP-L137
CCS 3.3.81.11
BIOS 5.33.01
PSP 01.30.01
EDMA3 01.11.01.04
The PSP 01.30.01 SPI driver does not work in EDMA mode with 16 bit data. It transfers only the lower 8 bits of every 16 bit word. I have ported over the char width related changes from PSP 2.10.01. It appears to work. Attached are the patched files. Are there any other changes I need to port over? Will there every be a newer version of PSP 1 or a PSP 2 thats supports the OMAP-L137? Also, I believe PSP 2.10 webpage note states support for DA830. Shouldn't that be DA850 to match OMAP-L138 and C6748?