Hi Champs,
While building the BIOS PSP application using the xdc, i am getting the warning message,
"warning: creating output section ".plt" without a SECTIONS specification"
The binary is built for DM814x - A8 core.
The tool chains being used are,
BIOS - 6_33_00_19
XDC - 3_23_00_32
CG tools for TMS470 - 4.9.0
It looks like some section is missing and it is being initialized by the xdc. Do i need to add something in the .cfg file?
Please find the attached cfg file also.
Let me know, if any more info is required.
Thanks and Regards,
Sandeep K