Hello,
I'm working in a signal processing system and I need to use UPP. I've implemented it using the driver you provide and I have it running in an OMAP L138 with DSPBIOS 5. However we need to implement it in the ARM core instead the DSP one so we need to make it run in SYSBIOS.
Is there any possibility to make uPP driver to run on ARM (to use it with SYSBIOS)?? Are you planning to publish a new version which support SYSBIOS? In short, is there any way to use UPP with high-level functions, without the need of going down to registers level?
Best Regards