This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTDX in CCS V5



Is there any plan to include RTDX back in the future? Why is it phased out? Any alternative?

  • Eruan,

    No, RTDX will not be brought back.

    The System Analyzer is the replacement, and is described here: http://processors.wiki.ti.com/index.php/Multicore_System_Analyzer

    Scott

  • I do not see capabilities like RTDX(where I can inject data in for processing and extract the output) in the the Multicore System Analyzer. Also the Multicore System Analyzer is not available for C55x. Or am I wrong?

  • Eruan,

    Correct, the System Analyzer is focused on instrumentation and analysis of the running application.  In the past, that was the primary use case of RTDX by DSP/BIOS.  The generalized data transport mechanism that RTDX also provided is not available with System Analyzer, and I don’t know of any alternatives to recommend to you.

    And right, there is no System Analyzer support on C55x.

    Scott

  • Upgrading to Windows 7 forces me to upgrade to CCS 5. Keeping up with the newest version of a development environment is supposed to be common sense, right? But now I have no RTDX anymore? This seems to me to be rather a huge step backwards. What if all my recent developments under CCS 3.x were totally relying on RTDX in the development/debugging phase?

    What else do I have to give up by moving to CCS 5 as compared to CCS 3.x? Is there a list somewhere which outlines all the great features of CCS 5 that I did not have in CCS 3.x. I do need motivation for upgrading ;-).

    Regards,

    Roland