This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

'utils.tci' Trying to open the Wrong File (one that doesn't exist...)



While attempting to compile this project I get the following error...

"C:/MyProjects/SRW_DSP/SRW/Project/BIOS/SRW_C64XX.tcf"

js: "C:/Program Files/Texas Instruments/xdctools_3_20_08_88/include/utils.tci", line 582: Error: Can't find import file: './SRW_C64XX.tci'

It is attempting to open ./SRW_C64XX.tci... which does not exist.  What I want it to open is SRW_C64XX.tci which is located in the same place as SRW_C64XX.tcf.  What I don't understand is where the ./ came from.  Is it something with Code Composer by any chance? (probably not)  Or has anyone ever had a similar problem?

Thanks for any help.

  • Was this a CCS 3.3 project that was imported into CCSv4 or a new project created with CCS4? This post discusses a similar error but I'm not sure how helpful it will be in your situation. I will also move your question to the BIOS forum as the experts there might have additional suggestions.

  • Hi Ellen,

    Can you please post the full build output you see when trying to build your project?

    Also, please attach your *.tcf file and any *.tci files that are included.

    Finally, which version of BIOS, XDCtools, Code Composer, and other components are you using?

    Thanks,

    Steve

  • Thank you for your replies.

    I actually managed to fix it by moving my .tci file to a different location.  There were only a couple locations that the .tcf was looking for it and by moving it to one of those it now builds.  I also altered the .tcf and that worked too.  Apparently the ./ just indicated that it was looking in the wrong directory.  I don't understand why including the path in CCS didn't work though...

    This was code written in CCSv3.3 that I imported to CCSv4.2 and I am having a horrible time trying to get it to run.

    Thanks again.

    Ellen