This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EZSDK 5.03.01 is now available for download



 

The Linux EZSDK Release 5.03.01.15 is available for download from http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/latest/index_FDS.html

This release supports DM816x and DM814x and has been validated on DM8168 PG2.0 and PG1.1 EVMs with DDR3 and DM8148 PG2.1 EVMs. The following high-level features are new from the previous EZSDK release version 5.03.00.09

  • GStreamer support, GStreamer Plug-in on Linux 2.6.37, AV Playback demo on Matrix with GStreamer
  • SW Mosaic component (EDMA based)
  • MJPEG decoder on IVAHD
  • Other critical bug fixes from previous EZSDK releases

This release includes the features and components listed at  http://processors.wiki.ti.com/index.php/EZSDK_Feature_List. The EZSDK comes with a set of pre-applied patches to several software components. Details on patches applied and errata are available at http://processors.wiki.ti.com/index.php/EZSDK_5.03_Patches_and_Errata. FAQ on EZSDK is at http://processors.wiki.ti.com/index.php/EZ_SDK_FAQ. Details on memory layout changes are available at http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map 

The landing page for EZSDK Wiki topics is http://processors.wiki.ti.com/index.php/Category:EZSDK and the landing page for OMX Wiki topics is http://processors.wiki.ti.com/index.php/Category:OMX