HI all,
I found that the RTC was alway reset. When reset the IPNC board, the RTC will run from year 2000.
# hwclock
Sat Jan 1 00:00:02 2000 0.000000 seconds
# hwclock
Sat Jan 1 00:00:05 2000 0.000000 seconds
BR
Terry K.G
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI all,
I found that the RTC was alway reset. When reset the IPNC board, the RTC will run from year 2000.
# hwclock
Sat Jan 1 00:00:02 2000 0.000000 seconds
# hwclock
Sat Jan 1 00:00:05 2000 0.000000 seconds
BR
Terry K.G
HI Kirill,
My board had battery yet.But I found 2 strange issues about R93 on mainboard.Here are the SCH & PCB copied from Appro:
A.if Connecting R93, it will display "RTC time out" when loading kernel.
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
B. If disconnect R93. The RTC will reset when power on.
# hwclock
Sat Jan 1 00:00:02 2000 0.000000 seconds
# hwclock
Sat Jan 1 00:00:05 2000 0.000000 seconds
BTW, can you help my other post--How to flash ubl+uboot to IPNC from Serial ?
BR
Terry K.G
Hi
Me too have the same issue, we aslo using appro refference design, when i put the R93 i am getting the "rtc wait time out !!!!!" due to the RTC Reset fail.. in the u-boot.
Can u put some light into this issue, Is this a silicon bug with DM365
Regrads
Joseph George
Dear Terry,
The status A is correct. Please turn off the IPNC about one hour and then reset the IPNC later, the messages "rtc wait time out !!!!!" will bypass. Of course, you can short the circuit about capacitor to discharge electricity directly.
Best Regards,
Appro Support Team
George,
Thanks for picthing in and helping to answer on this pending topic.
Regards,
Anshuman
Hi
Me too have the same issue, we aslo using appro refference design, (dm368)
Please let me know if a solution for this exists
Regrads
jun-sic
Hi ?
not be able to use the RTC dm365's are considered, connect an external RTC chip. And Replacing the RTC chip DS1307 rtc-ds1307.ko driver module from the kernel creates raised, but no there is no response. board-dm365-ipnc.c files at i2c/rtc set ds1307 need to register? Please help me.
Hi,
The platform is DM365 and DM368 IPNC. It display "RTC reset fail" in UBL and "rtc wait time out !!!!!" in loading kernel.
I found that RTC PRTCIF_CTRL Register's BUSY bit was always '1', even if I reset IPNC or power off. If turn off the IPNC about half one hour or short the circuit about capacitor, the message will bypass.
I don't konw what is the actual cause fro this issue. I will sell the IPNC product to my customers. When the RTC fail, customers can't turn off the IPNC about half one hour or short the circuit.
Can you tell me what is the actual cause and how to solve the problem ?
Is this a silicon bug with DM365 or DM368 ?
Thanks